![]() |
PDK API Guide for J721E
|
Holds the Enet_Pn_FIFO_Status register contents.
Data Fields | |
Uint32 | estBufAct |
Uint32 | estAddErr |
Uint32 | estCntErr |
Uint32 | txExpressMacAllow |
Uint32 | txPriActive |
Uint32 CSL_CPGMAC_SL_FIFOSTATUS::estBufAct |
EST RAM active buffer . Indicates the active 64-word fetch buffer when pn_est_onebuf is cleared to zero. Indicates the fetch ram address MSB when pn_est_onebuf set to one.
Uint32 CSL_CPGMAC_SL_FIFOSTATUS::estAddErr |
EST Address Error Indicates that the fetch ram was read again after the previous maximum buffer address read (the previous fetch from the maximum address is reused).
Uint32 CSL_CPGMAC_SL_FIFOSTATUS::estCntErr |
EST Fetch Count Error Indicates that insufficient clocks were programmed into the fetch count and that another fetch was commanded before the previous fetch finished.
Uint32 CSL_CPGMAC_SL_FIFOSTATUS::txExpressMacAllow |
EST transmit mac allow Bus that indicates the actual priorities assigned to the express queue (and inversely the priorities assigned to the prempt queue). The pn_mac_prempt[7:0] field in the Enet_Pn_IET_Control register indicates which priorities should be assigned to the express/prempt queues. The switch between queues happens only when the priority is empty and the actual assignment is shown in this field.
Uint32 CSL_CPGMAC_SL_FIFOSTATUS::txPriActive |
EST Transmit Priority Active Bus that indicates which priorities have packets (non-empty) at the time of the register read.