![]() |
PDK API Guide for J721E
|
Stream Frame Capture Control configuration. Used to specify the frame count value when when the CSIRX must generate interrupts FCC_START and FCC_STOP. This register must only be modified when the corresponding frame count enable is disabled.
Data Fields | |
uint16_t | frameCountStop |
uint16_t | frameCountStart |
uint16_t CSIRX_StreamFccCfg::frameCountStop |
Indicates the frame number on which the interrupt should be generated and the stream will stop outputting data on the pixel interface. (0x0000 will be continuous frames.)
uint16_t CSIRX_StreamFccCfg::frameCountStart |
Indicates the frame number on which the interrupt should be generated and the stream will start outputting data on the pixel interface. (0x0000 will be the current frame.)