![]() |
PDK API Guide for J721E
|
This file contains the definition of all the message IDs, message formats to be able to interact with the System Controller firmware for DKEK management.
Go to the source code of this file.
Functions | |
int32_t | Sciclient_setDKEK (const struct tisci_msg_sa2ul_set_dkek_req *req, struct tisci_msg_sa2ul_set_dkek_resp *resp, uint32_t timeout) |
Request to derive a KEK and set SA2UL DKEK register. More... | |
int32_t | Sciclient_releaseDKEK (const struct tisci_msg_sa2ul_release_dkek_req *req, struct tisci_msg_sa2ul_release_dkek_resp *resp, uint32_t timeout) |
Request to erase the DKEK register. More... | |
int32_t | Sciclient_getDKEK (const struct tisci_msg_sa2ul_get_dkek_req *req, struct tisci_msg_sa2ul_get_dkek_resp *resp, uint32_t timeout) |
Request for getting the firewall permissions. More... | |