![]() |
PDK API Guide for J721E
|
OS Abstraction Layer header.
============================================================================
Go to the source code of this file.
Data Structures | |
struct | Osal_StaticMemStatus |
This structure holds static memory status parameters of OSAL library. More... | |
struct | Osal_memRange |
Osal memory address range. More... | |
struct | Osal_HwAttrs |
Osal hw attributes structure. More... | |
Macros | |
#define | osal_WAIT_FOREVER (~((uint32_t)0U)) |
#define | osal_NO_WAIT ((uint32_t)0U) |
#define | OSAL_NONOS_SEMAPHOREP_SIZE_BYTES ((uint32_t) 48U) |
#define | OSAL_NONOS_HWIP_SIZE_BYTES ((uint32_t) 48U) |
#define | OSAL_FREERTOS_HWIP_C7X_SIZE_BYTES ((uint32_t) 56U) |
#define | OSAL_TIRTOS_SEMAPHOREP_SIZE_BYTES ((uint32_t) 96U) |
#define | OSAL_TIRTOS_HWIP_SIZE_BYTES (96U) |
#define | OSAL_FREERTOS_SEMAPHOREP_SIZE_BYTES ((uint32_t) 96U) |
#define | OSAL_FREERTOS_TASKP_SIZE_BYTES ((uint32_t) 128U) |
#define | OSAL_SAFERTOS_SEMAPHOREP_SIZE_BYTES ((uint32_t) 136U) |
#define | OSAL_SAFERTOS_TASKP_SIZE_BYTES ((uint32_t) 248U) |
#define | OSAL_Assert(expression) |
Assert checking function. More... | |
#define | OSAL_COMPILE_TIME_SIZE_CHECK(x, y) |
Osal Error return Codes | |
Return error codes for Osal generic APIs | |
#define | osal_OK (0) |
#define | osal_FAILURE (-(int32_t)(1)) |
#define | osal_UNSUPPORTED (-(int32_t)(2)) |
#define | osal_NOMEM (-(int32_t)(3)) |
Osal HwAttrs ValidBit definitions | |
#define | OSAL_HWATTR_SET_EXT_CLK (0x00000001U) |
#define | OSAL_HWATTR_SET_ECM_INT (0x00000002U) |
#define | OSAL_HWATTR_SET_HWACCESS_TYPE (0x00000004U) |
#define | OSAL_HWATTR_SET_OSALDELAY_TIMER_BASE (0x00000008U) |
#define | OSAL_HWATTR_SET_SEMP_EXT_BASE (0x00000010U) |
#define | OSAL_HWATTR_SET_HWIP_EXT_BASE (0x00000020U) |
#define | OSAL_HWATTR_SET_CPU_FREQ (0x00000040U) |
#define | OSAL_HWATTR_SET_TARG_PROC_LIST (0x00000080) |
Enumerations | |
enum | Osal_ThreadType { Osal_ThreadType_Hwi, Osal_ThreadType_Swi, Osal_ThreadType_Task, Osal_ThreadType_Main } |
This enum defines the multiple thread types used under OSAL library. More... | |
enum | Osal_HwAccessType { OSAL_HWACCESS_UNRESTRICTED, OSAL_HWACCESS_RESTRICTED } |
Osal hw access type. More... | |
Functions | |
void | Osal_DebugP_assert (int32_t expression, const char *file, int32_t line) |
Osal_ThreadType | Osal_getThreadType (void) |
Function to get the current thread type. More... | |
int32_t | Osal_delay (uint32_t nTicks) |
Function to delay/sleep the specified number of ticks. More... | |
int32_t | Osal_setHwAttrs (uint32_t ctrlBitMap, const Osal_HwAttrs *hwAttrs) |
Function to set the Hw Attributes. More... | |
int32_t | Osal_getHwAttrs (Osal_HwAttrs *hwAttrs) |
Function to get the Hw Attributes. More... | |
int32_t | Osal_getStaticMemStatus (Osal_StaticMemStatus *pMemStat) |
Function to get the static memory usage of OSAL library. More... | |
int32_t | Osal_getCoreId (void) |
Function to get the core ID of the running Core. More... | |
void | OS_init (void) |
Function for initializing the OS / scheduler. More... | |
void | OS_start (void) |
Function to strat OS / scheduler. More... | |
void | OS_stop (void) |
Function to stop OS / scheduler. More... | |
Variables | |
Osal_HwAttrs | gOsal_HwAttrs |
external references for Osal Hw Attribute structure More... | |