![]() |
PDK API Guide for J721E
|
DMSC controls the power management, security and resource management of the device.
Macros | |
#define | TISCI_MSG_VALUE_RM_SECONDARY_HOST_VALID ((uint32_t) 1u << 31u) |
This file contains: More... | |
#define | TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST (0xFFu) |
#define TISCI_MSG_VALUE_RM_SECONDARY_HOST_VALID ((uint32_t) 1u << 31u) |
This file contains:
WARNING!!: Autogenerated file from SYSFW. DO NOT MODIFY!!
System Firmware TISCI RM Messaging Core
Common TISCI Protocol Definitions for RM messagesThe secondary_host parameter is valid for any RM TISCI message utilizing the seconday host mechanic.
#define TISCI_MSG_VALUE_RM_UNUSED_SECONDARY_HOST (0xFFu) |
Value specified for the secondary_host element within TISCI RM messages to signify the secondary_host value is not used and the source host of the message is specified in the TISCI message header tisci_header::host field.