![]() |
PDK API Guide for J721E
|
Data Structures | |
struct | LwipifEnetAppIf_RxConfig |
struct | LwipifEnetAppIf_TxConfig |
struct | LwipifEnetAppIf_GetHandleInArgs |
Input arguments passed to the application via LwipifEnetAppCb_getHandle() when Enet's netif is initialized. More... | |
struct | Lwip2EnetAppIf_FreePktInfo |
Container structure of packet free callback info. More... | |
struct | LwipifEnetAppIf_RxHandleInfo |
RX-related parameters required by Enet's netif. They are populated by application. More... | |
struct | LwipifEnetAppIf_TxHandleInfo |
TX-related parameters required by Enet's netif. They are populated by application. More... | |
struct | LwipifEnetAppIf_GetHandleOutArgs |
Output arguments to be populated by application via LwipifEnetAppCb_getHandle() when Enet's netif is initialized. More... | |
struct | LwipifEnetAppIf_ReleaseHandleInfo |
Arguments passed to application by Enet's netif during deinitialization. More... | |
Functions | |
void | LwipifEnetAppCb_getHandle (LwipifEnetAppIf_GetHandleInArgs *inArgs, LwipifEnetAppIf_GetHandleOutArgs *outArgs) |
Callback function used by Enet's netif to delegate TX/RX channel open to the application. More... | |
void | LwipifEnetAppCb_releaseHandle (LwipifEnetAppIf_ReleaseHandleInfo *releaseInfo) |
Callback function used by Enet's netif to delegate TX/RX channel close to the application. More... | |
Typedefs | |
typedef void(* | LwipifEnetAppIf_FreePktCbFxn) (void *cbArg, EnetDma_PktQ *fqPktInfoQ, EnetDma_PktQ *cqPktInfoQ) |
Callback function used to free packets. More... | |
typedef bool(* | LwipifEnetAppIf_IsPhyLinkedCbFxn) (struct netif *netif, Enet_Handle hEnet) |
Callback function used to check PHY link status. More... | |
typedef bool(* | LwipifEnetAppIf_HandleRxPktFxn) (struct netif *netif, struct pbuf *pbuf) |
Callback function used to pass packets to application for processing. More... | |
Macros | |
#define | LWIP2ENET_RX_NUM (2U) |
Number of RX channels. More... | |
#define LWIP2ENET_RX_NUM (2U) |
Number of RX channels.
typedef void(* LwipifEnetAppIf_FreePktCbFxn) (void *cbArg, EnetDma_PktQ *fqPktInfoQ, EnetDma_PktQ *cqPktInfoQ) |
Callback function used to free packets.
Prototype of the callback function used by Enet's netif to free packets during deinitialization stage.
cbArg | Callback function argument. |
fqPktInfoQ | Pointer to free queue (FQ). |
cqPktInfoQ | Pointer to completion queue (CQ). |
typedef bool(* LwipifEnetAppIf_IsPhyLinkedCbFxn) (struct netif *netif, Enet_Handle hEnet) |
Callback function used to check PHY link status.
Prototype of the callback function used by Enet's netif to check the PHY link status.
netif | Enet's netif. |
hEnet | Enet driver handle. |
typedef bool(* LwipifEnetAppIf_HandleRxPktFxn) (struct netif *netif, struct pbuf *pbuf) |
Callback function used to pass packets to application for processing.
When application provides a valid callback function, netif will call this function for "processing":
This mechanism requires LWIPIF_APP_RX_PKT_HANDLING
build flag to be enabled.
netif | Enet's netif. |
pbuf | Enet driver handle. |
true | Packet will not be passed to the stack. |
false | Packet will be passed to the stack as usual. |
void LwipifEnetAppCb_getHandle | ( | LwipifEnetAppIf_GetHandleInArgs * | inArgs, |
LwipifEnetAppIf_GetHandleOutArgs * | outArgs | ||
) |
Callback function used by Enet's netif to delegate TX/RX channel open to the application.
This callback function is called by Enet's netif during initialization stage to open TX and RX channels. This callback must be implemented by the application.
inArgs | Pointer to parameters needed by application to open TX and RX channels. |
outArgs | Parameters obtained during TX/RX channel opening which need to be returned to Enet's netif, i.e. channel handles. |
void LwipifEnetAppCb_releaseHandle | ( | LwipifEnetAppIf_ReleaseHandleInfo * | releaseInfo | ) |
Callback function used by Enet's netif to delegate TX/RX channel close to the application.
This callback function is called by Enet's netif during deinitialization stage to close TX and RX channels. This callback must be implemented by the application.
releaseInfo | Pointer to parameters/handles needed by application to close TX and RX channels. |