![]() |
PDK API Guide for J721E
|
Prototypes for the driver API functions. The user application can link statically to the necessary API functions and call them directly.
Functions | |
uint32_t | CSITX_Probe (const CSITX_Config *config, CSITX_SysReq *memReq) |
uint32_t | CSITX_Init (CSITX_PrivateData *pD, const CSITX_Config *config, const CSITX_Callbacks *callbacks) |
void | CSITX_Isr (CSITX_PrivateData *pD) |
void | CSITX_Start (CSITX_PrivateData *pD) |
void | CSITX_Stop (CSITX_PrivateData *pD) |
void | CSITX_Destroy (void) |
uint32_t | CSITX_SetConfigurationMode (CSITX_PrivateData *pD, uint32_t enable) |
uint32_t | CSITX_GetConfigurationMode (CSITX_PrivateData *pD, uint32_t *enable) |
uint32_t | CSITX_SetDphyConfig (CSITX_PrivateData *pD, const CSITX_DphyConfig *config) |
uint32_t | CSITX_GetDphyConfig (CSITX_PrivateData *pD, CSITX_DphyConfig *config) |
uint32_t | CSITX_SetDphyConfig1 (CSITX_PrivateData *pD, const CSITX_DphyConfig1 *config) |
uint32_t | CSITX_GetDphyConfig1 (CSITX_PrivateData *pD, CSITX_DphyConfig1 *config) |
uint32_t | CSITX_SetVirtualChannelConfig (const CSITX_PrivateData *pD, const CSITX_VirtualChannelConfig *config, CSITX_VcNumber number) |
uint32_t | CSITX_GetVirtualChannelConfig (const CSITX_PrivateData *pD, CSITX_VirtualChannelConfig *config, CSITX_VcNumber number) |
uint32_t | CSITX_SetDataTypeConfig (const CSITX_PrivateData *pD, const CSITX_DataTypeConfig *config, CSITX_DtNumber number) |
uint32_t | CSITX_GetDataTypeConfig (const CSITX_PrivateData *pD, CSITX_DataTypeConfig *config, CSITX_DtNumber number) |
uint32_t | CSITX_SetStreamConfig (const CSITX_PrivateData *pD, const CSITX_StreamConfig *config, CSITX_IfNumber number) |
uint32_t | CSITX_GetStreamConfig (const CSITX_PrivateData *pD, CSITX_StreamConfig *config, CSITX_IfNumber number) |
uint32_t | CSITX_SetBypassModeEnable (CSITX_PrivateData *pD, bool enable) |
uint32_t | CSITX_GetBypassModeEnable (CSITX_PrivateData *pD, bool *enable) |
uint32_t | CSITX_SetSoftResetRequest (CSITX_PrivateData *pD, bool enable) |
uint32_t | CSITX_GetSoftResetRequest (CSITX_PrivateData *pD, bool *enable) |
uint32_t | CSITX_SetInterruptsEnable (CSITX_PrivateData *pD, bool enable) |
uint32_t | CSITX_GetInterruptsEnable (CSITX_PrivateData *pD, bool *enable) |
uint32_t | CSITX_GetStatusRegister (CSITX_PrivateData *pD, uint32_t *value) |
uint32_t | CSITX_GetDphyStatusRegister (CSITX_PrivateData *pD, uint32_t *value) |
uint32_t | CSITX_SetRegWaitBurstTime (CSITX_PrivateData *pD, CSITX_WaitBurstTimeConfig *config) |
uint32_t | CSITX_GetRegWaitBurstTime (CSITX_PrivateData *pD, CSITX_WaitBurstTimeConfig *config) |
uint32_t | CSITX_SetDphyClkWakeup (CSITX_PrivateData *pD, uint16_t value) |
uint32_t | CSITX_GetDphyClkWakeup (CSITX_PrivateData *pD, uint16_t *value) |
uint32_t | CSITX_SetDphyUlpsWakeup (CSITX_PrivateData *pD, uint16_t value) |
uint32_t | CSITX_GetDphyUlpsWakeup (CSITX_PrivateData *pD, uint16_t *value) |
uint32_t | CSITX_SetDebugEnable (CSITX_PrivateData *pD, bool enable) |
uint32_t | CSITX_GetDebugEnable (CSITX_PrivateData *pD, bool *enable) |
uint32_t | CSITX_GetDebugProtFsm (CSITX_PrivateData *pD, uint32_t *value, CSITX_IfNumber number) |
uint32_t | CSITX_GetDebugLnFsm (CSITX_PrivateData *pD, uint32_t *value) |
uint32_t | CSITX_GetDebugClkLnFsm (CSITX_PrivateData *pD, uint32_t *value) |
uint32_t | CSITX_GetDebugDataLnFsm (CSITX_PrivateData *pD, uint32_t *value) |
uint32_t | CSITX_SetTestGenericCtrl (CSITX_PrivateData *pD, uint16_t value) |
uint32_t | CSITX_GetTestGenericCtrl (CSITX_PrivateData *pD, uint16_t *value) |
uint32_t | CSITX_GetTestGenericStatus (CSITX_PrivateData *pD, uint16_t *value) |
uint32_t | CSITX_GetAsfInfo (const CSITX_PrivateData *pD, CSITX_AsfInfo *asfInfo) |
uint32_t | CSITX_GetDeviceConfig (const CSITX_PrivateData *pD, CSITX_DeviceConfig *value) |
uint32_t | CSITX_SetEpdConfig (CSITX_PrivateData *pD, const CSITX_EpdConfig *config) |
uint32_t | CSITX_GetEpdConfig (CSITX_PrivateData *pD, CSITX_EpdConfig *config) |
uint32_t | CSITX_SetScramblerMode (CSITX_PrivateData *pD, bool enable) |
uint32_t | CSITX_GetScramblerMode (CSITX_PrivateData *pD, bool *enable) |
uint32_t | CSITX_SetRxCompatibility (CSITX_PrivateData *pD, CSITX_RxCompatibilityConfig *config) |
uint32_t | CSITX_GetRxCompatibility (CSITX_PrivateData *pD, CSITX_RxCompatibilityConfig *config) |
uint32_t CSITX_Probe | ( | const CSITX_Config * | config, |
CSITX_SysReq * | memReq | ||
) |
"Get the driver's memory requirements to support the given configuration."
[in] | config | "Driver/hardware configuration required." |
[out] | memReq | "Size of the memory allocation required." |
uint32_t CSITX_Init | ( | CSITX_PrivateData * | pD, |
const CSITX_Config * | config, | ||
const CSITX_Callbacks * | callbacks | ||
) |
"Initialise the driver instance and state, configure the CSITX as specified in the 'config' settings. The function enables the datapath." @param [in] pD "Driver state info specific to this instance." @param [in] config "Specifies driver/hardware configuration." @param [in] callbacks "Client-supplied callback functions."
void CSITX_Isr | ( | CSITX_PrivateData * | pD | ) |
"Driver ISR. Platform-specific code is responsible for ensuring this gets called when the corresponding hardware's interrupt is asserted. Registering the ISR should be done after calling init, and before calling start. The driver's ISR will not attempt to lock any locks, but will perform client callbacks. If the client wishes to defer processing to non-interrupt time, it is responsible for doing so." @param [in] pD "Driver instance data filled by Init."
void CSITX_Start | ( | CSITX_PrivateData * | pD | ) |
"Start the CSITX driver, enabling interrupts. This is called after the client has successfully initialized the driver and hooked the driver's ISR (the isr member of this struct) to the IRQ." @param [in] pD "Driver state info specific to this instance."
void CSITX_Stop | ( | CSITX_PrivateData * | pD | ) |
"Stop the CSITX driver, disabling interrupts."
[in] | pD | "Driver state info specific to this instance." |
void CSITX_Destroy | ( | void | ) |
"Destructor for the driver."
uint32_t CSITX_SetConfigurationMode | ( | CSITX_PrivateData * | pD, |
uint32_t | enable | ||
) |
"Enables or disables Configuration Request."
[in] | pD | "Driver instance data." |
[in] | enable | "True to enable Configuration Request, false to disable". |
uint32_t CSITX_GetConfigurationMode | ( | CSITX_PrivateData * | pD, |
uint32_t * | enable | ||
) |
"Gets value of the Configuration request."
[in] | pD | "Driver instance data." |
[out] | enable | "'configuration_request' bit from the CONFIG register is tested. If enable Configuration Request is enabled, false otherwise." |
uint32_t CSITX_SetDphyConfig | ( | CSITX_PrivateData * | pD, |
const CSITX_DphyConfig * | config | ||
) |
"Performs D-PHY configuration."
[in] | pD | "Driver instance data." |
[in] | config | "Configuration to apply to D-PHY." |
uint32_t CSITX_GetDphyConfig | ( | CSITX_PrivateData * | pD, |
CSITX_DphyConfig * | config | ||
) |
"Reads the D-PHY configuration."
[in] | pD | "Driver instance data." |
[out] | config | "DPHY config." |
uint32_t CSITX_SetDphyConfig1 | ( | CSITX_PrivateData * | pD, |
const CSITX_DphyConfig1 * | config | ||
) |
"Performs D-PHY configuration (DPHY CFG1)."
[in] | pD | "Driver instance data." |
[in] | config | "Configuration to apply to DPHY CFG1." |
uint32_t CSITX_GetDphyConfig1 | ( | CSITX_PrivateData * | pD, |
CSITX_DphyConfig1 * | config | ||
) |
"Reads DPHY configuration (DPHY CFG1)."
[in] | pD | "Driver instance data." |
[out] | config | "DPHY CFG1 config." |
uint32_t CSITX_SetVirtualChannelConfig | ( | const CSITX_PrivateData * | pD, |
const CSITX_VirtualChannelConfig * | config, | ||
CSITX_VcNumber | number | ||
) |
"Writes a virtual channel configuration."
[in] | pD | "Driver instance data." |
[in] | config | "Virtual channel configuration." |
[in] | number | Number of the Virtual channel to configure |
uint32_t CSITX_GetVirtualChannelConfig | ( | const CSITX_PrivateData * | pD, |
CSITX_VirtualChannelConfig * | config, | ||
CSITX_VcNumber | number | ||
) |
"Reads a virtual channel configuration."
[in] | pD | "Driver instance data." |
[out] | config | "Virtual channel configuration." |
[in] | number | Number of the virtual channel |
uint32_t CSITX_SetDataTypeConfig | ( | const CSITX_PrivateData * | pD, |
const CSITX_DataTypeConfig * | config, | ||
CSITX_DtNumber | number | ||
) |
"Writes a data type configuration."
[in] | pD | "Driver instance data." |
[in] | config | "Data type configuration." |
[in] | number | Number of the Data type to configure. |
uint32_t CSITX_GetDataTypeConfig | ( | const CSITX_PrivateData * | pD, |
CSITX_DataTypeConfig * | config, | ||
CSITX_DtNumber | number | ||
) |
"Reads a data type configuration."
[in] | pD | "Driver instance data." |
[out] | config | "Data type configuration." |
[in] | number | Number of the data type |
uint32_t CSITX_SetStreamConfig | ( | const CSITX_PrivateData * | pD, |
const CSITX_StreamConfig * | config, | ||
CSITX_IfNumber | number | ||
) |
"Writes a stream configuration."
[in] | pD | "Driver instance data." |
[in] | config | "Stream configuration." |
[in] | number | Pixel interface number. |
uint32_t CSITX_GetStreamConfig | ( | const CSITX_PrivateData * | pD, |
CSITX_StreamConfig * | config, | ||
CSITX_IfNumber | number | ||
) |
"Reads a stream configuration."
[in] | pD | "Driver instance data." |
[out] | config | "Stream configuration." |
[in] | number | Pixel interface number. |
uint32_t CSITX_SetBypassModeEnable | ( | CSITX_PrivateData * | pD, |
bool | enable | ||
) |
"Enables or disables Bypass Mode request."
[in] | pD | "Driver instance data." |
[in] | enable | True to enable Bypass mode, false to disable. |
uint32_t CSITX_GetBypassModeEnable | ( | CSITX_PrivateData * | pD, |
bool * | enable | ||
) |
"Gets value of the Bypass Mode Enable request."
[in] | pD | "Driver instance data." |
[out] | enable | "'bypass_mode_enable' bit from the CONFIG register is tested. If enable Bypass Mode Enable is enabled, false otherwise." |
uint32_t CSITX_SetSoftResetRequest | ( | CSITX_PrivateData * | pD, |
bool | enable | ||
) |
"Enables or disables soft reset request."
[in] | pD | Driver instance data |
[in] | enable | True to enable soft reset request false to disable. |
uint32_t CSITX_GetSoftResetRequest | ( | CSITX_PrivateData * | pD, |
bool * | enable | ||
) |
"Gets value of the soft reset request."
[in] | pD | Driver instance data |
[out] | enable | "'soft_reset_request' bit from the CONFIG register is tested. If enable soft reset request is enabled, false otherwise." |
uint32_t CSITX_SetInterruptsEnable | ( | CSITX_PrivateData * | pD, |
bool | enable | ||
) |
"Enables or disables interrupts. Note that in order to generate interrupts the IRQ_MASK register must be configured first. If in the driver initialization stage the 'CSITX_Config.enableInterrupts = true', then the IRQ_MASK is configured that all interrupts are generated."
[in] | pD | Driver instance data |
[in] | enable | True to enable interrupts, false to disable. |
uint32_t CSITX_GetInterruptsEnable | ( | CSITX_PrivateData * | pD, |
bool * | enable | ||
) |
"Gets value of the interrupts."
[in] | pD | "Driver instance data." |
[out] | enable | "'irq_enable' bit from the CONFIG register If true interrupts are enabled, false otherwise." |
uint32_t CSITX_GetStatusRegister | ( | CSITX_PrivateData * | pD, |
uint32_t * | value | ||
) |
"Reads Status register value."
[in] | pD | "Driver instance data." |
[out] | value | "Contents of the STATUS register." |
uint32_t CSITX_GetDphyStatusRegister | ( | CSITX_PrivateData * | pD, |
uint32_t * | value | ||
) |
"Reads D-PHY Status register value."
[in] | pD | "Driver instance data." |
[out] | value | "Contents of the DPHY_STATUS register." |
uint32_t CSITX_SetRegWaitBurstTime | ( | CSITX_PrivateData * | pD, |
CSITX_WaitBurstTimeConfig * | config | ||
) |
"Writes DPHY Wait Time Configuration."
[in] | pD | "Driver instance data." |
[in] | config | DPHY Wait Time Configuration. |
uint32_t CSITX_GetRegWaitBurstTime | ( | CSITX_PrivateData * | pD, |
CSITX_WaitBurstTimeConfig * | config | ||
) |
"Reads DPHY Wait Time Configuration."
[in] | pD | "Driver instance data." |
[out] | config | "DPHY Wait Time Configuration." |
uint32_t CSITX_SetDphyClkWakeup | ( | CSITX_PrivateData * | pD, |
uint16_t | value | ||
) |
"Writes DPHY_CLK_WAKEUP register with value."
[in] | pD | "Driver instance data." |
[in] | value | Value to write to the DPHY_CLK_WAKEUP register. |
uint32_t CSITX_GetDphyClkWakeup | ( | CSITX_PrivateData * | pD, |
uint16_t * | value | ||
) |
"Reads DPHY_CLK_WAKEUP register value."
[in] | pD | "Driver instance data." |
[out] | value | "Contents of the DPHY_CLK_WAKEUP register." |
uint32_t CSITX_SetDphyUlpsWakeup | ( | CSITX_PrivateData * | pD, |
uint16_t | value | ||
) |
"Writes DPHY_ULPS_WAKEUP register with value."
[in] | pD | "Driver instance data." |
[in] | value | Value to write to the DPHY_ULPS_WAKEUP register. |
uint32_t CSITX_GetDphyUlpsWakeup | ( | CSITX_PrivateData * | pD, |
uint16_t * | value | ||
) |
"Reads DPHY_ULPS_WAKEUP register value."
[in] | pD | "Driver instance data." |
[out] | value | "Contents of the DPHY_ULPS_WAKEUP register." |
uint32_t CSITX_SetDebugEnable | ( | CSITX_PrivateData * | pD, |
bool | enable | ||
) |
"Enables or disables CSITX debugging functionality."
[in] | pD | "Driver instance data." |
[in] | enable | "True to enable debugging functionality, false to disable." |
uint32_t CSITX_GetDebugEnable | ( | CSITX_PrivateData * | pD, |
bool * | enable | ||
) |
"Reads status of the core debug functionality."
[in] | pD | "Driver instance data." |
[out] | enable | "True if the the core debug functionality is enabled false otherwise." |
uint32_t CSITX_GetDebugProtFsm | ( | CSITX_PrivateData * | pD, |
uint32_t * | value, | ||
CSITX_IfNumber | number | ||
) |
"Reads debug register for a given Pixel pixel interface."
[in] | pD | "Driver instance data." |
[out] | value | "Contents of the DEBUG_PROT_FSM register." |
[in] | number | Number of the Pixel interface. |
uint32_t CSITX_GetDebugLnFsm | ( | CSITX_PrivateData * | pD, |
uint32_t * | value | ||
) |
"Reads DEBUG_LN_FSM register register value."
[in] | pD | "Driver instance data." |
[out] | value | "Contents of the DEBUG_LN_FSM register." |
uint32_t CSITX_GetDebugClkLnFsm | ( | CSITX_PrivateData * | pD, |
uint32_t * | value | ||
) |
"Reads DEBUG_CLK_LN_FSM register register value."
[in] | pD | "Driver instance data." |
[out] | value | "Contents of the DEBUG_CLK_LN_FSM register." |
uint32_t CSITX_GetDebugDataLnFsm | ( | CSITX_PrivateData * | pD, |
uint32_t * | value | ||
) |
"Reads DEBUG_DATA_LN_FSM register register value."
[in] | pD | "Driver instance data." |
[out] | value | "Contents of the DEBUG_DATA_LN_FSM register." |
uint32_t CSITX_SetTestGenericCtrl | ( | CSITX_PrivateData * | pD, |
uint16_t | value | ||
) |
"Sets test_generic_ctrl field of the GENERIC Register."
[in] | pD | "Driver instance data." |
[in] | value | "Test generic_ctrl value." |
uint32_t CSITX_GetTestGenericCtrl | ( | CSITX_PrivateData * | pD, |
uint16_t * | value | ||
) |
"Gets test_generic_ctrl field of the GENERIC Register."
[in] | pD | "Driver instance data." |
[out] | value | "D-PHY config." |
uint32_t CSITX_GetTestGenericStatus | ( | CSITX_PrivateData * | pD, |
uint16_t * | value | ||
) |
"Reads test_generic_status field of the GENERIC register"
[in] | pD | "Driver instance data." |
[out] | value | "Contents of the test_generic_status field". |
uint32_t CSITX_GetAsfInfo | ( | const CSITX_PrivateData * | pD, |
CSITX_AsfInfo * | asfInfo | ||
) |
Retrieves ASF information from CSITX controller.
[in] | pD | Pointer to driver's private data object. |
[out] | asfInfo | Pointer to ASF information structure. |
uint32_t CSITX_GetDeviceConfig | ( | const CSITX_PrivateData * | pD, |
CSITX_DeviceConfig * | value | ||
) |
"Getter for DeviceConfig."
[in] | pD | "Pointer to the private data initialized by init". |
[out] | value | "Output value." |
uint32_t CSITX_SetEpdConfig | ( | CSITX_PrivateData * | pD, |
const CSITX_EpdConfig * | config | ||
) |
"Writes EPD configuration."
[in] | pD | "Driver instance data." |
[in] | config | EPD configuration. |
uint32_t CSITX_GetEpdConfig | ( | CSITX_PrivateData * | pD, |
CSITX_EpdConfig * | config | ||
) |
"Reads EPD configuration."
[in] | pD | "Driver instance data." |
[out] | config | EPD configuration. |
uint32_t CSITX_SetScramblerMode | ( | CSITX_PrivateData * | pD, |
bool | enable | ||
) |
"Enables or disables Scrambler mode."
[in] | pD | Driver instance data |
[in] | enable | True to enable scrambler mode, false to disable. |
uint32_t CSITX_GetScramblerMode | ( | CSITX_PrivateData * | pD, |
bool * | enable | ||
) |
"Gets value of the scrambler mode."
[in] | pD | Driver instance data |
[out] | enable | "Scrambler mode status." |
uint32_t CSITX_SetRxCompatibility | ( | CSITX_PrivateData * | pD, |
CSITX_RxCompatibilityConfig * | config | ||
) |
"Set CSIRX compatibility features."
[in] | pD | Driver instance data |
[in] | config | CSIRX compatibility configuration. |
uint32_t CSITX_GetRxCompatibility | ( | CSITX_PrivateData * | pD, |
CSITX_RxCompatibilityConfig * | config | ||
) |
"Get CSIRX compatibility features."
[in] | pD | Driver instance data |
[out] | config | CSIRX compatibility configuration. |