![]() |
PDK API Guide for J721E
|
Functions | |
uint32_t | CSL_ringaccGetRevision (const CSL_RingAccCfg *pCfg) |
Return revision of the RingAcc module. More... | |
void | CSL_ringaccInitRingCfg (CSL_RingAccRingCfg *pRingCfg) |
Initialize a CSL_RingAccRingCfg structure. More... | |
void | CSL_ringaccInitRingObj (uint32_t ringNum, CSL_RingAccRingCfg *pRing) |
Initialize the ring object. More... | |
int32_t | CSL_ringaccInitRing (CSL_RingAccCfg *pCfg, uint32_t ringNum, CSL_RingAccRingCfg *pRing) |
Initialize a ring. More... | |
int32_t | CSL_ringaccSetEvent (CSL_RingAccCfg *pCfg, uint32_t ringNum, uint32_t evtNum) |
Set the ring event. More... | |
uint32_t | CSL_ringaccGetRingNum (const CSL_RingAccRingCfg *pRing) |
Get the ring number associated with a ring. More... | |
void | CSL_ringaccSetRingOrderId (CSL_RingAccCfg *pCfg, const CSL_RingAccRingCfg *pRing, uint32_t orderId) |
Specify the orderid value for a ring. More... | |
void | CSL_ringaccCfgRingCred (CSL_RingAccCfg *pCfg, const CSL_RingAccRingCfg *pRing, bool bEnable, bool bLock) |
Configure the security credentials for a ring. More... | |
void | CSL_ringaccResetRing (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing) |
Reset a ring. More... | |
void * | CSL_ringaccGetCmdRingPtr (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing) |
Get pointer to next free command ring element. More... | |
void * | CSL_ringaccGetRspRingPtr (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing) |
Get pointer to next available response ring element. More... | |
static int32_t | CSL_ringaccSetRingDoorbell (CSL_RingAccCfg *pCfg, uint32_t ringNum, int32_t cnt) |
Write to the ring doorbell. More... | |
static void | CSL_ringaccCommitToCmdRing (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, int32_t cnt) |
Commit elements written to a ring. More... | |
void | CSL_ringaccAckRspRing (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, int32_t cnt) |
Acknowledge elements read from a ring. More... | |
int32_t | CSL_ringaccCfgTrace (CSL_RingAccCfg *pCfg, bool bTraceAll, bool bIncMsgData, uint32_t ringNum) |
Configure trace support. More... | |
int32_t | CSL_ringaccSetTraceEnable (CSL_RingAccCfg *pCfg, bool bEnable) |
Enable or disable trace support. More... | |
int32_t | CSL_ringaccEnableTrace (CSL_RingAccCfg *pCfg) |
Enable trace support. More... | |
int32_t | CSL_ringaccDisableTrace (CSL_RingAccCfg *pCfg) |
Disable trace support. More... | |
uint32_t | CSL_ringaccGetRingIdx (const CSL_RingAccCfg *pCfg, uint32_t ringNum) |
Get the current ring read/write index. More... | |
uint32_t | CSL_ringaccGetRingHwIdx (const CSL_RingAccCfg *pCfg, uint32_t ringNum) |
Get the current ring hardware read/write index (for debug). More... | |
uint32_t | CSL_ringaccGetRingOcc (const CSL_RingAccCfg *pCfg, uint32_t ringNum) |
Get the current ring occupancy. More... | |
uint32_t | CSL_ringaccGetRingHwOcc (const CSL_RingAccCfg *pCfg, uint32_t ringNum) |
Get the current ring hardware occupancy (for debug). More... | |
int32_t | CSL_ringaccCfgRingMonitor (CSL_RingAccCfg *pCfg, uint32_t monNum, CSL_RingAccMonitorType monType, uint32_t ringNum, uint32_t eventNum, CSL_RingAccMonitorDataSrc dataSrc, uint32_t data0Val, uint32_t data1Val) |
Configure a ring monitor. More... | |
int32_t | CSL_ringaccReadRingMonitor (const CSL_RingAccCfg *pCfg, uint32_t monNum, uint32_t *pData0, uint32_t *pData1) |
Read a ring monitor. More... | |
int32_t | CSL_ringaccPush32 (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint32_t val, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Push a 32-bit value to the tail of a ring. More... | |
int32_t | CSL_ringaccPop32 (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint32_t *pVal, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Pop a 32-bit value from the head of a ring. More... | |
int32_t | CSL_ringaccHwPop32 (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint32_t *pVal, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Mimic a hardware pop of a 32-bit value from the head of a ring. More... | |
int32_t | CSL_ringaccPeek32 (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint32_t *pVal, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Peek at a 32-bit value from the head of a ring. More... | |
int32_t | CSL_ringaccPush64 (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint64_t val, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Push a 64-bit value to the tail of a ring. More... | |
int32_t | CSL_ringaccPop64 (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint64_t *pVal, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Pop a 64-bit value from the head of a ring. More... | |
int32_t | CSL_ringaccHwPop64 (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint64_t *pVal, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Mimic a hardware pop of a 64-bit value from the head of a ring. More... | |
int32_t | CSL_ringaccPeek64 (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint64_t *pVal, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Peek at a 64-bit value from the head of a ring. More... | |
int32_t | CSL_ringaccWrData (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint8_t *pData, uint32_t numBytes, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Write data into a ring (ring mode only) More... | |
int32_t | CSL_ringaccRdData (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint8_t *pData, uint32_t numBytes, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Read data from a ring (ring mode only) More... | |
int32_t | CSL_ringaccPeekData (CSL_RingAccCfg *pCfg, CSL_RingAccRingCfg *pRing, uint8_t *pData, uint32_t numBytes, CSL_ringaccMemOpsFxnPtr pfMemOps) |
Peek at data from a ring (ring mode only) More... | |
uint32_t CSL_ringaccGetRevision | ( | const CSL_RingAccCfg * | pCfg | ) |
Return revision of the RingAcc module.
This function returns the contents of the RingAcc revision register. Consult the RingAcc module documentation for a description of the contents of the revision register.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
void CSL_ringaccInitRingCfg | ( | CSL_RingAccRingCfg * | pRingCfg | ) |
Initialize a CSL_RingAccRingCfg structure.
This function initializes the specified CSL_RingAccRingCfg structure to known, safe values. Software then only needs to configure elements that are different than their initialized values prior to calling the CSL_ringaccInitRing function.
All elements of the CSL_RingAccRingCfg structure are initialized to zero except for the following:
evtNum = CSL_RINGACC_RING_EVENT_DISABLE; // 0xFFFFU
pRingCfg | [OUT] Pointer to a CSL_RingAccRingCfg structure |
void CSL_ringaccInitRingObj | ( | uint32_t | ringNum, |
CSL_RingAccRingCfg * | pRing | ||
) |
Initialize the ring object.
This function is used to initialize the ring object without configuring the ring.
ringNum | [IN] The number of the ring (0-1023) to be initialized |
pRing | [OUT] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
int32_t CSL_ringaccInitRing | ( | CSL_RingAccCfg * | pCfg, |
uint32_t | ringNum, | ||
CSL_RingAccRingCfg * | pRing | ||
) |
Initialize a ring.
This function is used to initialize the ring specified by RingNum. A ring must be initialized prior to calling any of the following functions:
#CSL_ringaccPairRing #CSL_ringaccResetRing #CSL_ringaccGetCmdRingPtr #CSL_ringaccGetRspRingPtr #CSL_ringaccCommitToCmdRing #CSL_ringaccAckRspRing #CSL_ringaccSetRingOrderId
To use this function, allocate a CSL_RingAccRingCfg structure and initialize the following structure elements. Then, pass a pointer to this structure along with the other required arguments.
virtBase Virtual base address of the ring memory physBase Physical base address of the ring memory mode The mode of the ring elCnt Ring element count elSz Ring element size in bytes (4,8,16,32,64,128,256) evtNum Event number for the ring
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
ringNum | [IN] The number of the ring (0-1023) to be initialized |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
int32_t CSL_ringaccSetEvent | ( | CSL_RingAccCfg * | pCfg, |
uint32_t | ringNum, | ||
uint32_t | evtNum | ||
) |
Set the ring event.
This function is used to set the the ring event based on RingNum.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
ringNum | [IN] The number of the ring (0-1023) to be initialized |
evtNum | [IN] Event number for the ring |
uint32_t CSL_ringaccGetRingNum | ( | const CSL_RingAccRingCfg * | pRing | ) |
Get the ring number associated with a ring.
This function is used to get the ring number associated with the specified ring.
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
void CSL_ringaccSetRingOrderId | ( | CSL_RingAccCfg * | pCfg, |
const CSL_RingAccRingCfg * | pRing, | ||
uint32_t | orderId | ||
) |
Specify the orderid value for a ring.
This function is used to specify the orderid value for a ring's destination transactions. If orderId == CSL_RINGACC_ORDERID_BYPASS, then the orderid from the source transaction is used.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
orderId | [IN] The orderId value, or CSL_RINGACC_ORDERID_BYPASS to use the orderid from the source transaction |
void CSL_ringaccCfgRingCred | ( | CSL_RingAccCfg * | pCfg, |
const CSL_RingAccRingCfg * | pRing, | ||
bool | bEnable, | ||
bool | bLock | ||
) |
Configure the security credentials for a ring.
This function is used to configure the security credentials for a ring.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
bEnable | [IN] true = Region is enabled, false = disabled |
bLock | [IN] true = Region is locked (region values cannot be changed), false = region is not locked |
void CSL_ringaccResetRing | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing | ||
) |
Reset a ring.
This function is used to reset a ring. The ring is reset back to its original state where the ring occupancy is 0 (empty) and the ring read and write pointers are reset to 0.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
void* CSL_ringaccGetCmdRingPtr | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing | ||
) |
Get pointer to next free command ring element.
This function is used to get a pointer to the next free element of a a transmit ring. This pointer can then be used to write data into the ring.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
void* CSL_ringaccGetRspRingPtr | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing | ||
) |
Get pointer to next available response ring element.
This function is used to get a pointer to the next available receive element of a ring. This pointer can then be used to read data from the ring.
If the ring is paired, a successful return will also credit the paired command ring with an additional free entry.
After the data has been read from the ring, call the CSL_ringaccAckRspRing to acknowledge and return the element(s) that have been read.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
|
inlinestatic |
Write to the ring doorbell.
This function writes 'count' to the command ring doorbell register of the specified ring.
Normally, an application does not need to call this function as the CSL_ringaccCommitToCmdRing function calls it.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
ringNum | [IN] The ring number (0-1023) |
cnt | [IN] The count to write |
|
inlinestatic |
Commit elements written to a ring.
This function is used to commit (execute) elements that have been written to a ring.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
cnt | [IN] The number of elements written since the last call to CSL_ringaccCommitToCmdRing, or NULL to commit all outstanding entries. |
void CSL_ringaccAckRspRing | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
int32_t | cnt | ||
) |
Acknowledge elements read from a ring.
This function is used to acknowledge and return elements that have been read from a ring.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
cnt | [IN] The number of elements read since the last call to CSL_ringaccAckRspRing, or NULL to ACK all outstanding entries. |
int32_t CSL_ringaccCfgTrace | ( | CSL_RingAccCfg * | pCfg, |
bool | bTraceAll, | ||
bool | bIncMsgData, | ||
uint32_t | ringNum | ||
) |
Configure trace support.
This function configures trace support. Tracing is automatically disabled before the specified trace configuration is written.
When tracing is enabled (see the CSL_ringaccSetTraceEnable function) a trace output of all push, pop, and peek operations are output so that the traffic can be viewed at a later time.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
bTraceAll | [IN] If true, operations to every ring are traced. If false, only the ring specified by ringNum is traced. |
bIncMsgData | [IN] If true, message data is included in the trace output. |
ringNum | [IN] Specifies the ring whose operations are to be traced. This parameter is ignored when bTraceAll is true. |
int32_t CSL_ringaccSetTraceEnable | ( | CSL_RingAccCfg * | pCfg, |
bool | bEnable | ||
) |
Enable or disable trace support.
This function enables or disables trace support. Be sure and configure trace support using the CSL_ringaccCfgTrace function before enabling it.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
bEnable | [IN] If true, trace support is enabled. If false, it is disabled. |
int32_t CSL_ringaccEnableTrace | ( | CSL_RingAccCfg * | pCfg | ) |
Enable trace support.
This function enables trace support. Be sure and configure tarce support using the CSL_ringaccCfgTrace function before enabling it.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
int32_t CSL_ringaccDisableTrace | ( | CSL_RingAccCfg * | pCfg | ) |
Disable trace support.
This function disables trace support.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
uint32_t CSL_ringaccGetRingIdx | ( | const CSL_RingAccCfg * | pCfg, |
uint32_t | ringNum | ||
) |
Get the current ring read/write index.
This function returns the current command read/write index for the specified ring.
Normally, an application does not need to call this function.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
ringNum | [IN] The ring number (0-1023) |
uint32_t CSL_ringaccGetRingHwIdx | ( | const CSL_RingAccCfg * | pCfg, |
uint32_t | ringNum | ||
) |
Get the current ring hardware read/write index (for debug).
This function returns the current ring read/write index (as seen by HW) for the specified ring.
Normally, an application does not need to call this function.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
ringNum | [IN] The ring number (0-1023) |
uint32_t CSL_ringaccGetRingOcc | ( | const CSL_RingAccCfg * | pCfg, |
uint32_t | ringNum | ||
) |
Get the current ring occupancy.
This function returns the current ring occupancy for the specified ring.
Normally, an application does not need to call this function.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
ringNum | [IN] The ring number (0-1023) |
uint32_t CSL_ringaccGetRingHwOcc | ( | const CSL_RingAccCfg * | pCfg, |
uint32_t | ringNum | ||
) |
Get the current ring hardware occupancy (for debug).
This function returns the current ring occupancy (as seen by HW) for the specified ring.
Normally, an application does not need to call this function.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
ringNum | [IN] The ring number (0-1023) |
int32_t CSL_ringaccCfgRingMonitor | ( | CSL_RingAccCfg * | pCfg, |
uint32_t | monNum, | ||
CSL_RingAccMonitorType | monType, | ||
uint32_t | ringNum, | ||
uint32_t | eventNum, | ||
CSL_RingAccMonitorDataSrc | dataSrc, | ||
uint32_t | data0Val, | ||
uint32_t | data1Val | ||
) |
Configure a ring monitor.
This function is used to configure a ring monitor.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
monNum | [IN] The number of the monitor to configure |
monType | [IN] The type of ring monitor. See CSL_RingAccMonitorType for the available monitor types. |
ringNum | [IN] The number of the ring to monitor |
eventNum | [IN] The number of the event to produce if the monitor thresholds are exceeded (used only for the CSL_RINGACC_MONITOR_TYPE_THRESHOLD or CSL_RINGACC_MONITOR_TYPE_STARVATION monitor types). A value of CSL_RINGACC_MONITOR_INTR_DISABLE disables interrupts for this monitor. |
dataSrc | [IN] The type of data this monitor is tracking. See CSL_RingAccMonitorDataSrc for available data sources. This is only used for CSL_RINGACC_MONITOR_TYPE_THRESHOLD and CSL_RINGACC_MONITOR_TYPE_WATERMARK monitor types. |
data0Val | [IN] This value contains the low threshold value for the CSL_RINGACC_MONITOR_TYPE_THRESHOLD or CSL_RINGACC_MONITOR_TYPE_STARVATION monitor types. It is not used for the other monitor types. |
data1Val | [IN] This value contains the high threshold value for the CSL_RINGACC_MONITOR_TYPE_THRESHOLD or CSL_RINGACC_MONITOR_TYPE_STARVATION monitor types. It is not used for the other monitor types. |
int32_t CSL_ringaccReadRingMonitor | ( | const CSL_RingAccCfg * | pCfg, |
uint32_t | monNum, | ||
uint32_t * | pData0, | ||
uint32_t * | pData1 | ||
) |
Read a ring monitor.
This function is used to read data from an active ring monitor.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
monNum | [IN] The number of the monitor to read |
pData0 | [OUT] A pointer to where the following value (dependingon the type of monitor) is written: o CSL_RINGACC_MONITOR_TYPE_STATS: count of the number of writes to the queue o CSL_RINGACC_MONITOR_TYPE_THRESHOLD: low threshold value o CSL_RINGACC_MONITOR_TYPE_WATERMARK: low watermark value o CSL_RINGACC_MONITOR_TYPE_STARVATION: number of starvation events (a read to an empty queue) |
pData1 | [OUT] A pointer to where the following value (depending on the type of monitor) is written: o CSL_RINGACC_MONITOR_TYPE_STATS: count of the number of reads from the queue o CSL_RINGACC_MONITOR_TYPE_THRESHOLD: high threshold value o CSL_RINGACC_MONITOR_TYPE_WATERMARK: high watermark value o CSL_RINGACC_MONITOR_TYPE_STARVATION: not used |
int32_t CSL_ringaccPush32 | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint32_t | val, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Push a 32-bit value to the tail of a ring.
This function is used to push a 32-bit value to the tail of a ring. This function supports all ring modes.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
val | [IN] 32-bit value to write to the ring |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed). The memory fence call-back is used for rings configured in ring mode only. |
int32_t CSL_ringaccPop32 | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint32_t * | pVal, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Pop a 32-bit value from the head of a ring.
This function is used to pop a 32-bit value from the head of a ring. This function supports all ring modes.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
pVal | [OUT] Pointer where the popped value is returned |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed) |
int32_t CSL_ringaccHwPop32 | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint32_t * | pVal, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Mimic a hardware pop of a 32-bit value from the head of a ring.
This function is used to mimic a hardware pop operation from a ring. It can be called by software to pop values from a ring that is configured in Ring Mode, where software is the normal producer (pushing to the ring via the CSL_ringaccPush32 function) and hardware is the normal consumer (popping from the ring), such as a TX free queue ring.
The ring must be configured with a 4-byte element size. A 4-byte value is popped from the ring head and returned.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
pVal | [OUT] Pointer where the popped value is returned |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed) |
int32_t CSL_ringaccPeek32 | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint32_t * | pVal, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Peek at a 32-bit value from the head of a ring.
This function is used to peek at a 32-bit value from the head of a ring. This function supports all ring modes.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
pVal | [OUT] Pointer where the peeked value is returned |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed) |
int32_t CSL_ringaccPush64 | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint64_t | val, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Push a 64-bit value to the tail of a ring.
This function is used to push a 64-bit value to the tail of a ring. This function supports all ring modes.
This function can only be used when the calling processor is able to issue a 64-bit burst. If using a 32-bit processor, you should avoid using this function and instead use the proxy to read/write from/to rings.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
val | [IN] 32-bit value to write to the ring |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed). The memory fence call-back is used for rings configured in ring mode only. |
int32_t CSL_ringaccPop64 | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint64_t * | pVal, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Pop a 64-bit value from the head of a ring.
This function is used to pop a 64-bit value from the head of a ring. This function supports all ring modes.
This function can only be used when the calling processor is able to issue a 64-bit burst. If using a 32-bit processor, you should avoid using this function and instead use the proxy to read/write from/to rings.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
pVal | [OUT] Pointer where the popped value is returned |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed) |
int32_t CSL_ringaccHwPop64 | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint64_t * | pVal, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Mimic a hardware pop of a 64-bit value from the head of a ring.
This function is used to mimic a hardware pop operation from a ring. It can be called by software to pop values from a ring that is configured in Ring Mode, where software is the normal producer (pushing to the ring via the CSL_ringaccPush64 function) and hardware is the normal consumer (popping from the ring), such as a TX free queue ring.
The ring must be configured with an 8-byte element size. An 8-byte value is popped from the ring head and returned.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
pVal | [OUT] Pointer where the popped value is returned |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed) |
int32_t CSL_ringaccPeek64 | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint64_t * | pVal, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Peek at a 64-bit value from the head of a ring.
This function is used to peek at a 64-bit value from the head of a ring. This function supports all ring modes.
This function can only be used when the calling processor is able to issue a 64-bit burst. If using a 32-bit processor, you should avoid using this function and instead use the proxy to read/write from/to rings.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
pVal | [OUT] Pointer where the peeked value is returned |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed) |
int32_t CSL_ringaccWrData | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint8_t * | pData, | ||
uint32_t | numBytes, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Write data into a ring (ring mode only)
This function is used to write data into a ring. It can only be used with a ring configured in ring mode. This function does nothing if the ring is any other mode.
Note that software can only write to a given ring, or read from a given ring - it cannot write and read to/from a given ring.
To write data to rings configured in modes other than ring mode, use the proxy.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
pData | [IN] Pointer to the data to write |
numBytes | [IN] The number of bytes to write |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed). |
int32_t CSL_ringaccRdData | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint8_t * | pData, | ||
uint32_t | numBytes, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Read data from a ring (ring mode only)
This function is used to read data from a ring. It can only be used with a ring configured in ring mode. This function does nothing if the ring is any other mode.
To read data from rings configured in modes other than ring mode, use the proxy.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
pData | [IN] Pointer to where read data is returned |
numBytes | [IN] The number of bytes to read |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed) |
int32_t CSL_ringaccPeekData | ( | CSL_RingAccCfg * | pCfg, |
CSL_RingAccRingCfg * | pRing, | ||
uint8_t * | pData, | ||
uint32_t | numBytes, | ||
CSL_ringaccMemOpsFxnPtr | pfMemOps | ||
) |
Peek at data from a ring (ring mode only)
This function is used to peek at data from a ring. It can only be used with a ring configured in ring mode. This function does nothing if the ring is any other mode.
To peek at data from rings configured in modes other than ring mode, use the proxy.
pCfg | [IN] Pointer to a CSL_RingAccCfg structure containing the ring accelerator configuration |
pRing | [IN] Pointer to a CSL_RingAccRingCfg structure containing the ring configuration |
pData | [IN] Pointer to where read data is returned |
numBytes | [IN] The number of bytes to peek |
pfMemOps | [IN] Pointer to a memory ops call-back function (or NULL if not needed) |