![]() |
PDK API Guide for J721E
|
Macros | |
#define | CSL_DRU_MAX_CH (512U) |
Maximum number of channels supported by DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_CH macro. More... | |
#define | CSL_DRU_NUM_CH (64U) |
Number of channels supported by the DRU. More... | |
#define | CSL_DRU_MAX_QUEUE (8U) |
Maximum number of queues supported by DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_QUEUE macro. More... | |
#define | CSL_DRU_NUM_QUEUE (5U) |
Number of queues supported by the DRU. More... | |
#define | CSL_DRU_MAX_CORE (4U) |
Maximum number of core submission set supported by the DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_CORE macro. More... | |
#define | CSL_DRU_NUM_CORE (3U) |
Number of core submission set supported by the DRU. More... | |
DRU Owner - Direct TR submission or UDMA-C TR submission | |
DRU owner. | |
#define | CSL_DRU_OWNER_DIRECT_TR ((uint64_t) 0x0000U) |
Direct TR - SUBMISSION registers must be written to submit TR. More... | |
#define | CSL_DRU_OWNER_UDMAC_TR ((uint64_t) 0x0001U) |
UDMA-C TR - TR will be received through PSIL. More... | |
DRU Queue ID | |
DRU queue ID. 0th queue is a priority queue. All others are round robin queues. | |
#define | CSL_DRU_QUEUE_ID_0 ((uint32_t) 0x0000U) |
#define | CSL_DRU_QUEUE_ID_1 ((uint32_t) 0x0001U) |
#define | CSL_DRU_QUEUE_ID_2 ((uint32_t) 0x0002U) |
#define | CSL_DRU_QUEUE_ID_3 ((uint32_t) 0x0003U) |
#define | CSL_DRU_QUEUE_ID_4 ((uint32_t) 0x0004U) |
#define | CSL_DRU_QUEUE_ID_5 ((uint32_t) 0x0005U) |
#define | CSL_DRU_QUEUE_ID_6 ((uint32_t) 0x0006U) |
#define | CSL_DRU_QUEUE_ID_7 ((uint32_t) 0x0007U) |
DRU Core ID | |
DRU core ID used to submit non-atomic TR submission. Note: There are only three core ID set present in the AM65xx and J721E SOC. | |
#define | CSL_DRU_CORE_ID_0 ((uint32_t) 0x0000U) |
#define | CSL_DRU_CORE_ID_1 ((uint32_t) 0x0001U) |
#define | CSL_DRU_CORE_ID_2 ((uint32_t) 0x0002U) |
#define | CSL_DRU_CORE_ID_3 ((uint32_t) 0x0003U) |
#define CSL_DRU_MAX_CH (512U) |
Maximum number of channels supported by DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_CH macro.
#define CSL_DRU_NUM_CH (64U) |
Number of channels supported by the DRU.
#define CSL_DRU_MAX_QUEUE (8U) |
Maximum number of queues supported by DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_QUEUE macro.
#define CSL_DRU_NUM_QUEUE (5U) |
Number of queues supported by the DRU.
#define CSL_DRU_MAX_CORE (4U) |
Maximum number of core submission set supported by the DRU. This is just the maximum registers supported for programming. The actual channel supported is given by CSL_DRU_NUM_CORE macro.
#define CSL_DRU_NUM_CORE (3U) |
Number of core submission set supported by the DRU.
#define CSL_DRU_OWNER_DIRECT_TR ((uint64_t) 0x0000U) |
Direct TR - SUBMISSION registers must be written to submit TR.
#define CSL_DRU_OWNER_UDMAC_TR ((uint64_t) 0x0001U) |
UDMA-C TR - TR will be received through PSIL.
#define CSL_DRU_QUEUE_ID_0 ((uint32_t) 0x0000U) |
#define CSL_DRU_QUEUE_ID_1 ((uint32_t) 0x0001U) |
#define CSL_DRU_QUEUE_ID_2 ((uint32_t) 0x0002U) |
#define CSL_DRU_QUEUE_ID_3 ((uint32_t) 0x0003U) |
#define CSL_DRU_QUEUE_ID_4 ((uint32_t) 0x0004U) |
#define CSL_DRU_QUEUE_ID_5 ((uint32_t) 0x0005U) |
#define CSL_DRU_QUEUE_ID_6 ((uint32_t) 0x0006U) |
#define CSL_DRU_QUEUE_ID_7 ((uint32_t) 0x0007U) |
#define CSL_DRU_CORE_ID_0 ((uint32_t) 0x0000U) |
#define CSL_DRU_CORE_ID_1 ((uint32_t) 0x0001U) |
#define CSL_DRU_CORE_ID_2 ((uint32_t) 0x0002U) |
#define CSL_DRU_CORE_ID_3 ((uint32_t) 0x0003U) |