![]() |
PDK API Guide for J721E
|
Files | |
file | csitx_ss.h |
This file contains the prototypes of the APIs present in the device abstraction layer file of CSI TX SS. This also contains some related macros. | |
Data Structures | |
struct | CSL_CsitxRevisionId |
Structure for accessing Revision ID and Core Release Info. of CSI Tx module. More... | |
struct | CSL_CsitxColorbarGenCfg |
Structure for Color-bar generation configurations. More... | |
struct | CSL_CsitxRetransCfg |
Structure for re-transmission streams configurations. More... | |
struct | CSL_CsitxStrmStatus |
Structure for streams status. More... | |
struct | CSL_CsitxDMAConfig |
Structure for PSI-L/DMA configuration for CSI Tx SS. More... | |
Functions | |
void | CSL_csitxGetRevisionId (const CSL_csi_tx_ifRegs *ifRegisters, CSL_CsitxRevisionId *revId) |
This API is used get the CSI Tx revision ID. More... | |
int32_t | CSL_csitxColorbarCfg (const CSL_csi_tx_ifRegs *ifRegisters, const CSL_CsitxColorbarGenCfg *cfg) |
This API is used program the color bar generation parameters. More... | |
void | CSL_csitxEnableColorbarGen (CSL_csi_tx_ifRegs *ifRegisters, uint32_t enable) |
This API is used enable/disable Color-bar generation. More... | |
int32_t | CSL_csitxRetransCfg (const CSL_csi_tx_ifRegs *ifRegisters, const CSL_CsitxRetransCfg *cfg) |
This API is used program the re-transmission streams parameters. More... | |
void | CSL_csitxAssertPixelIfReset (CSL_csi_tx_ifRegs *ifRegisters, uint32_t assert) |
This API is used assert/de-assert reset for pixel interface. More... | |
void | CSL_csitxGetStrmStatus (const CSL_csi_tx_ifRegs *ifRegisters, CSL_CsitxStrmStatus *status) |
This API is used get the current stream status. More... | |
int32_t | CSL_csitxFrmToFrmDelayCfg (const CSL_csi_tx_ifRegs *ifRegisters, const uint32_t vc, const uint32_t delay) |
This API is used program frame to frame delay. More... | |
int32_t | CSL_csitxConfigDMA (CSL_csi_tx_ifRegs *ifRegisters, const CSL_CsitxDMAConfig *cfg) |
This API is used to configure DMA/PSIL thread. More... | |
Macros | |
#define | CSL_CSITX_PSI_L_THREAD_NUM_MAX ((uint32_t)32U) |
Maximum number of PSI-L Threads supported by CSI Tx SS. More... | |
CSITX DMA Data Size Shift | |
#define | CSL_CSITX_DMA_DATA_SIZE_SHIFT_8BITS (0U) |
DMA Data Size Shift: 8 bits. More... | |
#define | CSL_CSITX_DMA_DATA_SIZE_SHIFT_16BITS (1U) |
DMA Data Size Shift: 16 bits. More... | |
#define | CSL_CSITX_DMA_DATA_SIZE_SHIFT_32BITS (2U) |
DMA Data Size Shift: 32 bits. More... | |
CSITX YUV422 Mode | |
#define | CSL_CSITX_YUV422_MODE_UYVY (0U) |
YUV422 Mode: UYVY. More... | |
#define | CSL_CSITX_YUV422_MODE_YUYV (2U) |
YUV422 Mode: VYUY. More... | |
#define | CSL_CSITX_YUV422_MODE_VYUY (1U) |
YUV422 Mode: YUYV. More... | |
#define | CSL_CSITX_YUV422_MODE_YVYU (3U) |
YUV422 Mode: YVYU. More... | |
#define CSL_CSITX_PSI_L_THREAD_NUM_MAX ((uint32_t)32U) |
Maximum number of PSI-L Threads supported by CSI Tx SS.
#define CSL_CSITX_DMA_DATA_SIZE_SHIFT_8BITS (0U) |
DMA Data Size Shift: 8 bits.
#define CSL_CSITX_DMA_DATA_SIZE_SHIFT_16BITS (1U) |
DMA Data Size Shift: 16 bits.
#define CSL_CSITX_DMA_DATA_SIZE_SHIFT_32BITS (2U) |
DMA Data Size Shift: 32 bits.
#define CSL_CSITX_YUV422_MODE_UYVY (0U) |
YUV422 Mode: UYVY.
#define CSL_CSITX_YUV422_MODE_YUYV (2U) |
YUV422 Mode: VYUY.
#define CSL_CSITX_YUV422_MODE_VYUY (1U) |
YUV422 Mode: YUYV.
#define CSL_CSITX_YUV422_MODE_YVYU (3U) |
YUV422 Mode: YVYU.
void CSL_csitxGetRevisionId | ( | const CSL_csi_tx_ifRegs * | ifRegisters, |
CSL_CsitxRevisionId * | revId | ||
) |
This API is used get the CSI Tx revision ID.
ifRegisters | Base Address of the CSI Tx SS Registers. |
revId | Contains Revision ID of CSI Tx module. Refer to CSL_CsitxRevisionId. |
int32_t CSL_csitxColorbarCfg | ( | const CSL_csi_tx_ifRegs * | ifRegisters, |
const CSL_CsitxColorbarGenCfg * | cfg | ||
) |
This API is used program the color bar generation parameters.
ifRegisters | Base Address of the CSI Tx SS Registers. |
cfg | Color-bar generation configurations. Refer to CSL_CsitxColorbarGenCfg. |
void CSL_csitxEnableColorbarGen | ( | CSL_csi_tx_ifRegs * | ifRegisters, |
uint32_t | enable | ||
) |
This API is used enable/disable Color-bar generation.
ifRegisters | Base Address of the CSI Tx SS Registers. |
enable | Color-bar generation is enabled if it is TRUE. Color-bar generation is disabled if it is FALSE. |
int32_t CSL_csitxRetransCfg | ( | const CSL_csi_tx_ifRegs * | ifRegisters, |
const CSL_CsitxRetransCfg * | cfg | ||
) |
This API is used program the re-transmission streams parameters.
ifRegisters | Base Address of the CSI Tx SS Registers. |
cfg | Re-transmission streams configurations. Refer to CSL_CsitxRetransCfg. |
void CSL_csitxAssertPixelIfReset | ( | CSL_csi_tx_ifRegs * | ifRegisters, |
uint32_t | assert | ||
) |
This API is used assert/de-assert reset for pixel interface.
ifRegisters | Base Address of the CSI Tx SS Registers. |
assert | Reset is asserted if it is TRUE. Reset is not asserted if it is FALSE. |
void CSL_csitxGetStrmStatus | ( | const CSL_csi_tx_ifRegs * | ifRegisters, |
CSL_CsitxStrmStatus * | status | ||
) |
This API is used get the current stream status.
ifRegisters | Base Address of the CSI Tx SS Registers. |
status | Stream status. Refer to CSL_CsitxStrmStatus. |
int32_t CSL_csitxFrmToFrmDelayCfg | ( | const CSL_csi_tx_ifRegs * | ifRegisters, |
const uint32_t | vc, | ||
const uint32_t | delay | ||
) |
This API is used program frame to frame delay.
ifRegisters | Base Address of the CSI Tx SS Registers. |
vc | Virtual channel number for which delay needs to configured. |
delay | Delay in number of main clock cyles from start of last frame line to start of next frame first line. |
int32_t CSL_csitxConfigDMA | ( | CSL_csi_tx_ifRegs * | ifRegisters, |
const CSL_CsitxDMAConfig * | cfg | ||
) |
This API is used to configure DMA/PSIL thread.
ifRegisters | Base Address of the CSI Tx SS Registers. |
cfg | Pointer to DMA/PSIL Configurations. Refer to CSL_CsitxDMAConfig |