![]() |
PDK API Guide for J721E
|
Functions | |
void | CSL_CPSW_SS_getVersionInfo (CSL_Xge_cpsw_ss_sRegs *hCpswSsRegs, CSL_CPSW_SS_VERSION *versionInfo) |
void | CSL_CPSW_SS_INTD_getVersionInfo (CSL_cpswRegs_INTD *hCpswIntDRegs, CSL_CPSW_SS_INTD_VERSION *versionInfo) |
Uint32 | CSL_CPSW_SS_INTD_getEOIVector (CSL_cpswRegs_INTD *hCpswIntDRegs) |
void | CSL_CPSW_SS_INTD_setEOIVector (CSL_cpswRegs_INTD *hCpswIntDRegs, Uint32 eoiVector) |
Uint32 | CSL_CPSW_SS_INTD_getEOIIntrVector (CSL_cpswRegs_INTD *hCpswIntDRegs) |
Uint32 | CSL_CPSW_SS_INTD_getIntrVectorOutPulse (CSL_cpswRegs_INTD *hCpswIntDRegs) |
void | CSL_CPSW_SS_INTD_setEnableIntrCPSWEventInterrupt (CSL_cpswRegs_INTD *hCpswIntDRegs, Uint32 enable) |
Uint32 | CSL_CPSW_SS_INTD_getEnableIntrCPSWEventInterrupt (CSL_cpswRegs_INTD *hCpswIntDRegs) |
void | CSL_CPSW_SS_INTD_setClearIntrCPSWEventInterrupt (CSL_cpswRegs_INTD *hCpswIntDRegs) |
void | CSL_CPSW_SS_INTD_getStatusIntr (CSL_cpswRegs_INTD *hCpswIntDRegs, CSL_CPSW_SS_INTD_INTRSTATUS *intrStatus) |
void | CSL_CPSW_SS_INTD_setEnableIntrMdioInterrupt (CSL_cpswRegs_INTD *hCpswIntDRegs, Uint32 enable) |
Uint32 | CSL_CPSW_SS_INTD_getEnableIntrMdioInterrupt (CSL_cpswRegs_INTD *hCpswIntDRegs) |
void | CSL_CPSW_SS_INTD_setClearIntrMdioInterrupt (CSL_cpswRegs_INTD *hCpswIntDRegs) |
void | CSL_CPSW_SS_INTD_setEnableIntrStatInterrupt (CSL_cpswRegs_INTD *hCpswIntDRegs, Uint32 enable) |
Uint32 | CSL_CPSW_SS_INTD_getEnableIntrStatInterrupt (CSL_cpswRegs_INTD *hCpswIntDRegs) |
void | CSL_CPSW_SS_INTD_setClearIntrStatInterrupt (CSL_cpswRegs_INTD *hCpswIntDRegs) |
void | CSL_CPSW_SS_setSGMIIMode (CSL_Xge_cpsw_ss_sRegs *hCpswSsRegs, Uint32 macPortNum, CSL_SGMII_MODE sgmiiModeId) |
void | CSL_CPSW_SS_getRGMIIStatus (CSL_Xge_cpsw_ss_sRegs *hCpswSsRegs, Uint32 macPortNum, CSL_CPSW_SS_RGMIISTATUS *pRgmiiStatus) |
Uint32 | CSL_CPSW_SS_getSerdesResetIsolation (CSL_Xge_cpsw_ss_sRegs *hCpswSsRegs) |
void | CSL_CPSW_SS_setSerdesResetIsolation (CSL_Xge_cpsw_ss_sRegs *hCpswSsRegs, Uint32 resetIso) |
Uint32 | CSL_CPSW_SS_getQSGMIIControlRdCd (CSL_Xge_cpsw_ss_sRegs *hCpswSsRegs, Uint32 qsgmiiId) |
void | CSL_CPSW_SS_setQSGMIIControlRdCd (CSL_Xge_cpsw_ss_sRegs *hCpswSsRegs, Uint32 qsgmiiId, Uint32 qsgmiiControlRdCd) |
Uint32 | CSL_CPSW_SS_getQSGMIIStatusRxSync (CSL_Xge_cpsw_ss_sRegs *hCpswSsRegs, Uint32 qsgmiiId) |
Uint32 | CSL_CPSW_SS_getXGMIILinkStatus (CSL_Xge_cpsw_ss_sRegs *hCpswSsRegs, Uint32 xgmiiId) |
Uint32 | CSL_CPSW_SS_getSGMIILinkStatus (CSL_Xge_cpsw_ss_sRegs *hCpswSsRegs, Uint32 sgmiiId) |
void CSL_CPSW_SS_getVersionInfo | ( | CSL_Xge_cpsw_ss_sRegs * | hCpswSsRegs, |
CSL_CPSW_SS_VERSION * | versionInfo | ||
) |
============================================================================
CSL_CPSW_SS_getVersionInfo
Description
This function retrieves the ethernet switch subsystem version information.
Arguments
versionInfo CSL_CPSW_SS_VERSION structure that needs to be populated with the version info read from the hardware. *
Return Value
None
Pre Condition
None
Post Condition
None
Reads
XGE_CPSW_SS_S_IDVER_REG_MINOR_VER, XGE_CPSW_SS_S_IDVER_REG_MAJOR_VER, XGE_CPSW_SS_S_IDVER_REG_RTL_VER, XGE_CPSW_SS_S_IDVER_REG_IDENT
Example
CSL_CPSW_SS_VERSION versionInfo; CSL_CPSW_SS_getVersionInfo (&versionInfo);
void CSL_CPSW_SS_INTD_getVersionInfo | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs, |
CSL_CPSW_SS_INTD_VERSION * | versionInfo | ||
) |
============================================================================
CSL_CPSW_SS_getIntdVersionInfo
Description
This function retrieves the CPSW_SS INTD information.
Arguments
versionInfo CSL_CPSW_SS_INTD_VERSION structure that needs to be populated with the version info read from the hardware. *
Return Value
None
Uint32 CSL_CPSW_SS_INTD_getEOIVector | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs | ) |
============================================================================
CSL_CPSW_SS_INTD_getEOIVector
Description
This function retrieves the CPSW_SS INTD EOI_VECTOR from EOI_REG The EOI Register allows the software to perform an end of interrupt handshake to interrupts with an IP that does not have an EOI register. The EOI handshake allows system interrupts to be re-evaluated for the associate logic with the EOI vector value (to allow multiple logic paths to re-evaluate individually without separate EOI registers). The EOI occurs the cycle after the register is written
Arguments
none *
Return Value
eoiVector
void CSL_CPSW_SS_INTD_setEOIVector | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs, |
Uint32 | eoiVector | ||
) |
============================================================================
CSL_CPSW_SS_INTD_setEOIVector
Description
This function set the CPSW_SS INTD EOI_VECTOR in EOI_REG The EOI Register allows the software to perform an end of interrupt handshake to interrupts with an IP that does not have an EOI register. The EOI handshake allows system interrupts to be re-evaluated for the associate logic with the EOI vector value (to allow multiple logic paths to re-evaluate individually without separate EOI registers). The EOI occurs the cycle after the register is written
Arguments
eoiVector EOI vector to be set *
Return Value
none
Uint32 CSL_CPSW_SS_INTD_getEOIIntrVector | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs | ) |
============================================================================
CSL_CPSW_SS_INTD_getEOIIntrVector
Description
This function retrieves the CPSW_SS INTD INTR_VECTOR from INTR_VECTOR_REG
The EOI Interrupt Vector Register captures the active and prioritized interrupts so that software may quickly read the values rather than check every bit in the IP Interrupt Source Register. The exact definition of this register is configuration dependent Arguments
none *
Return Value
intrVector EOI Interrupt Vector value. This has the latest prioritized interrupt values.
Uint32 CSL_CPSW_SS_INTD_getIntrVectorOutPulse | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs | ) |
============================================================================
CSL_CPSW_SS_INTD_getIntrVectorOutPulse
Description
This function get the CPSW_SS INTD INTR_VECTOR_REG_OUT_PULSE
Arguments
none *
Return Value
intrVectorOutPulse field from INTR_VECTOR_REG_OUT_PULSE The Interrupt Vector Registers captures the interrupt vector of active and prioritized interrupts for each host based in that hosts' enabled interrupts
void CSL_CPSW_SS_INTD_setEnableIntrCPSWEventInterrupt | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs, |
Uint32 | enable | ||
) |
============================================================================
CSL_CPSW_SS_INTD_setEnableIntrCPSWEventInterrupt
Description
This function enables/disables the CPSW event interrupt
Arguments
enable Flag to enable/disable *
Return Value
none
Uint32 CSL_CPSW_SS_INTD_getEnableIntrCPSWEventInterrupt | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs | ) |
============================================================================
CSL_CPSW_SS_INTD_getEnableIntrCPSWEventInterrupt
Description
This function returns flag indicating if the CPSW event interrupt is enabled
Arguments
none *
Return Value
Flag indicating if the interrupt is enabled or not
void CSL_CPSW_SS_INTD_setClearIntrCPSWEventInterrupt | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs | ) |
============================================================================
CSL_CPSW_SS_INTD_setClearIntrCPSWEventInterrupt
Description
This function clears the CPSW EVENT Interrupt status by writing to the ENABLE_CLR_REG_OUT_PULSE_0 register
Arguments
none *
Return Value
none
void CSL_CPSW_SS_INTD_getStatusIntr | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs, |
CSL_CPSW_SS_INTD_INTRSTATUS * | intrStatus | ||
) |
============================================================================
CSL_CPSW_SS_INTD_getStatusIntr
Description
This function returns CSL_CPSW_SS_INTD_INTRSTATUS populated with status of various CPSW interrupts
Arguments
intrStatus Interrupt status to be populated *
Return Value
none
void CSL_CPSW_SS_INTD_setEnableIntrMdioInterrupt | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs, |
Uint32 | enable | ||
) |
============================================================================
CSL_CPSW_SS_INTD_setEnableIntrMdioInterrupt
Description
This function enables/disables the MDIO interrupt
Arguments
enable Flag to enable/disable *
Return Value
none
Uint32 CSL_CPSW_SS_INTD_getEnableIntrMdioInterrupt | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs | ) |
============================================================================
CSL_CPSW_SS_INTD_getEnableIntrMdioInterrupt
Description
This function returns flag indicating if the MDIO interrupt is enabled
Arguments
none *
Return Value
Flag indicating if the interrupt is enabled or not
void CSL_CPSW_SS_INTD_setClearIntrMdioInterrupt | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs | ) |
============================================================================
CSL_CPSW_SS_INTD_setClearIntrMdioInterrupt
Description
This function clears the CPSW MDIO Interrupt status by writing to the ENABLE_CLR_REG_OUT_PULSE_0 register
Arguments
none *
Return Value
none
void CSL_CPSW_SS_INTD_setEnableIntrStatInterrupt | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs, |
Uint32 | enable | ||
) |
============================================================================
CSL_CPSW_SS_INTD_setEnableIntrStatInterrupt
Description
This function enables/disables the STAT interrupt
Arguments
enable Flag to enable/disable *
Return Value
none
Uint32 CSL_CPSW_SS_INTD_getEnableIntrStatInterrupt | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs | ) |
============================================================================
CSL_CPSW_SS_INTD_getEnableIntrStatInterrupt
Description
This function returns flag indicating if the STAT interrupt is enabled
Arguments
none *
Return Value
Flag indicating if the interrupt is enabled or not
void CSL_CPSW_SS_INTD_setClearIntrStatInterrupt | ( | CSL_cpswRegs_INTD * | hCpswIntDRegs | ) |
============================================================================
CSL_CPSW_SS_INTD_setClearIntrStatInterrupt
Description
This function clears the CPSW STAT Interrupt status by writing to the ENABLE_CLR_REG_OUT_PULSE_0 register
Arguments
none *
Return Value
none
void CSL_CPSW_SS_setSGMIIMode | ( | CSL_Xge_cpsw_ss_sRegs * | hCpswSsRegs, |
Uint32 | macPortNum, | ||
CSL_SGMII_MODE | sgmiiModeId | ||
) |
============================================================================
CSL_CPSW_SS_setSGMIIMode
Description
This function sets the SGMII mode (fiber or copper) for the given macPort
Arguments
macPortNum Mac Port for which SGMII mode is set sgmiiModeId CSL_SGMII_MODE value *
Return Value
none
void CSL_CPSW_SS_getRGMIIStatus | ( | CSL_Xge_cpsw_ss_sRegs * | hCpswSsRegs, |
Uint32 | macPortNum, | ||
CSL_CPSW_SS_RGMIISTATUS * | pRgmiiStatus | ||
) |
============================================================================
CSL_CPSW_SS_getRGMIIStatus
Description
This function returns the RGMII status for the given macPort
Arguments
macPortNum Mac Port for which RGMII status is queried pRgmiiStatus RGMII status to be populated *
Return Value
none
Uint32 CSL_CPSW_SS_getSerdesResetIsolation | ( | CSL_Xge_cpsw_ss_sRegs * | hCpswSsRegs | ) |
============================================================================
CSL_CPSW_SS_getSerdesResetIsolation
Description
This function returns the Serdes reset isolation configuration
Arguments
none *
Return Value
Serdes Reset isolation value
void CSL_CPSW_SS_setSerdesResetIsolation | ( | CSL_Xge_cpsw_ss_sRegs * | hCpswSsRegs, |
Uint32 | resetIso | ||
) |
============================================================================
CSL_CPSW_SS_setSerdesResetIsolation
Description
This function sets the serdes reset isolation configuration
Arguments
resetIso Reset isolation configuration to be set *
Return Value
none
Uint32 CSL_CPSW_SS_getQSGMIIControlRdCd | ( | CSL_Xge_cpsw_ss_sRegs * | hCpswSsRegs, |
Uint32 | qsgmiiId | ||
) |
============================================================================
CSL_CPSW_SS_getQSGMIIControlRdCd
Description
This function returns the QSGMII control register for the given qsgmii
Arguments
qsgmiiId QSGMII (0/1) for which the QSGMII control register is queried *
Return Value
QSGMII control configuration for the given QSGMII id
void CSL_CPSW_SS_setQSGMIIControlRdCd | ( | CSL_Xge_cpsw_ss_sRegs * | hCpswSsRegs, |
Uint32 | qsgmiiId, | ||
Uint32 | qsgmiiControlRdCd | ||
) |
============================================================================
CSL_CPSW_SS_setQSGMIIControlRdCd
Description
This function sets the QSGMII control register for the given qsgmii
Arguments
qsgmiiId QSGMII (0/1) for which the QSGMII control register is set qsgmiiControlRdCd QSMII control configuration *
Return Value
QSGMII control configuration for the given QSGMII id
Uint32 CSL_CPSW_SS_getQSGMIIStatusRxSync | ( | CSL_Xge_cpsw_ss_sRegs * | hCpswSsRegs, |
Uint32 | qsgmiiId | ||
) |
============================================================================
CSL_CPSW_SS_getQSGMIIStatusRxSync
Description
This function returns the QSGMII status register for the given qsgmii
Arguments
qsgmiiId QSGMII (0/1) for which the QSGMII status register is queried *
Return Value
QSGMII status for the given QSGMII id
Uint32 CSL_CPSW_SS_getXGMIILinkStatus | ( | CSL_Xge_cpsw_ss_sRegs * | hCpswSsRegs, |
Uint32 | xgmiiId | ||
) |
============================================================================
CSL_CPSW_SS_getXGMIILinkStatus
Description
This function returns the XGMII link status register for the given xgmii
Arguments
xgmiiid XGMII (0/1) for which the XGMII status register is queried *
Return Value
XGMII status for the given XGMII id
Uint32 CSL_CPSW_SS_getSGMIILinkStatus | ( | CSL_Xge_cpsw_ss_sRegs * | hCpswSsRegs, |
Uint32 | sgmiiId | ||
) |
============================================================================
CSL_CPSW_SS_getSGMIILinkStatus
Description
This function returns the SGMII link status register for the given sgmii
Arguments
qsgmiiId QSGMII (0/1) for which the QSGMII status register is queried *
Return Value
SGMII link status for the given SGMII id