![]() |
PDK API Guide for J721E
|
This file contains the type definitions and helper macros for the Enet software queue.
Go to the source code of this file.
Data Structures | |
struct | EnetQ_Node |
A generic node structure for a single link list. More... | |
struct | EnetQ |
Generic queue. More... | |
Functions | |
void | EnetQueue_initQ (EnetQ *queue) |
Init queue. More... | |
void | EnetQueue_copyQ (EnetQ *dstQueue, const EnetQ *srcQueue) |
Copy queues. More... | |
void | EnetQueue_enq (EnetQ *queue, EnetQ_Node *node) |
Enqueue a packet into the queue. More... | |
void | EnetQueue_enqHead (EnetQ *queue, EnetQ_Node *node) |
Enqueue a packet at head into the queue. More... | |
EnetQ_Node * | EnetQueue_deq (EnetQ *queue) |
Dequeue a packet from the queue. More... | |
void | EnetQueue_append (EnetQ *dstQueue, EnetQ *srcQueue) |
Append queue. More... | |
uint32_t | EnetQueue_getQCount (EnetQ *queue) |
Get queue count. More... | |
void | EnetQueue_verifyQCount (EnetQ *queue) |
Checks queue corruption. More... | |