PDK API Guide for J721E
|
This file contains the type definitions and helper macros for the Ethernet PHY interface.
Go to the source code of this file.
Data Structures | |
struct | EnetPhy_GenericInArgs |
Generic input args. More... | |
struct | EnetPhy_ReadRegInArgs |
Input args for ENET_PHY_IOCTL_READ_EXT_REG command. More... | |
struct | EnetPhy_WriteRegInArgs |
Input args for ENET_PHY_IOCTL_WRITE_EXT_REG command. More... | |
struct | EnetPhy_C45ReadRegInArgs |
Input args for ENET_PHY_IOCTL_C45_READ_REG command. More... | |
struct | EnetPhy_C45WriteRegInArgs |
Input args for ENET_PHY_IOCTL_C45_WRITE_REG command. More... | |
Macros | |
#define | ENET_PHY_PUBLIC_IOCTL(x) |
Helper macro to create PHY IOCTL commands. More... | |
Enumerations | |
enum | EnetPhy_Ioctl_e { ENET_PHY_IOCTL_GET_ID = ENET_PHY_PUBLIC_IOCTL(0U), ENET_PHY_IOCTL_GET_SUPPORTED_MODES = ENET_PHY_PUBLIC_IOCTL(1U), ENET_PHY_IOCTL_GET_LOOPBACK_STATE = ENET_PHY_PUBLIC_IOCTL(2U), ENET_PHY_IOCTL_IS_ALIVE = ENET_PHY_PUBLIC_IOCTL(3U), ENET_PHY_IOCTL_IS_LINKED = ENET_PHY_PUBLIC_IOCTL(4U), ENET_PHY_IOCTL_GET_LINK_MODE = ENET_PHY_PUBLIC_IOCTL(5U), ENET_PHY_IOCTL_RESET = ENET_PHY_PUBLIC_IOCTL(6U), ENET_PHY_IOCTL_READ_REG = ENET_PHY_PUBLIC_IOCTL(7U), ENET_PHY_IOCTL_WRITE_REG = ENET_PHY_PUBLIC_IOCTL(8U), ENET_PHY_IOCTL_READ_EXT_REG = ENET_PHY_PUBLIC_IOCTL(9U), ENET_PHY_IOCTL_WRITE_EXT_REG = ENET_PHY_PUBLIC_IOCTL(10U), ENET_PHY_IOCTL_C45_READ_REG = ENET_PHY_PUBLIC_IOCTL(11U), ENET_PHY_IOCTL_C45_WRITE_REG = ENET_PHY_PUBLIC_IOCTL(12U), ENET_PHY_IOCTL_PRINT_REGS = ENET_PHY_PUBLIC_IOCTL(13U) } |
PHY IOCTL commands. More... | |
#define ENET_PHY_PUBLIC_IOCTL | ( | x | ) |
Helper macro to create PHY IOCTL commands.
enum EnetPhy_Ioctl_e |
PHY IOCTL commands.
Enumerator | |
---|---|
ENET_PHY_IOCTL_GET_ID | Get PHY identification. IOCTL parameters:
|
ENET_PHY_IOCTL_GET_SUPPORTED_MODES | Get PHY supported modes by local PHY device. IOCTL parameters:
|
ENET_PHY_IOCTL_GET_LOOPBACK_STATE | Check if PHY is in loopback or not. IOCTL parameters:
|
ENET_PHY_IOCTL_IS_ALIVE | Check PHY alive status. IOCTL parameters:
|
ENET_PHY_IOCTL_IS_LINKED | Check state-machine link state, that is, whether the state machine has reached the LINKED state. IOCTL parameters:
|
ENET_PHY_IOCTL_GET_LINK_MODE | Get the link speed and duplexity state after the state machine has reached the LINKED state. IOCTL parameters:
|
ENET_PHY_IOCTL_RESET | Reset PHY. IOCTL parameters:
|
ENET_PHY_IOCTL_READ_REG | Read PHY register. IOCTL parameters:
|
ENET_PHY_IOCTL_WRITE_REG | Write PHY register. IOCTL parameters:
|
ENET_PHY_IOCTL_READ_EXT_REG | Read PHY extended register. IOCTL parameters:
|
ENET_PHY_IOCTL_WRITE_EXT_REG | Write PHY extended register. IOCTL parameters:
|
ENET_PHY_IOCTL_C45_READ_REG | Read PHY register using Clause-45 frame. IOCTL parameters:
|
ENET_PHY_IOCTL_C45_WRITE_REG | Write PHY register using Clause-45 frame. IOCTL parameters:
|
ENET_PHY_IOCTL_PRINT_REGS | Print PHY registers. IOCTL parameters:
|