![]() |
PDK API Guide for J721E
|
CSITX event related parameters and API.
Go to the source code of this file.
Data Structures | |
struct | Csitx_EventPrms |
CSITX event related parameters. More... | |
struct | Csitx_EventStatus |
CSITX event status parameters. Instance of this structure will passed to the application call-back. More... | |
Typedefs | |
typedef void(* | CsitxDrv_EventCallback) (Csitx_EventStatus eventStatus, void *appData) |
CSITX event callback function. More... | |
Functions | |
void | Csitx_eventPrmsInit (Csitx_EventPrms *eventPrms) |
Csitx_EventPrms structure init function. More... | |