![]() |
PDK API Guide for J721E
|
CSIRX event related parameters and API.
Go to the source code of this file.
Data Structures | |
struct | Csirx_EventPrms |
CSIRX event related parameters. More... | |
struct | Csirx_EventStatus |
CSIRX event status parameters. Instance of this structure will passed to the application call-back. More... | |
struct | CsirxDrv_EventObj |
CSIRX event object. More... | |
Typedefs | |
typedef void(* | CsirxDrv_EventCallback) (Csirx_EventStatus eventStatus, void *appData) |
CSIRX event callback function. More... | |
Functions | |
void | Csirx_eventPrmsInit (Csirx_EventPrms *eventPrms) |
Csirx_EventPrms structure init function. More... | |
int32_t | CsirxDrv_eventGroupRegister (Fdrv_Handle drvHandle, Csirx_EventPrms *eventPrms) |
CSIRX event group registration. More... | |
int32_t | CsirxDrv_eventGroupUnRegister (Fdrv_Handle drvHandle, uint32_t eventGroup) |
CSIRX unregister group event. More... | |
int32_t | CsirxDrv_eventEnable (Fdrv_Handle drvHandle, uint32_t eventGroup, uint32_t eventType) |
Enable the event in event group. More... | |
int32_t | CsirxDrv_eventDisable (Fdrv_Handle drvHandle, uint32_t eventGroup, uint32_t eventType) |
Disable the event in event group. More... | |