![]() |
PDK API Guide for J721E
|
Semaphore module for the RTOS Porting Interface.
============================================================================
Semaphores can be counting semaphores or binary semaphores. Counting semaphores keep track of the number of times the semaphore has been posted with post functions. This is useful, for example, if you have a group of resources that are shared between tasks. Such tasks might call pend() to see if a resource is available before using one. A count of zero for a counting semaphore denotes that it is not available. A positive count denotes how many times a SemaphoreP_pend can be called before it is blocked (or returns SemaphoreP_TIMEOUT).
Binary semaphores can have only two states: available (count = 1) and unavailable (count = 0). They can be used to share a single resource between tasks. They can also be used for a basic signalling mechanism, where the semaphore can be posted multiple times. Binary semaphores do not keep track of the count; they simply track whether the semaphore has been posted or not.
Go to the source code of this file.
Semaphore status code | |
#define | SemaphoreP_OK (0) |
#define | SemaphoreP_FAILURE (-(int32_t)1) |
#define | SemaphoreP_TIMEOUT (-(int32_t)2) |
#define | SemaphoreP_UNSUPPORTED (-(int32_t)3) |
typedef int32_t | SemaphoreP_Status |
Status codes for SemaphoreP APIs. More... | |
Mode of Semaphore | |
#define | SemaphoreP_Mode_COUNTING (0x0U) |
#define | SemaphoreP_Mode_BINARY (0x1U) |
typedef uint32_t | SemaphoreP_Mode |
Mode of the semaphore. More... | |
Data Structures | |
struct | SemaphoreP_Params |
Basic SemaphoreP Parameters. More... | |
Macros | |
#define | SemaphoreP_WAIT_FOREVER (~((uint32_t)0U)) |
Wait forever define. More... | |
#define | SemaphoreP_NO_WAIT ((uint32_t)0U) |
No wait define. More... | |
Typedefs | |
typedef void * | SemaphoreP_Handle |
Opaque client reference to an instance of a SemaphoreP. More... | |
Functions | |
SemaphoreP_Handle | SemaphoreP_create (uint32_t count, const SemaphoreP_Params *semParams) |
Function to create a semaphore. More... | |
SemaphoreP_Status | SemaphoreP_delete (SemaphoreP_Handle semPhandle) |
Function to delete a semaphore. More... | |
void | SemaphoreP_Params_init (SemaphoreP_Params *semParams) |
Initialize params structure to default values. More... | |
SemaphoreP_Status | SemaphoreP_pend (SemaphoreP_Handle semPhandle, uint32_t timeout) |
Function to pend (wait) on a semaphore. More... | |
SemaphoreP_Status | SemaphoreP_post (SemaphoreP_Handle semPhandle) |
Function to post (signal) a semaphore. More... | |
SemaphoreP_Status | SemaphoreP_postFromClock (SemaphoreP_Handle semPhandle) |
Function to post (signal) a semaphore from an ClockP function. More... | |
SemaphoreP_Status | SemaphoreP_postFromISR (SemaphoreP_Handle semPhandle) |
Function to post (signal) a semaphore from an ISR. More... | |
int32_t | SemaphoreP_getCount (SemaphoreP_Handle semPhandle) |
Function to return the count of a semaphore. More... | |
SemaphoreP_Status | SemaphoreP_reset (SemaphoreP_Handle semPhandle) |
Function to clear a semaphore for resuse. More... | |