Vision Apps User Guide
Font and 2D Drawing API

Introduction

This module has the interface for drawing fonts and 2D primitives like lines.

NOTE: This is limited demo API and not a comprehensive 2D drawing library

Files

file  draw2d.h
 Font and 2D Drawing API.
 

Data Structures

struct  Draw2D_FontProperty
 
struct  Draw2D_BmpProperty
 
struct  Draw2D_BufInfo
 Buffer information into which font and 2d primitives will be draw. More...
 
struct  Draw2D_FontPrm
 Font parameters. More...
 
struct  Draw2D_BmpPrm
 Bitmap parameters. More...
 
struct  Draw2D_LinePrm
 Line draw parameters. More...
 
struct  Draw2D_RegionPrm
 Region Params. More...
 

Functions

int32_t Draw2D_create (Draw2D_Handle *pCtx)
 Create a context for drawing. More...
 
int32_t Draw2D_delete (Draw2D_Handle pCtx)
 Delete a previously created drawing context. More...
 
int32_t Draw2D_setBufInfo (Draw2D_Handle pCtx, Draw2D_BufInfo *pBufInfo)
 Associated a drawing buffer with a drawing context. More...
 
void Draw2D_updateBufAddr (Draw2D_Handle pCtx, uint8_t **bufAddr)
 Update drawing buffer. More...
 
int32_t Draw2D_clearBuf (Draw2D_Handle pCtx)
 Fill buffer with transperency color. More...
 
int32_t Draw2D_drawString (Draw2D_Handle pCtx, uint32_t startX, uint32_t startY, char *str, Draw2D_FontPrm *pPrm)
 Draw string of character into the drawing buffer. More...
 
int32_t Draw2D_drawString_rot (Draw2D_Handle pCtx, uint32_t startX, uint32_t startY, char *str, Draw2D_FontPrm *pPrm, uint32_t rotate)
 Draw string of character into the drawing buffer. More...
 
int32_t Draw2D_clearString (Draw2D_Handle pCtx, uint32_t startX, uint32_t startY, uint32_t stringLength, Draw2D_FontPrm *pPrm)
 Clear a area equal to stringLength in the drawing buffer. More...
 
int32_t Draw2D_getFontProperty (Draw2D_FontPrm *pPrm, Draw2D_FontProperty *pProp)
 Get properties of a given font. More...
 
int32_t Draw2D_getBmpProperty (Draw2D_BmpPrm *pPrm, Draw2D_BmpProperty *pProp)
 Get properties of a given bitmap. More...
 
int32_t Draw2D_drawLine (Draw2D_Handle pCtx, uint32_t startX, uint32_t startY, uint32_t endX, uint32_t endY, Draw2D_LinePrm *pPrm)
 Draw a line in the drawing buffer. More...
 
int32_t Draw2D_drawRect (Draw2D_Handle pCtx, uint32_t startX, uint32_t startY, uint32_t width, uint32_t height, Draw2D_LinePrm *pPrm)
 Draw a rectangle in the drawing buffer. More...
 
int32_t Draw2D_clearRegion (Draw2D_Handle pCtx, uint32_t startX, uint32_t startY, uint32_t width, uint32_t height)
 Clear a region in the drawing buffer with transperency color. More...
 
int32_t Draw2D_fillRegion (Draw2D_Handle pCtx, Draw2D_RegionPrm *prm)
 Draw a region in the drawing buffer with custom color. More...
 
void Draw2D_drawPixel (Draw2D_Handle pCtx, uint32_t px, uint32_t py, uint32_t color, uint32_t colorFormat)
 Draw pixel of a given color. More...
 
int32_t Draw2D_drawBmp (Draw2D_Handle pCtx, uint32_t startX, uint32_t startY, Draw2D_BmpPrm *pPrm)
 Draw a bitmap into the drawing buffer. More...
 
int32_t Draw2D_drawBmp_rot (Draw2D_Handle pCtx, uint32_t startX, uint32_t startY, Draw2D_BmpPrm *pPrm, uint32_t rotate)
 Draw a bitmap into the drawing buffer. More...
 
int32_t Draw2D_insertBmp (Draw2D_Handle pCtx, char *input_file, int32_t startX, int32_t startY)
 Draw a bitmap from BMP file at a specified display buffer location. More...
 
int32_t Draw2D_insertBmpFromMemory (Draw2D_Handle pCtx, void *buf, uint32_t buf_size, int32_t startX, int32_t startY)
 Draw a bitmap from BMP file (pre-copied at a memory location) at a specified display buffer location. More...
 
void Draw2D_setFontColor (uint16_t colorText, uint16_t colorBorder, uint16_t colorBg)
 Sets a global color to use for fonts in RGB565 format. More...
 
void Draw2D_resetFontColor ()
 Restore font to default. More...
 
static uint32_t Draw2D_floor (uint32_t val, uint32_t align)
 Initialize In queue parameters of a link. More...
 

Typedefs

typedef void * Draw2D_Handle
 Draw 2D object handle. More...
 

Enumerations

enum  Draw2D_DataFormat {
  DRAW2D_DF_YUV422I_UYVY = 0x0000,
  DRAW2D_DF_YUV422I_YUYV,
  DRAW2D_DF_YUV422I_YVYU,
  DRAW2D_DF_YUV422I_VYUY,
  DRAW2D_DF_YUV422SP_UV,
  DRAW2D_DF_YUV422SP_VU,
  DRAW2D_DF_YUV422P,
  DRAW2D_DF_YUV420SP_UV,
  DRAW2D_DF_YUV420SP_VU,
  DRAW2D_DF_YUV420P,
  DRAW2D_DF_YUV444P,
  DRAW2D_DF_YUV444I,
  DRAW2D_DF_RGB16_565,
  DRAW2D_DF_BGRA16_4444,
  DRAW2D_DF_RGB24_888,
  DRAW2D_DF_ARGB32_8888,
  DRAW2D_DF_RGBA32_8888,
  DRAW2D_DF_BGR16_565,
  DRAW2D_DF_BGR24_888,
  DRAW2D_DF_ABGR32_8888,
  DRAW2D_DF_BGRA32_8888,
  DRAW2D_DF_MISC,
  DRAW2D_DF_INVALID,
  DRAW2D_DF_FORCE32BITS = 0xFFFFFFFF
}
 Enums for data format. More...
 

Macros

#define DRAW2D_MAX_PLANES   (3)
 
#define RGB888_TO_RGB565(r, g, b)   ((((uint32_t)(r>>3) & 0x1F) << 11) | (((uint32_t)(g>>2) & 0x3F) << 5) | (((uint32_t)(b>>3) & 0x1F)))
 Macro that converts RGB888 to RGB565. More...
 
#define RGB888_TO_BGRA444(r, g, b, a)   ((((uint32_t)(r>>4) & 0xF) << 0) | (((uint32_t)(g>>4) & 0xF) << 4) | (((uint32_t)(b>>4) & 0xF)<<8)| (((uint32_t)(a>>4) & 0xF)<<12))
 
#define DRAW2D_TRANSPARENT_COLOR   (RGB888_TO_RGB565(0, 0, 0))
 
#define DRAW2D_TRANSPARENT_COLOR_FORMAT   (DRAW2D_DF_BGR16_565)
 
#define DRAW2D_BMP_IDX_TI_LOGO_0   (0)
 
#define DRAW2D_BMP_IDX_TI_LOGO_1   (1)
 
#define DRAW2D_BMP_IDX_TI_LOGO_2   (2)
 
#define DRAW2D_BMP_IDX_TI_LOGO_3   (3)
 
#define DRAW2D_BMP_IDX_TI_LOGO_4   (4)
 
#define DRAW2D_BMP_IDX_TI_LOGO_5   (5)
 
#define DRAW2D_BMP_IDX_DOF_COLOUR_MAP   (6)
 
#define DRAW2D_BMP_IDX_SDE_COLOUR_MAP   (7)
 

Macro Definition Documentation

◆ DRAW2D_MAX_PLANES

#define DRAW2D_MAX_PLANES   (3)

◆ RGB888_TO_RGB565

#define RGB888_TO_RGB565 (   r,
  g,
 
)    ((((uint32_t)(r>>3) & 0x1F) << 11) | (((uint32_t)(g>>2) & 0x3F) << 5) | (((uint32_t)(b>>3) & 0x1F)))

Macro that converts RGB888 to RGB565.

◆ RGB888_TO_BGRA444

#define RGB888_TO_BGRA444 (   r,
  g,
  b,
 
)    ((((uint32_t)(r>>4) & 0xF) << 0) | (((uint32_t)(g>>4) & 0xF) << 4) | (((uint32_t)(b>>4) & 0xF)<<8)| (((uint32_t)(a>>4) & 0xF)<<12))

◆ DRAW2D_TRANSPARENT_COLOR

#define DRAW2D_TRANSPARENT_COLOR   (RGB888_TO_RGB565(0, 0, 0))

◆ DRAW2D_TRANSPARENT_COLOR_FORMAT

#define DRAW2D_TRANSPARENT_COLOR_FORMAT   (DRAW2D_DF_BGR16_565)

◆ DRAW2D_BMP_IDX_TI_LOGO_0

#define DRAW2D_BMP_IDX_TI_LOGO_0   (0)

◆ DRAW2D_BMP_IDX_TI_LOGO_1

#define DRAW2D_BMP_IDX_TI_LOGO_1   (1)

◆ DRAW2D_BMP_IDX_TI_LOGO_2

#define DRAW2D_BMP_IDX_TI_LOGO_2   (2)

◆ DRAW2D_BMP_IDX_TI_LOGO_3

#define DRAW2D_BMP_IDX_TI_LOGO_3   (3)

◆ DRAW2D_BMP_IDX_TI_LOGO_4

#define DRAW2D_BMP_IDX_TI_LOGO_4   (4)

◆ DRAW2D_BMP_IDX_TI_LOGO_5

#define DRAW2D_BMP_IDX_TI_LOGO_5   (5)

◆ DRAW2D_BMP_IDX_DOF_COLOUR_MAP

#define DRAW2D_BMP_IDX_DOF_COLOUR_MAP   (6)

◆ DRAW2D_BMP_IDX_SDE_COLOUR_MAP

#define DRAW2D_BMP_IDX_SDE_COLOUR_MAP   (7)

Typedef Documentation

◆ Draw2D_Handle

typedef void* Draw2D_Handle

Draw 2D object handle.

Enumeration Type Documentation

◆ Draw2D_DataFormat

Enums for data format.

All data formats may not be supported by all links. For supported data formats please look link header file.

Enumerator
DRAW2D_DF_YUV422I_UYVY 

YUV 422 Interleaved format - UYVY.

DRAW2D_DF_YUV422I_YUYV 

YUV 422 Interleaved format - YUYV.

DRAW2D_DF_YUV422I_YVYU 

YUV 422 Interleaved format - YVYU.

DRAW2D_DF_YUV422I_VYUY 

YUV 422 Interleaved format - VYUY.

DRAW2D_DF_YUV422SP_UV 

YUV 422 Semi-Planar - Y separate, UV interleaved.

DRAW2D_DF_YUV422SP_VU 

YUV 422 Semi-Planar - Y separate, VU interleaved.

DRAW2D_DF_YUV422P 

YUV 422 Planar - Y, U and V separate.

DRAW2D_DF_YUV420SP_UV 

YUV 420 Semi-Planar - Y separate, UV interleaved.

DRAW2D_DF_YUV420SP_VU 

YUV 420 Semi-Planar - Y separate, VU interleaved.

DRAW2D_DF_YUV420P 

YUV 420 Planar - Y, U and V separate.

DRAW2D_DF_YUV444P 

YUV 444 Planar - Y, U and V separate.

DRAW2D_DF_YUV444I 

YUV 444 interleaved - YUVYUV...

DRAW2D_DF_RGB16_565 

RGB565 16-bit - 5-bits R, 6-bits G, 5-bits B.

DRAW2D_DF_BGRA16_4444 

BGRA 16-bit - 4-bits R, 4-bits G, 4-bits B, 4-bits Alpha (LSB).

DRAW2D_DF_RGB24_888 

RGB24 24-bit - 8-bits R, 8-bits G, 8-bits B.

DRAW2D_DF_ARGB32_8888 

ARGB32 32-bit - 8-bits R, 8-bits G, 8-bits B, 8-bit Alpha (MSB).

DRAW2D_DF_RGBA32_8888 

RGBA32 32-bit - 8-bits R, 8-bits G, 8-bits B, 8-bit Alpha (LSB).

DRAW2D_DF_BGR16_565 

BGR565 16-bit - 5-bits B, 6-bits G, 5-bits R.

DRAW2D_DF_BGR24_888 

BGR888 24-bit - 8-bits B, 8-bits G, 8-bits R.

DRAW2D_DF_ABGR32_8888 

ABGR8888 32-bit - 8-bits B, 8-bits G, 8-bits R, 8-bit Alpha (MSB).

DRAW2D_DF_BGRA32_8888 

BGRA8888 32-bit - 8-bits B, 8-bits G, 8-bits R, 8-bit Alpha (LSB).

DRAW2D_DF_MISC 

For future purpose.

DRAW2D_DF_INVALID 

Invalid data format. Could be used to initialize variables.

DRAW2D_DF_FORCE32BITS 

This should be the last value after the max enumeration value. This is to make sure enum size defaults to 32 bits always regardless of compiler.

Function Documentation

◆ Draw2D_create()

int32_t Draw2D_create ( Draw2D_Handle pCtx)

Create a context for drawing.

   MUST be called before calling any other Draw2D API
Parameters
pCtx[OUT] Created Draw 2D context
Returns
VX_SUCCESS on success

◆ Draw2D_delete()

int32_t Draw2D_delete ( Draw2D_Handle  pCtx)

Delete a previously created drawing context.

Parameters
pCtx[IN] Draw 2D context
Returns
VX_SUCCESS on success

◆ Draw2D_setBufInfo()

int32_t Draw2D_setBufInfo ( Draw2D_Handle  pCtx,
Draw2D_BufInfo pBufInfo 
)

Associated a drawing buffer with a drawing context.

   This API MUST be called after Draw2D_create() and before any drawing
   API
Parameters
pCtx[IN] Draw 2D context
pBufInfo[IN] Buffer information
Returns
VX_SUCCESS on success

◆ Draw2D_updateBufAddr()

void Draw2D_updateBufAddr ( Draw2D_Handle  pCtx,
uint8_t **  bufAddr 
)

Update drawing buffer.

   This API can be used to update the buffer address when needed
Parameters
pCtx[IN] Draw 2D context
bufAddr[IN] Array of buffer addresses
Returns
VX_SUCCESS on success

◆ Draw2D_clearBuf()

int32_t Draw2D_clearBuf ( Draw2D_Handle  pCtx)

Fill buffer with transperency color.

Parameters
pCtx[IN] Draw 2D context
Returns
VX_SUCCESS on success

◆ Draw2D_drawString()

int32_t Draw2D_drawString ( Draw2D_Handle  pCtx,
uint32_t  startX,
uint32_t  startY,
char *  str,
Draw2D_FontPrm pPrm 
)

Draw string of character into the drawing buffer.

Parameters
pCtx[IN] Draw 2D context
startX[IN] X-position in the buffer
startY[IN] Y-position in the buffer
str[IN] Ascii string to draw
pPrm[IN] Font to use when drawing, when set to NULL default properties used
Returns
VX_SUCCESS on success

◆ Draw2D_drawString_rot()

int32_t Draw2D_drawString_rot ( Draw2D_Handle  pCtx,
uint32_t  startX,
uint32_t  startY,
char *  str,
Draw2D_FontPrm pPrm,
uint32_t  rotate 
)

Draw string of character into the drawing buffer.

Parameters
pCtx[IN] Draw 2D context
startX[IN] X-position in the buffer
startY[IN] Y-position in the buffer
str[IN] Ascii string to draw
pPrm[IN] Font to use when drawing, when set to NULL default properties used
rotate[IN] Set 1 to rotate
Returns
VX_SUCCESS on success

◆ Draw2D_clearString()

int32_t Draw2D_clearString ( Draw2D_Handle  pCtx,
uint32_t  startX,
uint32_t  startY,
uint32_t  stringLength,
Draw2D_FontPrm pPrm 
)

Clear a area equal to stringLength in the drawing buffer.

   This is used to erase a string of previously written characters.
   Internal this draws the 'SPACE' stringLength times
Parameters
pCtx[IN] Draw 2D context
startX[IN] start X-position in the buffer
startY[IN] start Y-position in the buffer
stringLength[IN] Length of string to clear
pPrm[IN] Font to use when drawing, when set to NULL default properties used
Returns
VX_SUCCESS on success

◆ Draw2D_getFontProperty()

int32_t Draw2D_getFontProperty ( Draw2D_FontPrm pPrm,
Draw2D_FontProperty pProp 
)

Get properties of a given font.

Parameters
pPrm[IN] Font to use when drawing, when set to NULL default properties used
pProp[OUT] Font properties like width x height, bpp etc
Returns
VX_SUCCESS on success

◆ Draw2D_getBmpProperty()

int32_t Draw2D_getBmpProperty ( Draw2D_BmpPrm pPrm,
Draw2D_BmpProperty pProp 
)

Get properties of a given bitmap.

Parameters
pPrm[IN] Bitmap to use when drawing, when set to NULL default properties used
pProp[OUT] Bitmap properties like width x height, bpp etc
Returns
VX_SUCCESS on success

◆ Draw2D_drawLine()

int32_t Draw2D_drawLine ( Draw2D_Handle  pCtx,
uint32_t  startX,
uint32_t  startY,
uint32_t  endX,
uint32_t  endY,
Draw2D_LinePrm pPrm 
)

Draw a line in the drawing buffer.

   Currently only horizontal or vertical lines can be drawn
   So make sure endX or endY  is equal to startX or startY

   To clear a line, call the same API with color as transperency
   color in line properties
Parameters
pCtx[IN] Draw 2D context
startX[IN] start X-position in the buffer
startY[IN] start Y-position in the buffer
endX[IN] end X-position in the buffer
endY[IN] end Y-position in the buffer
pPrm[IN] Line properties to use when drawing, when set to NULL default properties used
Returns
VX_SUCCESS on success

◆ Draw2D_drawRect()

int32_t Draw2D_drawRect ( Draw2D_Handle  pCtx,
uint32_t  startX,
uint32_t  startY,
uint32_t  width,
uint32_t  height,
Draw2D_LinePrm pPrm 
)

Draw a rectangle in the drawing buffer.

   Internally uses Draw2D_drawLine() 4 times to draw the rectangle

   To clear a rectangle, call the same API with color as transperency
   color in line properties
Parameters
pCtx[IN] Draw 2D context
startX[IN] start X-position in the buffer
startY[IN] start Y-position in the buffer
width[IN] width of rectangle in pixels
height[IN] height of rectangle in lines
pPrm[IN] Line properties to use when drawing, when set to NULL default properties used
Returns
VX_SUCCESS on success

◆ Draw2D_clearRegion()

int32_t Draw2D_clearRegion ( Draw2D_Handle  pCtx,
uint32_t  startX,
uint32_t  startY,
uint32_t  width,
uint32_t  height 
)

Clear a region in the drawing buffer with transperency color.

Parameters
pCtx[IN] Draw 2D context
startX[IN] start X-position in the buffer
startY[IN] start Y-position in the buffer
width[IN] width of region in pixels
height[IN] height of region in lines
Returns
VX_SUCCESS on success

◆ Draw2D_fillRegion()

int32_t Draw2D_fillRegion ( Draw2D_Handle  pCtx,
Draw2D_RegionPrm prm 
)

Draw a region in the drawing buffer with custom color.

Parameters
pCtx[IN] Draw 2D context
prm[IN] Region Parameters
Returns
VX_SUCCESS on success

◆ Draw2D_drawPixel()

void Draw2D_drawPixel ( Draw2D_Handle  pCtx,
uint32_t  px,
uint32_t  py,
uint32_t  color,
uint32_t  colorFormat 
)

Draw pixel of a given color.

   Representation of color in this function depends on the data format
   set during Draw2D_setBufInfo()

   ex, 16-bit value for RGB565 data format
Parameters
pCtx[IN] Draw 2D context
px[IN] X-position in the buffer
py[IN] Y-position in the buffer
color[IN] Color used to draw the pixel
colorFormat[IN] Color format of the color
Returns
VX_SUCCESS on success

◆ Draw2D_drawBmp()

int32_t Draw2D_drawBmp ( Draw2D_Handle  pCtx,
uint32_t  startX,
uint32_t  startY,
Draw2D_BmpPrm pPrm 
)

Draw a bitmap into the drawing buffer.

Parameters
pCtx[IN] Draw 2D context
startX[IN] X-position in the buffer
startY[IN] Y-position in the buffer
pPrm[IN] Bitmap to use when drawing, when set to NULL default properties used
Returns
VX_SUCCESS on success

◆ Draw2D_drawBmp_rot()

int32_t Draw2D_drawBmp_rot ( Draw2D_Handle  pCtx,
uint32_t  startX,
uint32_t  startY,
Draw2D_BmpPrm pPrm,
uint32_t  rotate 
)

Draw a bitmap into the drawing buffer.

Parameters
pCtx[IN] Draw 2D context
startX[IN] X-position in the buffer
startY[IN] Y-position in the buffer
pPrm[IN] Bitmap to use when drawing, when set to NULL default properties used
rotate[IN] rotation angle, 0: 90 deg, 1: 180 deg, 2: 270 deg
Returns
VX_SUCCESS on success

◆ Draw2D_insertBmp()

int32_t Draw2D_insertBmp ( Draw2D_Handle  pCtx,
char *  input_file,
int32_t  startX,
int32_t  startY 
)

Draw a bitmap from BMP file at a specified display buffer location.

Parameters
pCtx[IN] Draw 2D context
input_file[IN] input .BMP file name
startX[IN] X position in display buffer
startY[IN] Y position in display buffer

◆ Draw2D_insertBmpFromMemory()

int32_t Draw2D_insertBmpFromMemory ( Draw2D_Handle  pCtx,
void *  buf,
uint32_t  buf_size,
int32_t  startX,
int32_t  startY 
)

Draw a bitmap from BMP file (pre-copied at a memory location) at a specified display buffer location.

Parameters
pCtx[IN] Draw 2D context
buf[IN] .BMP file in memory location
buf_size[IN] size of BMP file buffer
startX[IN] X position in display buffer
startY[IN] Y position in display buffer

◆ Draw2D_setFontColor()

void Draw2D_setFontColor ( uint16_t  colorText,
uint16_t  colorBorder,
uint16_t  colorBg 
)

Sets a global color to use for fonts in RGB565 format.

Parameters
colorText[IN] Color of text
colorBorder[IN] Color of text border
colorBg[IN] Color of text background

◆ Draw2D_resetFontColor()

void Draw2D_resetFontColor ( )

Restore font to default.

◆ Draw2D_floor()

static uint32_t Draw2D_floor ( uint32_t  val,
uint32_t  align 
)
inlinestatic

Initialize In queue parameters of a link.

Parameters
val[IN] Value to be rounded off
align[IN] Value to which val to be rounded
Returns
aligned value of val