![]() |
PDK API Guide for J721E
|
TPS65941 voltage monitoring details object structure.
Data Fields | |
uint8_t | monitortype |
uint8_t | regularEnable |
uint8_t | currentLimit |
uint8_t | voltOverLimit |
uint8_t | voltUnderLimit |
uint8_t | pgoodEnable |
uint8_t | overVoltEnable |
uint8_t Board_Tps65941VoltMonitorCfg::monitortype |
uint8_t Board_Tps65941VoltMonitorCfg::regularEnable |
Value to represent type of monitor (voltage/current)
uint8_t Board_Tps65941VoltMonitorCfg::currentLimit |
Value to represent regulator enable/disable
uint8_t Board_Tps65941VoltMonitorCfg::voltOverLimit |
Value to represent current limit
uint8_t Board_Tps65941VoltMonitorCfg::voltUnderLimit |
Value to represent voltage over limit
uint8_t Board_Tps65941VoltMonitorCfg::pgoodEnable |
Value to represent voltage under limit
uint8_t Board_Tps65941VoltMonitorCfg::overVoltEnable |
Value to represent PGood enable/disable