PDK API Guide for J721E
|
TPS65941 power resource details object structure.
Data Fields | |
uint8_t | cntrRegAddr |
uint8_t | cfgRegAddr |
uint8_t | voltageRegAddr |
uint8_t | pgRegAddr |
uint8_t Board_Tps65941PwrResourceRegCfg::cntrRegAddr |
uint8_t Board_Tps65941PwrResourceRegCfg::cfgRegAddr |
Register address of the power resource control
uint8_t Board_Tps65941PwrResourceRegCfg::voltageRegAddr |
Register address of the power resource configuration
uint8_t Board_Tps65941PwrResourceRegCfg::pgRegAddr |
Register address of the power resource voltage