![]() |
PDK API Guide for J721E
|
Application Interfaces provided by DS90UB926 FPD-Link device library.
Functions | |
Board_STATUS | Board_fpdUb926SetI2SChBEnableModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
I2S channel-B enable mode control. More... | |
Board_STATUS | Board_fpdUb926SetI2SChBOverrideModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
I2S channel-B override mode control. More... | |
Board_STATUS | Board_fpdUb926SetI2STransportSelModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
I2S Transport select mode control. More... | |
Board_STATUS | Board_fpdUb926SetI2SGenModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
I2S generation mode control. More... | |
Board_STATUS | Board_fpdUb926SetPassRGBModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
Pass RGB mode control. More... | |
Board_STATUS | Board_fpdUb926SetOverrideFCConfigModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
Override forward channel configuation mode control. More... | |
Board_STATUS | Board_fpdUb926SetRGB18bitModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
RGB 18-bit mode control. More... | |
Board_STATUS | Board_fpdUb926GetPLLLockStatus (void *handle, Board_FpdModuleObj *fpdModParams, bool *pllLockStatus) |
Get PLL lock status. More... | |
Board_STATUS | Board_fpdUb926RmtSerSlvDevAliasIdCfg (void *handle, Board_FpdModuleObj *fpdModParams, Board_FpdRmtDevObj *fpdRmtParams) |
Remote serializer slave device id config. More... | |
Board_STATUS | Board_fpdUb926SetI2CPassThrAllModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
I2C pass through all mode control. More... | |
Board_STATUS | Board_fpdUb926SetI2CPassThrModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
I2C pass through mode control. More... | |
Board_STATUS | Board_fpdUb926SetI2CBusFreq (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgBitRate) |
I2C bus frequency set. More... | |
Board_STATUS | Board_fpdUb926SetBackChModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
Deserializer back channel mode control. More... | |
Board_STATUS | Board_fpdUb926SetDigitalRst1ModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
Deserializer digital reset1 mode control. More... | |
Board_STATUS | Board_fpdUb926SetRmtAutoPwrDwnModeCtrl (void *handle, Board_FpdModuleObj *fpdModParams, uint8_t cfgMode) |
Remote auto-power down mode control. More... | |
void | Board_fpdUb926GetI2CAddr (uint8_t *domain, uint8_t *chNum, uint8_t *i2cAddr) |
Get ub926 i2c address. More... | |
Board_STATUS Board_fpdUb926SetI2SChBEnableModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
I2S channel-B enable mode control.
This function is used for configuring the deserializer I2S Channel-B mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926SetI2SChBOverrideModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
I2S channel-B override mode control.
This function is used for configuring the deserializer I2S Channel-B override mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926SetI2STransportSelModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
I2S Transport select mode control.
This function is used for configuring the deserializer I2S transport select mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926SetI2SGenModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
I2S generation mode control.
This function is used for configuring the deserializer I2S generation mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926SetPassRGBModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
Pass RGB mode control.
This function is used for configuring the deserializer RGB pass mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926SetOverrideFCConfigModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
Override forward channel configuation mode control.
This function is used for configuring the deserializer override forward channel mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926SetRGB18bitModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
RGB 18-bit mode control.
This function is used for configuring the deserializer RGB 18-bit mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926GetPLLLockStatus | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
bool * | pllLockStatus | ||
) |
Get PLL lock status.
This function is used for reading the deserializer PLL lock status
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
pllLockStatus | [IN/OUT] Buffer to hold PLL lock status |
Board_STATUS Board_fpdUb926RmtSerSlvDevAliasIdCfg | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
Board_FpdRmtDevObj * | fpdRmtParams | ||
) |
Remote serializer slave device id config.
This function is used for configuring the remote serializer slave device ID
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
fpdRmtParams | [IN] structure holding the fpd params |
Board_STATUS Board_fpdUb926SetI2CPassThrAllModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
I2C pass through all mode control.
This function is used for configuring the deserializer I2C pass through all mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926SetI2CPassThrModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
I2C pass through mode control.
This function is used for configuring the deserializer I2C pass through mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926SetI2CBusFreq | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgBitRate | ||
) |
I2C bus frequency set.
This function is used for setting the deserializer I2C bus frequency
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgBitRate | [IN] Indicates I2C serial clock frequency config modes BOARD_FPD_KBPS_100 - 100 KBPS BOARD_FPD_KBPS_400 - 400 KBPS |
Board_STATUS Board_fpdUb926SetBackChModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
Deserializer back channel mode control.
This function is used for configuring the deserializer back channel mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926SetDigitalRst1ModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
Deserializer digital reset1 mode control.
This function is used for configuring the deserializer digital reset1 mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
Board_STATUS Board_fpdUb926SetRmtAutoPwrDwnModeCtrl | ( | void * | handle, |
Board_FpdModuleObj * | fpdModParams, | ||
uint8_t | cfgMode | ||
) |
Remote auto-power down mode control.
This function is used for configuring the deserializer auto power down mode
handle | [IN] Low level driver handle |
fpdModParams | [IN] FPD module params |
cfgMode | [IN] Config mode - Indicates Enable or Disable |
void Board_fpdUb926GetI2CAddr | ( | uint8_t * | domain, |
uint8_t * | chNum, | ||
uint8_t * | i2cAddr | ||
) |
Get ub926 i2c address.
This function is used to get the I2C address and channel details of UB926 module.
domain | [IN] I2C instance domain |
chNum | [IN] buffer to hold i2c channel number |
i2cAddr | [IN] buffer to hold i2c address |