Vision Apps User Guide
Memory allocation APIs

Introduction

This section contains APIs for memory allocation.

Data Structures

struct  app_mem_heap_prm_t
 Heap initialization parameters. More...
 
struct  app_mem_init_prm_t
 Memory module initialization parameters. More...
 
struct  app_mem_stats_t
 Heap statistics and information. More...
 

Functions

static void * APP_MEM_ALIGNPTR (void *val, uint32_t align)
 Align ptr value to 'align' bytes. More...
 
static uint64_t APP_MEM_ALIGN64 (uint64_t val, uint32_t align)
 Align 64b value to 'align' bytes. More...
 
static uint32_t APP_MEM_ALIGN32 (uint32_t val, uint32_t align)
 Align 32b value to 'align' bytes. More...
 
void appMemInitPrmSetDefault (app_mem_init_prm_t *prm)
 Set defaults to app_mem_init_prm_t. More...
 
int32_t appMemInit (app_mem_init_prm_t *prm)
 Init heaps for memory allocation. More...
 
int32_t appMemDeInit ()
 De-Init heaps for memory allocation. More...
 
void * appMemAlloc (uint32_t heap_id, uint32_t size, uint32_t align)
 Alloc memory from specific heap. More...
 
int32_t appMemResetScratchHeap (uint32_t heap_id)
 Reset scratch memory. More...
 
int32_t appMemFree (uint32_t heap_id, void *ptr, uint32_t size)
 Free memory that was previously allocated. More...
 
uint32_t appMemGetDmaBufFd (void *virPtr, volatile uint32_t *dmaBufFdOffset)
 Return dmaBufFd of a CMEM buffer pointer. More...
 
int32_t appMemTranslateDmaBufFd (uint32_t dmaBufFd, uint32_t size, uint64_t *virtPtr, uint64_t *phyPtr)
 Translates a given 'dmaBufFd' to virtual and physical addresses. More...
 
void appMemCloseDmaBufFd (int32_t dmaBufFd)
 Close the dmaBufFd of a CMEM buffer pointer. More...
 
uint64_t appMemGetVirt2PhyBufPtr (uint64_t virtPtr, uint32_t heap_id)
 Return physical ptr corresponds to a CMEM virtual ptr. More...
 
int32_t appMemStats (uint32_t heap_id, app_mem_stats_t *stats)
 Return heap statistics and information. More...
 
void appMemCacheInv (void *ptr, uint32_t size)
 Invalidate a section of memory from cache. More...
 
void appMemCacheWb (void *ptr, uint32_t size)
 Write back a section of memory from cache. More...
 
void appMemCacheWbInv (void *ptr, uint32_t size)
 Write back and invalidate a section of memory from cache. More...
 

Macros

#define APP_MEM_HEAP_NAME_MAX   (16u)
 Max characters to use for heap name. More...
 

Memory heap ID

#define APP_MEM_HEAP_DDR   (0u)
 Heap located in DDR. More...
 
#define APP_MEM_HEAP_L3   (1u)
 Heap located in L3 memory (MSMC) More...
 
#define APP_MEM_HEAP_L2   (2u)
 Heap located in L2 local memory of a CPU. More...
 
#define APP_MEM_HEAP_L1   (3u)
 Heap located in L1 local memory of a CPU. More...
 
#define APP_MEM_HEAP_DDR_SCRATCH   (4u)
 Heap located in DDR and is used as scratch. More...
 
#define APP_MEM_HEAP_DDR_NON_CACHE   (5u)
 Heap located in DDR and in non-cache memory. More...
 
#define APP_MEM_HEAP_MAX   (6u)
 Max heaps in system. More...
 

Memory heap creation flags

#define APP_MEM_HEAP_FLAGS_TYPE_LINEAR_ALLOCATE   (0x00000001u)
 Heap flag to indicate heap is of type "linear allocater". More...
 
#define APP_MEM_HEAP_FLAGS_IS_SHARED   (0x00000004u)
 Heap flag to indicate if memory that is allcoate will be shared with another CPU. More...
 
#define APP_MEM_HEAP_FLAGS_DO_CLEAR_ON_ALLOC   (0x00000008u)
 Heap flag to indicate if memory should be set to 0 after alloc. More...
 

Macro Definition Documentation

◆ APP_MEM_HEAP_NAME_MAX

#define APP_MEM_HEAP_NAME_MAX   (16u)

Max characters to use for heap name.

◆ APP_MEM_HEAP_DDR

#define APP_MEM_HEAP_DDR   (0u)

Heap located in DDR.

◆ APP_MEM_HEAP_L3

#define APP_MEM_HEAP_L3   (1u)

Heap located in L3 memory (MSMC)

◆ APP_MEM_HEAP_L2

#define APP_MEM_HEAP_L2   (2u)

Heap located in L2 local memory of a CPU.

◆ APP_MEM_HEAP_L1

#define APP_MEM_HEAP_L1   (3u)

Heap located in L1 local memory of a CPU.

◆ APP_MEM_HEAP_DDR_SCRATCH

#define APP_MEM_HEAP_DDR_SCRATCH   (4u)

Heap located in DDR and is used as scratch.

◆ APP_MEM_HEAP_DDR_NON_CACHE

#define APP_MEM_HEAP_DDR_NON_CACHE   (5u)

Heap located in DDR and in non-cache memory.

◆ APP_MEM_HEAP_MAX

#define APP_MEM_HEAP_MAX   (6u)

Max heaps in system.

◆ APP_MEM_HEAP_FLAGS_TYPE_LINEAR_ALLOCATE

#define APP_MEM_HEAP_FLAGS_TYPE_LINEAR_ALLOCATE   (0x00000001u)

Heap flag to indicate heap is of type "linear allocater".

Here alloc increments a offset by alloc size and free resets the offset. This is used typically for L2 memory to allocate it as scratch among multiple algorithms on DSP.

When this flag is not set heap type is normal dynamic memory allocator heap

◆ APP_MEM_HEAP_FLAGS_IS_SHARED

#define APP_MEM_HEAP_FLAGS_IS_SHARED   (0x00000004u)

Heap flag to indicate if memory that is allcoate will be shared with another CPU.

◆ APP_MEM_HEAP_FLAGS_DO_CLEAR_ON_ALLOC

#define APP_MEM_HEAP_FLAGS_DO_CLEAR_ON_ALLOC   (0x00000008u)

Heap flag to indicate if memory should be set to 0 after alloc.

Function Documentation

◆ APP_MEM_ALIGNPTR()

static void* APP_MEM_ALIGNPTR ( void *  val,
uint32_t  align 
)
inlinestatic

Align ptr value to 'align' bytes.

◆ APP_MEM_ALIGN64()

static uint64_t APP_MEM_ALIGN64 ( uint64_t  val,
uint32_t  align 
)
inlinestatic

Align 64b value to 'align' bytes.

◆ APP_MEM_ALIGN32()

static uint32_t APP_MEM_ALIGN32 ( uint32_t  val,
uint32_t  align 
)
inlinestatic

Align 32b value to 'align' bytes.

◆ appMemInitPrmSetDefault()

void appMemInitPrmSetDefault ( app_mem_init_prm_t prm)

Set defaults to app_mem_init_prm_t.

Recommend to be called before calling appMemInit() Override default with user specific parameters

By default all heaps are disabled.

Parameters
prm[out] Default initialized parameters

◆ appMemInit()

int32_t appMemInit ( app_mem_init_prm_t prm)

Init heaps for memory allocation.

Parameters
prm[in] Initialization parameters
Returns
0 on success else failure

◆ appMemDeInit()

int32_t appMemDeInit ( )

De-Init heaps for memory allocation.

Returns
0 on success else failure

◆ appMemAlloc()

void* appMemAlloc ( uint32_t  heap_id,
uint32_t  size,
uint32_t  align 
)

Alloc memory from specific heap.

Parameters
heap_id[in] See APP_MEM_HEAP_* \ Incase of Linux CMEM, set CMEM block ID
size[in] Size in bytes to allocate
align[in] Minimum alignment requested
Returns
pointer to memory or NULL in case of failure

◆ appMemResetScratchHeap()

int32_t appMemResetScratchHeap ( uint32_t  heap_id)

Reset scratch memory.

Parameters
heap_id[in] See APP_MEM_HEAP_* \ Incase of Linux CMEM, set CMEM block ID
Returns
0 on success else failure

◆ appMemFree()

int32_t appMemFree ( uint32_t  heap_id,
void *  ptr,
uint32_t  size 
)

Free memory that was previously allocated.

Parameters
heap_id[in] See APP_MEM_HEAP_* \ Incase of Linux CMEM, set CMEM block ID
ptr[in] pointer to allocated memory
size[in] size of allocated memory
Returns
0 on success else failure

◆ appMemGetDmaBufFd()

uint32_t appMemGetDmaBufFd ( void *  virPtr,
volatile uint32_t *  dmaBufFdOffset 
)

Return dmaBufFd of a CMEM buffer pointer.

Parameters
virPtr[in] pointer to allocated memory
dmaBufFdOffset[out] offset within the DMA BUF FD where the data is located
Returns
dmaBufFd or NULL in case of failure

◆ appMemTranslateDmaBufFd()

int32_t appMemTranslateDmaBufFd ( uint32_t  dmaBufFd,
uint32_t  size,
uint64_t *  virtPtr,
uint64_t *  phyPtr 
)

Translates a given 'dmaBufFd' to virtual and physical addresses.

Parameters
dmaBufFd[in] DMA Buffer Id to translate.
size[in] Size of buffer in bytes
virtPtr[out] Virtual address of the memory represented by 'dmaBufFd'.
phyPtr[out] Physical address of the memory represented by 'dmaBufFd'.
Returns
0, if the translation is successful or < 0 otherwise.

◆ appMemCloseDmaBufFd()

void appMemCloseDmaBufFd ( int32_t  dmaBufFd)

Close the dmaBufFd of a CMEM buffer pointer.

Parameters
dmaBufFd[in] value of dmaBufFd

◆ appMemGetVirt2PhyBufPtr()

uint64_t appMemGetVirt2PhyBufPtr ( uint64_t  virtPtr,
uint32_t  heap_id 
)

Return physical ptr corresponds to a CMEM virtual ptr.

Parameters
virtPtr[in] pointer to allocated memory
heap_id[in] heap ID
Returns
Physical pointer to memory or NULL in case of failure

◆ appMemStats()

int32_t appMemStats ( uint32_t  heap_id,
app_mem_stats_t stats 
)

Return heap statistics and information.

Parameters
heap_id[in] See APP_MEM_HEAP_* \ Incase of Linux CMEM, set CMEM block ID
stats[in] Heap statistics and information
Returns
0 on success else failure

◆ appMemCacheInv()

void appMemCacheInv ( void *  ptr,
uint32_t  size 
)

Invalidate a section of memory from cache.

Parameters
ptr[in] Memory address for cache ops
size[in] Size of memory to perform the cache ops

◆ appMemCacheWb()

void appMemCacheWb ( void *  ptr,
uint32_t  size 
)

Write back a section of memory from cache.

Parameters
ptr[in] Memory address for cache ops
size[in] Size of memory to perform the cache ops

◆ appMemCacheWbInv()

void appMemCacheWbInv ( void *  ptr,
uint32_t  size 
)

Write back and invalidate a section of memory from cache.

Parameters
ptr[in] Memory address for cache ops
size[in] Size of memory to perform the cache ops