MCUSW
|
This files defines ICU MCAL configuration structures
Data Structures | |
struct | Icu_DutyCycleType |
This type defines Duty Cycle struct. More... | |
struct | Icu_ChannelConfigType_PC |
ICU Channel Config Structure of Pre-Compile only. More... | |
struct | Icu_ConfigType_PC |
ICU Config Structure of Pre-Compile only. More... | |
struct | Icu_ChannelConfigType |
ICU Channel Config Structure. More... | |
struct | Icu_ConfigType |
ICU Config Structure. More... | |
Functions | |
void | Icu_Init (const Icu_ConfigType *ConfigPtr) |
Service for ICU initialization. More... | |
void | Icu_DeInit (void) |
Service for ICU de-initialization. More... | |
void | Icu_SetActivationCondition (Icu_ChannelType Channel, Icu_ActivationType Activation) |
Service for setting Activation Condition. More... | |
void | Icu_DisableNotification (Icu_ChannelType Channel) |
Service for disabling notification. More... | |
void | Icu_EnableNotification (Icu_ChannelType Channel) |
Service for enabling notification. More... | |
Icu_InputStateType | Icu_GetInputState (Icu_ChannelType Channel) |
Service for getting the ICU input status. More... | |
void | Icu_StartTimestamp (Icu_ChannelType Channel, Icu_ValueType *BufferPtr, uint16 BufferSize, uint16 NotifyInterval) |
Service for starts the captuing of timer values on the edges. More... | |
void | Icu_StopTimestamp (Icu_ChannelType Channel) |
Service for stopping the timestamp measurement. More... | |
Icu_IndexType | Icu_GetTimestampIndex (Icu_ChannelType Channel) |
Service for reading the timestamp index of a givem channel. More... | |
void | Icu_ResetEdgeCount (Icu_ChannelType Channel) |
Service for resets the value of the counted edges to zero. More... | |
void | Icu_EnableEdgeCount (Icu_ChannelType Channel) |
Service enabling the counting of edges of a given channel. More... | |
void | Icu_DisableEdgeCount (Icu_ChannelType Channel) |
Service for disabling the couting of edges of the given channel. More... | |
Icu_EdgeNumberType | Icu_GetEdgeNumbers (Icu_ChannelType Channel) |
Service for reading the number of counted edges. More... | |
void | Icu_EnableEdgeDetection (Icu_ChannelType Channel) |
Service for enabling/re-enabling the detection of edges of the given channel. More... | |
void | Icu_DisableEdgeDetection (Icu_ChannelType Channel) |
Service for disabling the detection of edges of the given channel. More... | |
void | Icu_StartSignalMeasurement (Icu_ChannelType Channel) |
Service for starting the measurement of signals. More... | |
void | Icu_StopSignalMeasurement (Icu_ChannelType Channel) |
Service for stopping the measurement of signals. More... | |
Icu_ValueType | Icu_GetTimeElapsed (Icu_ChannelType Channel) |
Service for reading the elasped time for the given channel. More... | |
void | Icu_GetDutyCycleValues (Icu_ChannelType Channel, Icu_DutyCycleType *DutyCycleValues) |
Service for reading the coherent active time and period time of given channel. More... | |
Variables | |
const struct Icu_ConfigType_PC_s | IcuConfigSet_PC |
ICU Configuration structure declaration. More... | |
const struct Icu_ConfigType_s | IcuConfigSet |
Macros | |
#define | ICU_PRE_COMPILE_VARIANT (STD_ON ) |
ICU Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time) More... | |
#define | ICU_DE_INIT_API (STD_ON) |
Enable/Disable Icu DeInit API. More... | |
#define | ICU_EDGE_COUNT_API (STD_ON) |
Enable/Disable Edge Count API. More... | |
#define | ICU_EDGE_DETECT_API (STD_ON) |
Enable/Disable Edge Detect API. More... | |
#define | ICU_GET_DUTY_CYCLE_VALUES_API (STD_ON) |
Enable/Disable Get Duty Cycle Values API. More... | |
#define | ICU_GET_INPUT_STATE_API (STD_ON) |
Enable/Disable Get Input State API. More... | |
#define | ICU_GET_TIME_ELAPSED_API (STD_ON) |
Enable/Disable Get Time Elapsed API. More... | |
#define | ICU_GET_VERSION_INFO_API (STD_ON) |
Enable/Disable Get Version Info API. More... | |
#define | ICU_SIGNAL_MEASUREMENT_API (STD_ON) |
Enable/Disable Signal Measurement API. More... | |
#define | ICU_TIMESTAMP_API (STD_ON) |
Enable/Disable Timestamp API. More... | |
#define | ICU_DEV_ERROR_DETECT (STD_ON) |
Enable/Disable Development error detet. More... | |
#define | IcuConf_IcuChannelConfiguration_IcuChannel_0 (1U) |
Channel ID Symbolic Names Configured channel ID(s) More... | |
#define | ICU_INIT_CONFIG_PC IcuConfigSet |
Pre Compile config macro name. More... | |
Macros to define Rising and Falling edge config for capture registers | |
enum | Icu_ModeType { ICU_MODE_NORMAL, ICU_MODE_SLEEP } |
This type defines a range of mode type. More... | |
enum | Icu_InputStateType { ICU_ACTIVE, ICU_IDLE } |
This type defines a input state of ICU driver. More... | |
enum | Icu_ActivationType { ICU_RISING_EDGE, ICU_FALLING_EDGE, ICU_BOTH_EDGES } |
This type defines Activation range. More... | |
enum | Icu_MeasurementModeType { ICU_MODE_SIGNAL_EDGE_DETECT, ICU_MODE_SIGNAL_MEASUREMENT, ICU_MODE_TIMESTAMP, ICU_MODE_EDGE_COUNTER } |
This type defines available measurement modes. More... | |
enum | Icu_SignalMeasurementPropertyType { ICU_LOW_TIME, ICU_HIGH_TIME, ICU_PERIOD_TIME, ICU_DUTY_CYCLE } |
This type defines Signal Measurement Property range. More... | |
enum | Icu_TimestampBufferType { ICU_LINEAR_BUFFER, ICU_CIRCULAR_BUFFER } |
This type defines TimeStamp Property range. More... | |
typedef uint16 | Icu_ValueType |
This type defines Value type. More... | |
typedef uint32 | Icu_IndexType |
This type defines return value Icu_GetTimeStampIndex. More... | |
typedef uint32 | Icu_EdgeNumberType |
This type defines return value of Icu-Icu_GetEdgeNumbers. More... | |
typedef void(* | Icu_NotifyFuncType) (void) |
Notification callback function pointer. More... | |
typedef uint8 | Icu_ChannelType |
This type defines Channel type. More... | |
typedef uint8 | Icu_ChannelPrescalerType |
This type defines Prescaler type. More... | |
#define ICU_PRE_COMPILE_VARIANT (STD_ON ) |
ICU Build Variant. Build variants.(i.e Pre-compile,Post-build or Link time)
#define ICU_DE_INIT_API (STD_ON) |
Enable/Disable Icu DeInit API.
#define ICU_EDGE_COUNT_API (STD_ON) |
Enable/Disable Edge Count API.
#define ICU_EDGE_DETECT_API (STD_ON) |
Enable/Disable Edge Detect API.
#define ICU_GET_DUTY_CYCLE_VALUES_API (STD_ON) |
Enable/Disable Get Duty Cycle Values API.
#define ICU_GET_INPUT_STATE_API (STD_ON) |
Enable/Disable Get Input State API.
#define ICU_GET_TIME_ELAPSED_API (STD_ON) |
Enable/Disable Get Time Elapsed API.
#define ICU_GET_VERSION_INFO_API (STD_ON) |
Enable/Disable Get Version Info API.
#define ICU_SIGNAL_MEASUREMENT_API (STD_ON) |
Enable/Disable Signal Measurement API.
#define ICU_TIMESTAMP_API (STD_ON) |
Enable/Disable Timestamp API.
#define ICU_DEV_ERROR_DETECT (STD_ON) |
Enable/Disable Development error detet.
#define IcuConf_IcuChannelConfiguration_IcuChannel_0 (1U) |
Channel ID Symbolic Names Configured channel ID(s)
Channel identifiers
#define ICU_INIT_CONFIG_PC IcuConfigSet |
Pre Compile config macro name.
typedef uint16 Icu_ValueType |
This type defines Value type.
typedef uint32 Icu_IndexType |
This type defines return value Icu_GetTimeStampIndex.
typedef uint32 Icu_EdgeNumberType |
This type defines return value of Icu-Icu_GetEdgeNumbers.
typedef void(* Icu_NotifyFuncType) (void) |
Notification callback function pointer.
typedef uint8 Icu_ChannelType |
This type defines Channel type.
typedef uint8 Icu_ChannelPrescalerType |
This type defines Prescaler type.
enum Icu_ModeType |
enum Icu_InputStateType |
enum Icu_ActivationType |
void Icu_Init | ( | const Icu_ConfigType * | ConfigPtr | ) |
Service for ICU initialization.
* Service name : Icu_Init * Syntax : Icu_Init(const Icu_ConfigType* ConfigPtr) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x00 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : Pointer to the configuration * Parameters (out) : None * Return value : void * Description : Initializes internal variables * and the ECAP unit of the micro controller. * The function can be called on task level. *
void Icu_DeInit | ( | void | ) |
Service for ICU de-initialization.
* Service name : Icu_DeInit * Syntax : Icu_DeInit(void) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x01 * Sync/Async : Synchronous * Reentrancy : Non Reentrant * Parameters (in) : None * Parameters (out) : None * Return value : void * Description : DeInit ECAP module *
void Icu_SetActivationCondition | ( | Icu_ChannelType | Channel, |
Icu_ActivationType | Activation | ||
) |
Service for setting Activation Condition.
* Service name : Icu_SetActivationCondition * Syntax : Icu_SetActivationCondition(Icu_ChannelType Channel, * Icu_ActivationType Activation) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x05 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (in) : Icu_ActivationType Activation * Parameters (out) : None * Return value : void * Description : This service sets the Activation edge for channel * Type of activation (if supported by hardware) * ICU_RISING_EDGE, ICU_FALLING_EDGE, ICU_BOTH_EDGES *
void Icu_DisableNotification | ( | Icu_ChannelType | Channel | ) |
Service for disabling notification.
* Service name : Icu_DisableNotification * Syntax : Icu_DisableNotification(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x06 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service disables the notificaiton of a channel *
void Icu_EnableNotification | ( | Icu_ChannelType | Channel | ) |
Service for enabling notification.
* Service name : Icu_EnableNotification * Syntax : Icu_EnableNotification(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x07 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service enables the notificaiton of a channel *
Icu_InputStateType Icu_GetInputState | ( | Icu_ChannelType | Channel | ) |
Service for getting the ICU input status.
* Service name : Icu_GetInputState * Syntax : Icu_GetInputState(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x08 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service returns the status of the ICU input *
void Icu_StartTimestamp | ( | Icu_ChannelType | Channel, |
Icu_ValueType * | BufferPtr, | ||
uint16 | BufferSize, | ||
uint16 | NotifyInterval | ||
) |
Service for starts the captuing of timer values on the edges.
* Service name : Icu_StartTimestamp * Syntax : Icu_StartTimestamp(Icu_ChannelType Channel, * Icu_ValueType* BufferPtr, * uint16 BufferSize, * uint16 NotifyInterval) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x09 * Sync/Async : Asynchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (in) : uint16 BufferSize * Parameters (in) : uint16 NotifyInterval * Parameters (out) : Icu_ValueType* BufferPtr * Return value : void * Description : This service starts the capturing of timer values on the edges *
void Icu_StopTimestamp | ( | Icu_ChannelType | Channel | ) |
Service for stopping the timestamp measurement.
* Service name : Icu_StopTimestamp * Syntax : Icu_StopTimestamp(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0A * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service stops timestamp measurement of the given channel. *
Icu_IndexType Icu_GetTimestampIndex | ( | Icu_ChannelType | Channel | ) |
Service for reading the timestamp index of a givem channel.
* Service name : Icu_GetTimestampIndex * Syntax : Icu_GetTimestampIndex(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0B * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service reads the timestamp index of a given channel. *
void Icu_ResetEdgeCount | ( | Icu_ChannelType | Channel | ) |
Service for resets the value of the counted edges to zero.
* Service name : Icu_ResetEdgeCount * Syntax : Icu_ResetEdgeCount(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0C * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service resets the value of the counted edges to zero. *
void Icu_EnableEdgeCount | ( | Icu_ChannelType | Channel | ) |
Service enabling the counting of edges of a given channel.
* Service name : Icu_EnableEdgeCount * Syntax : Icu_EnableEdgeCount(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0D * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service enables the couting of edges of the given channel. *
void Icu_DisableEdgeCount | ( | Icu_ChannelType | Channel | ) |
Service for disabling the couting of edges of the given channel.
* Service name : Icu_DisableEdgeCount * Syntax : Icu_DisableEdgeCount(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x0E * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service disables the couting of edges of a given channel. *
Icu_EdgeNumberType Icu_GetEdgeNumbers | ( | Icu_ChannelType | Channel | ) |
Service for reading the number of counted edges.
* Service name : Icu_GetEdgeNumbers * Syntax : Icu_GetEdgeNumbers(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x0F * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service reads the number of counted edges. *
void Icu_EnableEdgeDetection | ( | Icu_ChannelType | Channel | ) |
Service for enabling/re-enabling the detection of edges of the given channel.
* Service name : Icu_EnableEdgeDetection * Syntax : Icu_EnableEdgeDetection(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x16 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service enables/re-enables the detection of edges of a channel. *
void Icu_DisableEdgeDetection | ( | Icu_ChannelType | Channel | ) |
Service for disabling the detection of edges of the given channel.
* Service name : Icu_EnableEdgeDetection * Syntax : Icu_EnableEdgeDetection(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x17 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service disables the detection of edges of a channel. *
void Icu_StartSignalMeasurement | ( | Icu_ChannelType | Channel | ) |
Service for starting the measurement of signals.
* Service name : Icu_StartSignalMeasurement * Syntax : Icu_StartSignalMeasurement(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x13 * Sync/Async : Asynchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service starts the measurement of signals of a given channel. *
void Icu_StopSignalMeasurement | ( | Icu_ChannelType | Channel | ) |
Service for stopping the measurement of signals.
* Service name : Icu_StopSignalMeasurement * Syntax : Icu_StopSignalMeasurement(Icu_ChannelType Channel) * Mode : Supervisor Mode (Privileged Mode) * Service ID[hex] : 0x14 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service stops the measurement of signals of a given channel. *
Icu_ValueType Icu_GetTimeElapsed | ( | Icu_ChannelType | Channel | ) |
Service for reading the elasped time for the given channel.
* Service name : Icu_GetTimeElapsed * Syntax : Icu_GetTimeElapsed(Icu_ChannelType Channel) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x10 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : None * Return value : void * Description : This service reads elasped time for a given channel. *
void Icu_GetDutyCycleValues | ( | Icu_ChannelType | Channel, |
Icu_DutyCycleType * | DutyCycleValues | ||
) |
Service for reading the coherent active time and period time of given channel.
* Service name : Icu_GetTimeElapsed * Syntax : Icu_GetTimeElapsed(Icu_ChannelType Channel, * Icu_DutyCycleType* DutyCycleValues) * Mode : User Mode (Non-Privileged Mode) * Service ID[hex] : 0x11 * Sync/Async : Synchronous * Reentrancy : Reentrant * Parameters (in) : Icu_ChannelType Channel * Parameters (out) : Icu_DutyCycleType* DutyCycleValues * Return value : void * Description : This service reads active time and period of given channel. *
const struct Icu_ConfigType_PC_s IcuConfigSet_PC |
ICU Configuration structure declaration.
const struct Icu_ConfigType_s IcuConfigSet |