MCUSW
|
This file contains generated pre compile configurations for CDD IPC MCAL driver.
Go to the source code of this file.
Macros | |
#define | CDD_IPC_PRE_COMPILE_VARIANT (STD_ON) |
Pre-Compile Build Variant flag. STD_ON for VariantPreCompile / STD_OFF for VariantPostBuild. More... | |
#define | CDD_IPC_DEV_ERROR_DETECT (STD_ON) |
Enable/disable CDD Ipc dev detect error. More... | |
#define | CDD_IPC_ISR_TYPE (CDD_IPC_ISR_CAT2) |
ISR type. More... | |
#define | CDD_IPC_NEW_MSG_NTFY_FXN Cdd_IpcNewMessageNotify |
#define | CDD_IPC_NEW_CTRL_MSG_NTFY_FXN Cdd_IpcNewCtrlMessageNotify |
Pre-Compile Switches for API Services | |
#define | CDD_IPC_VERSION_INFO_API (STD_ON) |
Enable/disable version info API. More... | |
#define | CDD_IPC_DEINIT_API (STD_ON) |
Enable/disable De Initialization API. More... | |
#define | CDD_IPC_ANNOUNCE_API (STD_ON) |
Enable/disable Service Announcement API. More... | |
#define | CDD_IPC_REGISTER_READBACK_API (STD_ON) |
Enable/disable Critical Register read back API. More... | |
#define | CDD_IPC_IS_INIT_DONE_API (STD_ON) |
Enable/disable Cdd_IpcIsInitDone API. More... | |
#define | CDD_IPC_GET_MAX_MSG_SIZE_API (STD_ON) |
Enable/disable Cdd_IpcGetMaxMsgSize API. More... | |
Dependency configurations | |
#define | CDD_IPC_OS_COUNTER_ID ((CounterType)OsCounter_0) |
Counter ID for counter used to count wait ticks. More... | |
Cdd Ipc DEM Error codes to report | |
Pre-compile switches for enabling/disabling DEM events | |
#define | DemConf_DemEventParameter_CDD_IPC_DEM_NO_EVENT (0xFFFFU) |
#define | CDD_IPC_DEM_NO_EVENT DemConf_DemEventParameter_CDD_IPC_DEM_NO_EVENT |
#define | CDD_IPC_E_HARDWARE_ERROR (DemConf_DemEventParameter_CDD_IPC_E_HARDWARE_ERROR) |
Hardware failed. More... | |
CORE Names | |
#define | CDD_IPC_CORE_MPU1_0 (0u) |
#define | CDD_IPC_CORE_MCU1_0 (1U) |
#define | CDD_IPC_CORE_MCU1_1 (2U) |
#define | CDD_IPC_CORE_MCU2_0 (3U) |
#define | CDD_IPC_CORE_MCU2_1 (4U) |
#define | CDD_IPC_CORE_MCU3_0 (5U) |
#define | CDD_IPC_CORE_MCU3_1 (6U) |
#define | CDD_IPC_CORE_C66X_1 (7U) |
#define | CDD_IPC_CORE_C66X_2 (8U) |
#define | CDD_IPC_CORE_C7X_1 (9U) |
#define | CDD_IPC_CORE_MPU1_1 (10U) |
#define | CDD_IPC_CORE_MAX_PROCS (11U) |
#define | CDD_IPC_OWN_CORE_ID (CDD_IPC_CORE_MCU1_0) |
Used core identifiers. More... | |
#define | CDD_IPC_REMOTE_CORE_MCU2_0_USED |
#define | CDD_IPC_REMOTE_CORE_MPU1_0_USED |
#define | CDD_IPC_REMOTE_CORE_MCU2_1_USED |
VirtIO Object | |
#define | CDD_IPC_VERTIO_OBJECT_SIZE (0x1000U) |
Communication Channel ID & Configured Buffer sizes | |
#define | CddIpcConf_IpcComChanId_Cdd_IpcMpu10 (0U) |
#define | CddIpcConf_IpcComChanId_Cdd_IpcMcu20 (1U) |
#define | CddIpcConf_IpcComChanId_Cdd_IpcMcu21 (2U) |
#define | CDD_IPC_RPMSG_OBJ_SIZE (256U) |
#define | CDD_IPC_CH_0_BUFF_SIZE ((256U * 512U) + CDD_IPC_RPMSG_OBJ_SIZE) |
#define | CDD_IPC_CH_1_BUFF_SIZE ((256U * 512U) + CDD_IPC_RPMSG_OBJ_SIZE) |
#define | CDD_IPC_CH_2_BUFF_SIZE ((256U * 512U) + CDD_IPC_RPMSG_OBJ_SIZE) |
#define | CDD_IPC_MAX_CHANNEL_CFG (3U) |
Functions | |
void | Cdd_IpcNewMessageNotify (uint32 comId) |
New Message notification function. More... | |
void | Cdd_IpcNewCtrlMessageNotify (uint32 remoteProcId) |
New Control Message notification function. More... | |
Variables | |
const struct Cdd_IpcConfigType_s | CddIpcConfiguraions_PC |
const struct Cdd_IpcChannelBufType_s | Cdd_IpcCommChanBufferPtr [CDD_IPC_MAX_CHANNEL_CFG] |
A array of buffer pointers that describe memory allocated to local communication channels. More... | |
uint8 | Cdd_IpcDrvVertIoObj [CDD_IPC_VERTIO_OBJECT_SIZE] |
Communication Channels configured. More... | |