MCUSW
|
This file contains generated pre compile configuration file for ADC MCAL driver.
Go to the source code of this file.
Macros | |
#define | ADC_VARIANT_POST_BUILD (STD_ON) |
ADC Build Variant. Build variants.(i.e Pre Compile,Post Build) More... | |
#define | ADC_DEV_ERROR_DETECT (STD_ON) |
Pre Compile config macro name. More... | |
#define | ADC_GROUP_LOG (STD_OFF) |
Enable/disable ADC group log. More... | |
#define | ADC_MAX_GROUP_LOG (100U) |
Maximum group log entries when logging is ON. More... | |
#define | ADC_FIFO_ERR_LOG (STD_OFF) |
Enable/disable ADC FIFO error log. More... | |
#define | ADC_MAX_FIFO_ERR_LOG (100U) |
Maximum FIFO error log entries when logging is ON. More... | |
#define | ADC_VERSION_INFO_API (STD_ON) |
Enable/disable ADC get version info API. More... | |
#define | ADC_READ_GROUP_API (STD_ON) |
Read group API. More... | |
#define | ADC_GRP_NOTIF_CAPABILITY_API (STD_ON) |
Enable/disable ADC enable/disable group notify API. More... | |
#define | ADC_ENABLE_START_STOP_GROUP_API (STD_ON) |
Enable/disable ADC start/stop group notify API. More... | |
#define | ADC_DEINIT_API (STD_ON) |
Enable/disable ADC deinit API. More... | |
#define | ADC_PRIORITY_IMPLEMENTATION (ADC_PRIORITY_HW_SW) |
Determines whether a priority mechanism is available for prioritization of the conversion requests and if available, the type of prioritization mechanism. More... | |
#define | ADC_ENABLE_QUEUING (STD_ON) |
Determines, if the queuing mechanism is active in case of priority mechanism disabled. More... | |
#define | ADC_RESULT_ALIGNMENT (ADC_ALIGN_RIGHT) |
Alignment of ADC raw results in ADC result buffer (left/right alignment) More... | |
#define | ADC_MAX_GROUP (2U) |
Maximum group across all hwunit. More... | |
#define | ADC_MAX_HW_UNIT (2U) |
Maximum HW unit - This should match the sum for the below units ISR which are ON. More... | |
#define | ADC_INSTANCE_0 |
#define | ADC_INSTANCE_1 |
#define | ADC_ISR_TYPE (ADC_ISR_CAT1) |
ISR type. More... | |
#define | ADC_OS_COUNTER_ID ((CounterType)0U) |
Counter ID for counter used to count wait ticks. More... | |
#define | ADC_TIMEOUT_DURATION (10000U) |
ADC timeout - used in ADC AFE busy wait and FSM busy wait. More... | |
#define | ADC_REGISTER_READBACK_API (STD_ON) |
Enable/disable ADC register read back API. More... | |
#define | ADC_DIFFERENTIAL_INPUT_ENABLE (STD_OFF) |
Enable/disable ADC differential input support. More... | |
Adc Group Id names | |
Defines for symbolic names for the AdcGroupId | |
#define | AdcConf_AdcHwUnit_AdcHwUnit_0_AdcGroup_AdcGroup_0 (0U) |
#define | ADC_GROUP_ID_0 AdcConf_AdcHwUnit_AdcHwUnit_0_AdcGroup_AdcGroup_0 |
#define | AdcConf_AdcHwUnit_AdcHwUnit_1_AdcGroup_AdcGroup_0 (1U) |
#define | ADC_GROUP_ID_1 AdcConf_AdcHwUnit_AdcHwUnit_1_AdcGroup_AdcGroup_0 |
Adc Hw Unit Id names | |
Defines for symbolic names for the AdcHwUnitId | |
#define | AdcConf_AdcHwUnit_AdcHwUnit_0 (ADC_UNIT_0) |
#define | ADC_HW_UNIT_ID_0 AdcConf_AdcHwUnit_AdcHwUnit_0 |
#define | AdcConf_AdcHwUnit_AdcHwUnit_1 (ADC_UNIT_1) |
#define | ADC_HW_UNIT_ID_1 AdcConf_AdcHwUnit_AdcHwUnit_1 |
Adc Group Channel Id names | |
Defines for symbolic names for the Adc Group Channel Id | |
#define | AdcConf_AdcHwUnit_AdcHwUnit_0_AdcGroup_AdcGroup_0_AdcChannel_AdcChannel_0 (0U) |
Channel Ids for each group. More... | |
#define | ADC_HW_UNIT_ID_ADCHWUNIT_0_GROUP_ID_CHANNEL_ID_ADCCHANNEL_0 AdcConf_AdcHwUnit_AdcHwUnit_0_AdcGroup_AdcGroup_0_AdcChannel_AdcChannel_0 |
#define | AdcConf_AdcHwUnit_AdcHwUnit_1_AdcGroup_AdcGroup_0_AdcChannel_AdcChannel_0 (0U) |
#define | ADC_HW_UNIT_ID_ADCHWUNIT_1_GROUP_ID_CHANNEL_ID_ADCCHANNEL_0 AdcConf_AdcHwUnit_AdcHwUnit_1_AdcGroup_AdcGroup_0_AdcChannel_AdcChannel_0 |
Adc Channel Id names | |
Defines for symbolic names for the Adc Channel Id | |
#define | AdcConf_AdcHwUnit_AdcHwUnit_0_AdcChannel_AdcChannel_0 (0U) |
Channel Ids for all channels. More... | |
#define | ADC_HW_UNIT_ID_ADCHWUNIT_0_CHANNEL_ID_ADCCHANNEL_0 AdcConf_AdcHwUnit_AdcHwUnit_0_AdcChannel_AdcChannel_0 |
#define | AdcConf_AdcHwUnit_AdcHwUnit_1_AdcChannel_AdcChannel_0 (0U) |
#define | ADC_HW_UNIT_ID_ADCHWUNIT_1_CHANNEL_ID_ADCCHANNEL_0 AdcConf_AdcHwUnit_AdcHwUnit_1_AdcChannel_AdcChannel_0 |
ADC DEM Error codes to report | |
Pre-compile switches for enabling/disabling DEM events | |
#define | DemConf_DemEventParameter_ADC_DEM_NO_EVENT (0xFFFFU) |
#define | ADC_DEM_NO_EVENT DemConf_DemEventParameter_ADC_DEM_NO_EVENT |
#define | ADC_E_HARDWARE_ERROR (DemConf_DemEventParameter_ADC_E_HARDWARE_ERROR) |
Hardware failed. More... | |
Variables | |
const struct Adc_ConfigType_s | AdcConfigSet |
ADC Configuration struct declaration. More... | |