![]() |
TIOVX User Guide
|
Internal APIs for platform operations.
Enumerations | |
| enum | tivx_platform_lock_type_e { TIVX_PLATFORM_LOCK_OBJ_DESC_TABLE = 0, TIVX_PLATFORM_LOCK_CONTEXT, TIVX_PLATFORM_LOCK_DATA_REF_QUEUE, TIVX_PLATFORM_LOCK_LOG_RT_INDEX, TIVX_PLATFORM_LOCK_LOG_RT, TIVX_PLATFORM_LOCK_MAX } |
| Types of system level locks. More... | |
Functions | |
| vx_enum | tivxPlatformGetTargetId (const char *target_name) |
| Convert a target name to a specific target ID. More... | |
| void | tivxPlatformGetTargetName (vx_enum target_id, char *target_name) |
| Convert a specific target ID to a target name. More... | |
| vx_bool | tivxPlatformTargetMatch (const char *kernel_target_name, const char *target_string) |
| Match a user specified target_string with kernel suported target name. More... | |
| void | tivxPlatformGetObjDescTableInfo (tivx_obj_desc_table_info_t *table_info) |
| Return shared memory info which holds the object descriptors. More... | |
| void | tivxPlatformGetLogRtShmInfo (void **shm_base, uint32_t *shm_size) |
| Return shared memory info which holds the run-time logger buffer. More... | |
| void | tivxPlatformSystemLock (vx_enum lock_id) |
| Take a system level lock. More... | |
| void | tivxPlatformSystemUnlock (vx_enum lock_id) |
| Release system level lock. | |
| uint64_t | tivxPlatformGetTimeInUsecs (void) |
| Get the time in micro seconds. | |
| vx_status | tivxPlatformInit (void) |
| Init Platform module. | |
| void | tivxPlatformDeInit (void) |
| DeInit Platform module. | |
| void | tivxPlatformPrintf (const char *format) |
| Print given string. | |
| void | tivxPlatformCreateTargets (void) |
| Function to set the target configuration. More... | |
| void | tivxPlatformDeleteTargets (void) |
| Function to destroy created targets. | |
| void | tivxPlatformActivate (void) |
| Utility function to enable Platform specific things Currently Used for EVE algorithm to enable EDMA. | |
| void | tivxPlatformDeactivate (void) |
| Utility function to disable Platform specific things Currently Used for EVE algorithm to disable EDMA. | |
| void * | tivxPlatformGetDmaObj (void) |
| Utility function to get Platform specific things Used to obtain DMA handle. | |
Types of system level locks.
Definition at line 85 of file tivx_platform.h.
| vx_enum tivxPlatformGetTargetId | ( | const char * | target_name | ) |
Convert a target name to a specific target ID.
| target_name | [in] Target name |
| void tivxPlatformGetTargetName | ( | vx_enum | target_id, |
| char * | target_name | ||
| ) |
Convert a specific target ID to a target name.
| target_id | [in] Target ID |
| target_name | [out] Target name |
| vx_bool tivxPlatformTargetMatch | ( | const char * | kernel_target_name, |
| const char * | target_string | ||
| ) |
Match a user specified target_string with kernel suported target name.
| kernel_target_name | [in] Kernel supported target name |
| target_string | [in] user specified target string |
| void tivxPlatformGetObjDescTableInfo | ( | tivx_obj_desc_table_info_t * | table_info | ) |
Return shared memory info which holds the object descriptors.
This is platform APIs since method of specifying shared memory, number of object descriptors is platform dependant
| void tivxPlatformGetLogRtShmInfo | ( | void ** | shm_base, |
| uint32_t * | shm_size | ||
| ) |
Return shared memory info which holds the run-time logger buffer.
This is platform APIs since method of specifying shared memory, is platform dependant
| void tivxPlatformSystemLock | ( | vx_enum | lock_id | ) |
Take a system level lock.
This locks is taken across all targets to mutual exclusion across targets
| void tivxPlatformCreateTargets | ( | void | ) |
Function to set the target configuration.
It creates target and adds it to the list of targets supported on each core.