2.1. Release Notes - 07_01_00

2.1.1. Introduction

This release notes provides important information that will assist you in using the PDK software package for the Jacinto family of devices. This document provides the product information and known issues that are specific to the PDK software package.

2.1.2. What’s New

ID Description Module Supported Platforms
PDK-5359 Support J7200 Platform COMMON J7200
PDK-2409 CSL-FL: Hyperflash Support CSL J7200
PDK-4928 Support Firewall control layer for TISCI features SCICLIENT J721E, J7200, AM65xx
PDK-7557 Support for UDMA SW Trigger Example UDMA J721E, J7200
PDK-5071 Support population of resource table by quering DMSC board config UDMA J721E
PDK-5687 Support virtual to physical address translation in DMAUtils UDMA J721E
PDK-5593 Support use case of MPU/Linux and MCU/Baremetal IPC J721E, J7200, AM65xx
PDK-6615 Support tone mapping LUT programation of outputs 2/3 VHWA LDC J721E
PDK-5666 Support run-time adding/removing of channels CSI-RX J721E
PDK-5528 SBL: xSPI Flash Boot Media Support SBL J7200
PDK-5530 SBL: boot both RTOS and HLOS images in SD/MMC bootmode SBL J721E, J7200
PDK-5531 SBL: boot SPL/U-boot on Cortex-A cores in SD/MMC bootmode SBL J721E, J7200
PDK-5603 SBL: boot both RTOS and HLOS images in OSPI/xSPI bootmode SBL J721E, J7200
PDK-5627 SBL: boot SPL/U-boot on Cortex-A cores in OSPI/xSPI bootmode SBL J721E, J7200
PDK-6133 Safety Example: Watchdog Timer (WDT/RTI) Diagnostics J721E
PDK-5911 Safety Example: Error Correcting Code (ECC) Diagnostics J721E
PDK-5910 Safety Example: MCU R5F - Error Signaling Module (ESM) Diagnostics J721E
PDK-5879 MSMC3.RAM-T1 - Software test of memory parity Diagnostics J721E
ETHFW-1626 Enet LLD - support for J721E and J7VCL Enet J721E, J7200
PDK-5853 Support for LP8764x(Hera) PMIC device PMIC J721E, J7200
PDK-5839 Support for PMIC Watchdog in trigger mode and Q&A mode PMIC J721E, J7200
PDK-5849 Support to execute runtime-BIST and to query Error Recovery Count PMIC J721E, J7200
PDK-5837 Support for NSLEEP configurations for Low-Power, Ultra low power PMIC J721E, J7200
PDK-5844 Support for Standby with CAN Wake-Up and RTC Wake-Up PMIC J721E, J7200
PDK-5841 Support to configure/readback of BUCK/LDO regulator voltages PMIC J721E, J7200
PDK-5833 Support to configure/readback of ESM_MCU/ESC_SoC error monitors PMIC J721E, J7200

2.1.3. Upgrade and Compatibility

This release introduces the new architecture for System firmware where the TI Foundational Security (TIFS) is running on the DMSC on J7200 and J721E devices and Power Management & Resource Management (collectively known as Device Management (DM)) runs as a library on the MCU1_0 R5F. For AM65xx device, the DM function continues to run on the DMSC. Refer individual sections below regarding the impact to each component.

2.1.3.1. Build and Packaging

  • The PDK package is now a separate package each platform, i.e. this package contains drivers required for Jacinto platform only.

  • Only the files applicable to a particular platform is packaged. This is to done to reduce the overall package size, remove unwanted files for users for better file/folder navigation and also to ensure that a file which is not applicable for a platform is not included by application un-intentionally

    • Due to this some of the application interface files may be missing from the package compared to last release. Users are advised to remove the inclusion of these files in their application for the respective platform builds

2.1.3.2. Memory Map and Linker Command

System Firmware architecture has been updated for J7200 and J721E devices to run Device Management services on the MCU1_0 R5F. For details, see Sciclient upgrade and compatibility information.

In order to support this new architecture, additional memory sections are reserved in MCU MSRAM for the boot and initialization sequence, and new data sections are introduced by the supporting libraries.

SoC-wide

A portion of the MCU SRAM is reserved for exchange of data between SBL and the Device Manager, summarized in the below table:

Address Size Purpose Persistence
0x41C8_0000 8 KB Hold the Board configuration passed between SPL/SBL and SCISERVER_APP Can be claimed once MCU1_0 app executes Sciclient_init on MCU1_0
0x41cf_fb00 1.25 KB Common header used in ROM combined image format as well. Can be claimed once MCU1_0 app executes Sciclient_init on MCU1_0

For more information on the purpose and implementation of these reserved regions, refer to Board configuration passing between SPL/SBL and MCU1_0 applications. Also, PDK common linker command file could be used as reference PDK_INSTALL_DIR/packages/ti/build/j721e/linker_r5.lds

MCU1_0 Applications

Linker configuration files for MCU1_0 applications must be updated to comprehend placement of additional sections introduced by the Device Manager implementation

  • Passing of the board configuration between SBL and the MCU1_0 application may optionally be replaced by referencing a local copy of the board configuration data structures within the Sciclient library. Regardless of which method for sending board configuration data, the .boardcfg_data section is defined by default for the placement of these structures in the application memory map.

Important

The .boardcfg_data section must be placed in SoC-internal SRAM if the local board configuration data structures are used instead of what is passed by SBL. Do not place this section in DDR.

  • MCU1_0 R5F applications are expected to co-host Device Management services which are implemented via the RM/PM HAL library. This library introduces additional data sections, which are free to be placed anywhere as required by the integrating application:
    • .const.devgroup.MAIN
    • .const.devgroup.MCU_WAKEUP
    • .const.devgroup.DMSC_INTERNAL
    • .bss.devgroup.MAIN
    • .bss.devgroup.MCU_WAKEUP
    • .bss.devgroup.DMSC_INTERNAL

2.1.3.3. OSPI Flash Memory Map

The default flash memory layout used by the SBL to load multicore application images has been updated in this release. It now uses the following flash address offsets:

Image Type Flash Offset Example Binary Name
SBL 0x0 OSPI/CUST SBL, E.g.: sbl_ospi_img_mcu1_0_release.tiimage
TIFS 0x80000 tifs.bin for GP device, or tifs-hs-enc.bin for HS device
App Image 0x100000 Application image, E.g.: udma_memcpy_testapp_mcu2_0_release.appimage
Optional: XIP bin 0x1C0000 XIP app binary, E.g.: can_profile_xip_app_mcu1_0_release.xer5f.bin

2.1.3.4. Sciclient

  • Sciclient supports the new split architecture for System Firmware, with TI Foundational Security (TIFS) running on the DMSC and the Device Management (DM) functions running on the MCU R5F

  • Sciserver
    • Runs on MCU R5F (mcu1_0) core
    • Processes the power management (PM) and resource mangement (RM) messages in DM on MCU R5F
    • Forwards processor boot control or firewall configuration to TIFS on DMSC
    • Forwards TIFS responses back to non-secure hosts for the above forwarded messages
  • RM/PM HAL
    • A library to process RM and PM messages
  • Sciclient library
    • Added sciclient_direct library for MCU R5F (mcu1_0) applications
    • Applications on other cores remain to use the sciclient library

Important

In cases where multiple-core application is being deployed on j721e or j7200 and mcu 10 is hosting an application. The mcu 10 application shall start Sciserver

Example : IPC examples supports ipc demo app on multiple cores (including mcu 10), it initializes sciserver on mcu 10 before initializing ipc application.

Please refer PDK_INSTALL_DIR/packages/ti/drv/ipc/examples/common/src/main_tirtos.c and function ipc_initSciclient () & Ipc_setupSciServer () for more details

2.1.3.5. Execution of apps with CCS

The steps to run applications with CCS has been updated. Refer Link for detailed steps.

2.1.3.6. SBL

  • The SBL provides support on J721E and J7200 for the new split architecture for System Firmware, with TI Foundational Security (TIFS) running on the DMSC and the Device Management (DM) functions running on the MCU R5F. Sciclient API requests for security related operations will continue to be sent to the DMSC, while other Sciclient API requests for the non-secure Resource Managment (RM) and Power Management (PM) operations will be handled directly on the MCU R5F.
  • The OSPI PHY on the SoC requires a PHY tuning procedure to be performed to ensure good stability and performance is achieved for the high-speed transfers performed when the PHY is enabled. The BOARD library linked in with the SBL handles this procedure as part of the SBL boot sequence. However, a PHY tuning data binary must be flashed to the start address of the last flash sector of the OSPI/xSPI device on the board. This data is used by the OSPI driver during the boot sequence for tuning the PHY.
  • HLOS + RTOS boot is now supported by the SBL, with new SBL build targets for support of HLOS (or U-boot) boot on the Cortex-A cores in the MAIN domain. MMC/SD boot and OSPI/xSPI flash boot options are supported.
  • Tooling is provided to created a “combined” .appimage file with the desired HLOS & RTOS images that the SBL can load, parse, and subsequently load & start on each of the remote cores that have been targeted to boot.

2.1.3.7. SYSBIOS Configuration

  • Main Domain R5F Timer
    • Updated to use DM Timers instance 6 & 7 of main domain for Main Domain R5F. By default SYSBIOS uses instance 12 & 13
    • DM Timers instances 9 to 20 are not powered on by default, requires to be explicitly powered on
    • Without this configuration, sysbios application would not be functional
  • The sysbios reserved interrupt number “0”
    • MCAN instance 0 in MCU and interrupt line 0 cannot used with default sysbios configuration
    • Recommend to re-configure sysbios to use a different interrupt number

2.1.3.8. UDMA

  • Update in Udma_RmInitPrms->startIrIntr and Udma_RmInitPrms->numIrIntr
    • Earlier this parameters referred to the core interrupt range.
    • Its updated to refer to IR Interrupt range for alligning with Sciclient BoardCfg RM.
  • Udma_eventUnregister for UDMA_EVENT_TYPE_RING / UDMA_EVENT_TYPE_DMA_COMPLETION will return failure when Ring Occupancy is non-zero.
    • This is to make sure that there is no resource leak, because unregistering these events will reset the ring.
    • All the unprocessed descriptors in the ring / processed descriptors returned to the ring, should be dequeued using Udma_ringFlushRaw / Udma_ringDequeueRaw before unregistering these events.

2.1.3.9. ENET

Low-level driver support for CPSW Ethernet peripherals has been migrated from CPSW LLD to Enet LLD. Enet LLD provides a unified interface for Ethernet peripherals available in TI processors, though this release currently supports only peripherals of the CPSW family, such as CPSW_2G, CPSW_5G and CPSW_9G.

Enet LLD supports the following devices and processing cores:

  • J721E device
    • CPSW_2G on MCU R5F (mcu1_0), Main R5F Core 1 (mcu2_1) and A72 core (mpu1_0).
    • CPSW_9G on Main R5F Core 0 (mcu2_0).
  • J7200 device
    • CPSW_2G on MCU R5F (mcu1_0), Main R5F Core 1 (mcu2_1) and A72 core (mpu1_0).
    • CPSW_5G on Main R5F Core 0 (mcu2_0).

There are similarities between Enet LLD and CPSW LLD top-level APIs as both provide IOCTL-based APIs for control and configuration path, and direct call APIs for data path.

CPSW LLD ENET LLD Comments
Cpsw_initParams() Enet_initCfg() Requires peripheral type and instance id
Cpsw_init() Enet_init()  
Cpsw_deinit() Enet_deinit() Requires peripheral inst id
Cpsw_open() Enet_open()  
Cpsw_close() Enet_close()  
Cpsw_ioctl() Enet_ioctl()  
Cpsw_periodicTick() Enet_periodicTick()  
CpswDma_initRxFlowParams() EnetDma_initRxChParams()  
CpswDma_pktInfoInit() EnetDma_initPktInfo()  
CpswDma_openRxFlow() EnetDma_openRxCh()  
CpswDma_closeRxFlow() EnetDma_closeRxCh()  
CpswDma_initTxChParams() EnetDma_initTxChParams()  
CpswDma_openTxCh() EnetDma_openTxCh()  
CpswDma_closeTxCh() EnetDma_closeTxCh()  
CpswDma_retrieveRxPackets() EnetDma_retrieveRxPktQ() EnetDma_retrieveRxPkt() Added new API for single packet reception
CpswDma_submitRxPackets() EnetDma_submitRxPktQ() EnetDma_submitRxPkt() Added new API for single packet reception
CpswDma_retrieveTxDonePackets() EnetDma_retrieveTxPktQ() EnetDma_retrieveTxPkt() Added new API for single packet transmission
CpswDma_submitTxReadyPackets() EnetDma_submitTxPktQ() EnetDma_submitTxPkt() Added new API for single packet transmission

The following API changes with respect to CPSW LLD are worth noting:

  • CPSW peripheral id was defined as a variable of type Cpsw_Type in CPSW LLD, as only Ethernet devices of the CPSW family were supported. Enet LLD defines the peripheral id as a combination of the peripheral type (Enet_Type) and the instance number.
  • MAC ports ids in CPSW LLD were 0-based (CPSW_MAC_PORT_0, CPSW_MAC_PORT_1 and so on), but Enet LLD has 1-based ids (ENET_MAC_PORT_1, ENET_MAC_PORT_2 and so on).
  • Enet LLD uses DMA RX channel as a generic term for the RX data direction. This refers to a UDMA RX flow in Jacinto 7 devices, but can refer to an actual DMA channel in other devices (i.e. CPDMA RX channel in TPR12).
  • Enet LLD provides DMA APIs to transfer a single packet, in addition to the packet queue APIs which were also supported in CPSW LLD. Single packet APIs should be used to reduce the overhead incurred if sending a single packet via packet queue APIs.
  • Enet DMA submit queue APIs (EnetDma_submitRxPktQ() and EnetDma_submitTxPktQ()) no longer require a queue for unused packets unlike the corresponding CPSW LLD APIs. In Enet LLD, the unused packets are passed back to the submit queue.

Enet LLD IOCTLs are grouped into generic and peripheral specific. Generic IOCTLs are common for different types of peripherals, and peripheral specific IOCTLs are applicable only to certain peripheral or family of peripherals. Please refer to the Enet LLD driver API Guide for further details on new APIs and IOCTLs.

A CPSW to Enet LLD migration document [LINK] and helper script is provided along with this release to facilitate the translation of CPSW LLD to Enet LLD APIs. The helper script can be found at PDK_INSTALL_DIR/packages/ti/drv/enet/docs/migration/cpswtoenet.txt.

2.1.3.10. PMIC

  • Initialize pmic core handle for PMIC LLD API has a parameter “pPmicConfigData” which is modified as “const Pmic_CoreCfg_t *pPmicConfigData” instead of “Pmic_CoreCfg_t *pPmicConfigData” struct type.

  • Modified pPmic_SubSysInfo structure member of Pmic_CoreHandle_s structure as const Pmic_DevSubSysInfo_t *pPmic_SubSysInfo instead of Pmic_DevSubSysInfo_t *pPmic_SubSysInfo.

  • Set Recovery Counter Configuration API
    • Has a parameter “pRecovCnt” which is modified as “Pmic_RecovCntCfg_t recovCntCfg” instead of “Pmic_RecovCntCfg_t *pRecovCnt”
    • Modified Pmic_RecovCntCfg_s sturture members as validParams and clrCnt instead of cfgType and clrVal respectively.
  • Get Recovery Counter Configuration API
    • Has a parameter “pRecovCntCfgVal” which is modified as “Pmic_RecovCntCfg_t *pRecovCntCfg” instead of “uint8_t *pRecovCntCfgVal”
  • Renamed the PMIC device specific sub folder name as tps6594x instead of tps65941 which is defined in the path “include/cfg” and also renamed the PMIC device specific file name as pmic_gpio_tps6594x.h instead of pmic_gpio_tps65941.h which is defined in the path “include/cfg/tps65941”
    • This results in include path change in PMIC GPIO Interface file as <cfg/tps6594x pmic_gpio_tps6594x.h> instead of <cfg/tps65941/pmic_gpio_tps65941.h>.
  • Added new member configuration type PMIC_NPWRON_CFG_POLARITY_VALID and PMIC_ENABLE_CFG_POLARITY_VALID for the validParams member of Pmic_GpioCfg_s structure. Also added shift values for the new member configuration type PMIC_NPWRON_CFG_POLARITY_VALID_SHIFT and PMIC_ENABLE_CFG_POLARITY_VALID_SHIFT

  • Removed Macro “PMIC_GPIO_PINFUNC_MAX” from PMIC GPIO Interface file

  • Modified Macros names of PMIC device type as “PMIC_DEV_LEO_TPS6594X” or “PMIC_DEV_HERA_LP8764X” instead of “PMIC_DEV_LEO_TPS6594” or “PMIC_DEV_HERA_LP8764” respectively

  • Pmic_GpioCfg_s structure
    • Modified Valid values of pinFunc member of the Pmic_GpioCfg_s structure as “Pmic_Tps6594xLeo_GpioPinFunc” (for TPS6594x Leo Device) or “Pmic_Lp8764xHera_GpioPinFunc” (for LP8764x Hera Device) instead of Pmic_GpioPinFunc
    • Modified Valid values of pullCtrl member of the Pmic_GpioCfg_s structure as “Pmic_GpioPinPullCtrl” instead of Pmic_Gpio_PU_PD_Sel
    • pinPolarity member of the Pmic_GpioCfg_s structure is valid for Enable Pin when PMIC_ENABLE_CFG_POLARITY_VALID bit is set
  • For all GPIO APIs
    • Has a parameter “pin” which is modified as “const uint8_t pin” instead of “uint8_t pin”.
    • Has a parameter “pin” whose valid values as Pmic_Tps6594xLeo_GpioPin(for TPS6594x Leo Device)/ Pmic_Lp8764xHera_GpioPin(for LP8764x Hera Device) instead of Pmic_GpioPin
  • PMIC GPIO set configuration API
    • Has a parameter “pGpioCfg” which is modified as “const Pmic_GpioCfg_t gpioCfg” instead of “Pmic_GpioCfg_t *pGpioCfg” struct type
    • Has a parameter “pinValue” which is modified as “const uint8_t pinValue” instead of “uint8_t pinValue”.
  • PMIC GPIO interrupt configuration API
    • Has a parameter “maskPol” which is modified as “const uint8_t maskPol” instead of “uint8_t maskPol”.
    • Has a parameter “intrType” which is modified as “const uint8_t intrType” instead of “uint8_t intrType”.
    • Added a new value for the “intrType” parameter as “PMIC_GPIO_FALL_RISE_INTERRUPT” and PMIC_GPIO_DISABLE_INTERRUPT macro value is changed as “2” instead of “3”
  • Added new API to configure NPwron/Enable Pin - Pmic_gpioSetNPwronEnablePinConfiguration instead of Pmic_gpioSetConfiguration

  • Added new API to readback NPwron/Enable Pin - Pmic_gpioGetNPwronEnablePinConfiguration instead of Pmic_gpioGetConfiguration

  • Pmic_RtcDate_s Structure
    • Renamed “week” member as “weekday” of the Pmic_RtcDate_s structure
    • Modified validParams member configuration type as PMIC_RTC_DATE_CFG_WEEKDAY_VALID instead of PMIC_RTC_DATE_CFG_WEEK_VALID of Pmic_RtcDate_s structure. Also modified shift values for the validParams member configuration type as PMIC_RTC_DATE_CFG_WEEKDAY_VALID_SHIFT instead of PMIC_RTC_DATE_CFG_WEEK_VALID_SHIFT
  • Removed the below defined Macros from PMIC RTC Interface file

    PMIC_RTC_AUTO_COMP_ON, PMIC_RTC_MINUTE_SEC_MAX, PMIC_RTC_12HFMT_HR_MIN, PMIC_RTC_12HFMT_HR_MAX, PMIC_RTC_24HFMT_HR_MAX, PMIC_RTC_DAY_MIN, PMIC_RTC_YEAR_MIN, PMIC_RTC_YEAR_MAX, PMIC_RTC_NLPY_FEB_MNTH_DAY_MAX, PMIC_RTC_LPY_FEB_MNTH_DAY_MAX, PMIC_RTC_MNTH_DAY_MAX_30, PMIC_RTC_MNTH_DAY_MAX_31, PMIC_RTC_CONVERT_4BIT_MSB_TO_DEC, PMIC_RTC_EXTRACT_YEAR_DECIMAL_0_99, PMIC_RTC_OPS_FOR_RTC, PMIC_RTC_OPS_FOR_ALARM

  • PMIC RTC Set the alarm interrupt configurations API
    • Renamed the API Pmic_rtcSetAlarmIntr as Pmic_rtcSetAlarmInfo
    • Has a parameter pTimeCfg which is modified as “const Pmic_RtcTime_t timeCfg” instead of “Pmic_RtcTime_t *pTimeCfg”.
    • Has a parameter pDateCfg which is modified as “const Pmic_RtcDate_t dateCfg” instead of “Pmic_RtcDate_t *pDateCfg”
  • PMIC RTC Get the alarm interrupt configurations API
    • Renamed the API Pmic_rtcGetAlarmIntr as Pmic_rtcGetAlarmInfo
  • PMIC RTC Set the timer interrupt configurations API
    • Renamed the API Pmic_rtcSetTimerIntr as Pmic_rtcSetTimerPeriod
    • Has a parameter timerPeriod which is modified as “const uint8_t timerPeriod” instead of “uint8_t *timerPeriod”
  • PMIC RTC Get the timer interrupt configurations API
    • Renamed the API Pmic_rtcGetTimerIntr to Pmic_rtcGetTimerPeriod
  • PMIC RTC Set date and time function API
    • Has a parameter pTimeCfg which is modified as “const Pmic_RtcTime_t timeCfg” instead of “Pmic_RtcTime_t *pTimeCfg”.
    • Has a parameter pDateCfg which is modified as “const Pmic_RtcDate_t dateCfg” instead of “Pmic_RtcDate_t *pDateCfg”.
  • PMIC RTC Set frequency compensation API
    • Has a parameter compensation which is modified as “const uint16_t compensation” instead of “uint16_t *compensation”.
  • PMIC RTC Enable/Disable API
    • Modified enableRtc parameter datatype as bool instead of 8 bit unsigned integer.
  • Removed these files included in PMIC IRQ Interface file
    • pmic_core_priv.h, pmic_irq_tps65941_priv.h, pmic_irq_priv.h
  • Removed IRQ relates macros as defined below
    • Pmic_IrqID such as PMIC_IRQID, PMIC_IRQID_L1REG, PMIC_IRQID_L2REG, PMIC_IRQID_BITMASK
    • Pmic_InterruptId such as PMIC_INT_ID_BUCK1_OV, PMIC_INT_ID_BUCK1_UV etc.,
    • Pmic_IrqInterruptMask such as PMIC_IRQ_MASK_BUCK1_2_MASK, PMIC_IRQ_BUCK2_ILIM_MASK etc.,
  • PMIC IRQ Read Error Status API
    • Has a parameter pErrStat which is modified as “Pmic_IrqStatus_t *pErrStat” instead of “uint16_t *pErrStat”.
    • Added Pmic_IrqStatus_s structure which stores all available interrupts using bit fields.
    • Has a parameter clearIRQ which is modified as “const bool clearIRQ” instead of “bool clearIRQ”.
  • PMIC IRQ clear Error Status API
    • Has a parameter errStat which is modified as “const uint8_t irqNum” instead of “const uint32_t errStat” irqNum valid values as Pmic_tps6594x_IrqNum (for TPS6594x Leo Device)/Pmic_lp8764x_IrqNum(for LP8764x Hera Device)/Pmic_IrqNum(for all interrupts except gpio)
  • PMIC IRQ MASK/UNMASK API
    • Has a parameter interruptMask which is modified as “const uint8_t irqNum” instead of “uint16_t interruptMask”. irqNum valid values as Pmic_tps6594x_IrqNum (for TPS6594x Leo Device)/Pmic_lp8764x_IrqNum(for LP8764x Hera Device)/Pmic_IrqNum(for all interrupts except gpio)
    • Has a parameter mask which is modified as “const bool mask” instead of “bool mask”.
  • Added new API to mask/unmask GPIO interrupts - Pmic_irqGpioMaskIntr instead of Pmic_irqMaskIntr

  • Added New Macros values related to appropriate error codes of PMIC APIs

    Macro Value Description
    PMIC_ST_ERR_INV_WDG_ANSWER (-((int32_t)23)) Error Code for Invalid Watchdog Answer
    PMIC_ST_ERR_WDG_EARLY_ANSWER (-((int32_t)24)) Error Code for Watchdog early Answer
    PMIC_ST_ERR_FAIL (-((int32_t)32)) Error Code for any other failures
    PMIC_ST_ERR_ESM_STARTED (-((int32_t)33)) Error Code for ESM in Start State
    PMIC_ST_ERR_INV_ESM_VAL (-((int32_t)34)) Error Code for Invalid ESM delay1, delay2, HMAX, HMIN, LMAX and LMIN values
    PMIC_ST_WARN_INV_DEVICE_ID (-((int32_t)35)) Warning Code for Device ID mismatch
  • Modified Macros values related to appropriate error code of PMIC APIs.

    Old Macro Old Value New Value
    PMIC_ST_ERR_INV_VOLTAGE (-((int32_t)2)) (-((int32_t)14))
    PMIC_ST_ERR_INV_REGULATOR (-((int32_t)3)) (-((int32_t)15))
    PMIC_ST_ERR_I2C_COMM_FAIL (-((int32_t)4)) (-((int32_t)8))
    PMIC_ST_ERR_SPI_COMM_FAIL (-((int32_t)5)) (-((int32_t)9))
    PMIC_ST_ERR_COMM_INTF_INIT_FAIL (-((int32_t)6)) (-((int32_t)12))
    PMIC_ST_ERR_INV_GPIO (-((int32_t)7)) (-((int32_t)18))
    PMIC_ST_ERR_INV_GPIO_FUNC (-((int32_t)8)) (-((int32_t)19))
    PMIC_ST_ERR_INV_GPIO_LINE_PARAMS (-((int32_t)9)) (-((int32_t)20))
    PMIC_ST_ERR_NULL_PARAM (-((int32_t)10)) (-((int32_t)2))
    PMIC_ST_ERR_INV_PARAM (-((int32_t)11)) (-((int32_t)3))
    PMIC_ST_ERR_INV_ESM_TARGET (-((int32_t)12)) (-((int32_t)25))
    PMIC_ST_ERR_INV_ESM_MODE (-((int32_t)13)) (-((int32_t)26))
    PMIC_ST_ERR_INTF_SETUP_FAILED (-((int32_t)14)) (-((int32_t)11))
    PMIC_ST_ERR_INV_DEVICE (-((int32_t)15)) (-((int32_t)4))
    PMIC_ST_ERR_PIN_NOT_GPIO (-((int32_t)16)) (-((int32_t)21))
    PMIC_ST_ERR_INV_WDG_MODE (-((int32_t)17)) Removed
    PMIC_ST_ERR_INV_WDG_WINDOW (-((int32_t)18)) (-((int32_t)22))
    PMIC_ST_ERR_INV_TEMP_THRESHOLD (-((int32_t)19)) (-((int32_t)17))
    PMIC_ST_ERR_INV_PGOOD_LEVEL (-((int32_t)20)) (-((int32_t)16))
    PMIC_ST_ERR_INV_INT (-((int32_t)21)) (-((int32_t)27))
    PMIC_ST_ERR_CLEAR_INT_FAILED (-((int32_t)22)) (-((int32_t)28))
    PMIC_ST_ERR_UNINIT (-((int32_t)23)) (-((int32_t)13))
    PMIC_ST_ERR_DATA_IO_CRC (-((int32_t)24)) (-((int32_t)10))
    PMIC_ST_ERR_NULL_FPTR (-((int32_t)25)) (-((int32_t)5))
    PMIC_ST_ERR_INV_TIME (-((int32_t)26)) (-((int32_t)29))
    PMIC_ST_ERR_INV_DATE (-((int32_t)27)) (-((int32_t)30))
    PMIC_ST_ERR_RTC_STOP_FAIL (-((int32_t)28)) (-((int32_t)31))
    PMIC_ST_ERR_INV_ANSWER_COUNT (-((int32_t)29)) Removed
    PMIC_ST_ERR_INV_SUBSYSTEM (-((int32_t)30)) (-((int32_t)6))
    PMIC_ST_ERR_INSUFFICIENT_CFG (-((int32_t)31)) (-((int32_t)7))

2.1.4. Device Support

  • J721E EVM, J721E-HS EVM (BOARD=j721e_evm)

2.1.5. Validation Information

This release is validated on J7200 EVM for the applicable components. For details on the validated examples refer to the platform specific test report present in PDK_INSTALL_DIR/docs/test_report folder.

2.1.6. Tool Chain Information

Refer to SDK level documentation for Tool Chain and dependent component version used to validate this release.

2.1.7. Fixed Issues

ID Head Line Module Affected Versions Affected Platforms
PDK-7479 Luma and Chroma components are not properly stored CSI2RX, CSI2TX 07.00.00 J721E
PDK-6852 CSITX does not work in less than 4 lane mode CSI2TX 07.00.00 J721E
PDK-6762 UART test fails for MCU 1_0 CSL 07.00.00 AM65xx, J721E
PDK-6925 R5 cache function uses incorrect cache line size CSL 07.00.00 J721E, J7200, AM65xx
PDK-8203 DCC source update not working CSL 07.00.00 J721E, J7200, AM65xx
PDK-6839 CSL_serdesEnableLanes does not configure torrent SERDES CSL 07.00.00 J721E
PDK-7573 IPG setting for ICSSG does not take effect for 2nd port EMAC 07.00.00 AM65xx
PDK-6734 Driver updates to support wire clock feature in TX CFG EMAC 07.00.00 AM65xx
PDK-7536 C6x: ipc examples: Trace buffer contents remain in the Cache upon a crash IPC 07.00.00 J721E
PDK-7625 Message reception is delayed if sent to core before it is booted IPC 07.00.00 J721E
PDK-8103 TimerP_getTimeInUsecs API return wrong time value in Bare-metal OSAL 07.00.00 J721E
PDK-5258 OSPI PHY Mode Temperature Sensitivity OSPI 06.02.00 J721E
PDK-7402 Typo in ICSS instance enums in PRUSS LLD PRUSS 07.00.00 J721E
PDK-7091 AM65 pruicss_intc.c interrupt initialization sequence doesn’t protect spurious interrupt PRUSS 07.00.00 AM65xx
PDK-7045 Unable to set USE_DKEK flag in SA2UL security context SA2UL 07.00.00 J721E, AM65xx
PRSDK-5448 SBL boot from MMCSD fails intermittently SBL 05.02.00 AM65xx
PDK-8189 SBL doesn’t allow an external app to use OSPI with DMA SBL 07.00.00 J721E
PDK-7627 Multi-Stage bootloading fails on HS device SBL 07.00.00 J721E
PRSDK-5626 OSPI Read using UDMA fails on AM65x HS devices. SBL 05.03.00 AM65xx
PRSDK-6382 SBL: R5F: Core 1 boot is not working with unsigned binary with ipc images SBL 06.01.00 AM65xx
PDK-6980 Inconsistent naming of TISCI defines in sciclient SCICLIENT 07.00.00 J721E, J7200, AM65xx
PDK-7120 Incorrect Error interrupt registration in scalar VHWA MSC 07.00.00 J721E
PDK-7024 Incorrect max size of the LSC table VHWA VISS 07.00.00 J721E
PDK-6800 Watchdog timer diagnostic test fails DIAG 07.00.00 AM65xx
PRSDK-8607 Board_init(SBL_PLL_INIT) is configuring PLL directly without going through SYSFW. BOARD 06.03.00 AM65xx
PRSDK-7891 CPSW RGMII diagnostic test failure BOARD 06.01.00 J721E

2.1.8. Known Issues

ID Head Line Module Reported in Release Affected Platforms Impact Workaround in this release
PDK-5224. Active DP -> HDMI adapter doesn’t work DSS 00.09.01 J721E DP to HDMI adapter for display cannot be used. None
PDK-5040. Display stops working if two pipelines are started back to back DSS 06.02.00 J721E None, if the workaround is in place. Wait for a frame to go out from a pipeline before starting the next one
PDK-6992. Display flickers for BT601 output format DSS 07.00.00 J721E   None
PDK-8320 ICSS V1 CSL not up to date with ICSSG CSL 07.00.00 J721E, AM65xx None Patch available. Will be included in next release
PDK-6975. Pulsar (R5F) : High priority interrupt is missed by VIM CSL, OSAL 07.00.00 J721E, J7200, AM65xx Baremetal implementation is pending Use SYSBIOS instead of baremetal
PDK-6649. Timer osal - noos - Timer delete doesn’t “free” timer OSAL 06.02.00 J721E Resource leak if create/delete called in a loop. But typically this is not done for Timer. Use the same timer in the application without create/deleting multiple times
PDK-6534. Timer osal - noos - Timer should be reset first before registering interrupts OSAL 06.02.00 J721E None if the workaround is in place Reset the timer before using
PDK-6758. pcie qos examples fails for 2 lane configuration PCIE 07.00.00 AM65xx None None
PRSDK-8036 PCIE-0: Intermittent failures during Gen 3 mode on AM65x PG2.0 PCIE 06.02.00 AM65xx None None
PDK-8407. J721E: MCU Timer 0 is not usable from application (sysbios) with SBL OSAL, SBL 07.01.00 J721E None Use any other timer
PDK-8586 Early CAN response measurement is beyond 50 ms for J721E SBL 07.01.00 J721E   None
PDK-8300. UDMA MCU NAVSS Channel Num 5 is not functional, when booting the application using the SBL bootloader. UDMA 07.01.00 J721E Low Impact. UDMA MCU NAVSS Channel 5 can’t be used when booting the application using the SBL bootloader. Use any other channel. In the defaultBoardCfg Channel no. 5 is not used. The issue will be seen only when the boardcfg is updated to use channel 5.
PDK-6789. MCU/Main NAVSS UDMA memcpy from L2SRAM fails UDMA 07.00.00 J721E Transfer works fine when source buffer, destination buffer and TRPD buffers are in L2SRAM. The issue happens only when the ring memory is in L2SRAM location Use ring memory from non-L2SRAM location
PDK-5228. Output mismatch when each region requiring 3 TRs VHWA 01.00.00 J721E In multi-region mode with more then 3 TR per region can’t be used In multi-region mode for each region less than 3 TR should be used
PDK-5226. DOF generated wrong output with SOF if pixel in all row are not enabled VHWA 01.00.00, 00.09.01 J721E When using the SOF if the Paxel rows without any pixel enabled is not in consecutive pair with lead to lead to output mismatch This issue is due to shift in flowvector out buffer. While generating the SOF binary map make sure that Paxel rows without any pixel enabled should be in consecutive pair
PDK-5217. VPAC VISS driver doesn’t support several valid mux combinations for outputs VHWA 01.00.00, 00.09.01 J721E VISS output with Chroma only and one of the RGB component enabled may not work Enable YUV420 instead of Chroma only while using RGB component
PDK-7048. Master Slave: Data corruption in mode 0 McSPI 07.01.00 J7200 None Most likely EVM looback routing issue. Debug pending
ETH-1534. [CPSW] Packet drop with QSGMII ports IPerf Enet 06.02.00 J721E, J7200 None None
ETH-1670. mcu2_1: loopback: Test fails to setup interrupts in iteration 2 Enet 07.01.00 J721E None Avoid restarting Enet LLD on J721E mcu2_1 core
PDK-6742. McASP regression test app some tests are failing McASP 07.00.00 AM65xx The issue is most likely a application configuration None
PRSDK-5074 McASP driver hangs with small buffer size McASP 05.01.00 J721E, AM65xx None Use packet size 32 samples or greater
PDK-8166. MMCSD read/write failure with 1.8V MMCSD 07.00.00 AM65xx    
PDK-8537. Sciclient_rmIrqRelease API is failing SCICLIENT 07.01.00 J721E    
PDK-8502 Uniflash flash programmer failure in DMA mode BOARD 07.01.00 J721E, AM65xx    
PDK-8311. Recent DDR config update to 4266 MT/s causing DDR memory failures on some boards BOARD 07.01.00 J721E Occational failures seen. Restart should work Issue seen with unqualified sample. Replace sample
PDK-6549. MCU2 core diagnostic tests not running through sbl BOARD 07.00.00 J721E None Use CCS/JTAG to run the tests
PDK-6548. Display port (eDP) diagnostic test failure BOARD 07.00.00 J721E None Use display sample application
PDK-6707. PCIe diagnostic test failure BOARD 07.00.00 AM65xx None Use PCIe driver sample application
PDK-8131 PMIC: Asynchronous Interrupt tests failure on Main domain R5 Cores BOARD 07.01.00 J7200 None Use Polled mode
PDK-8577 PMIC: Asynchronous Interrupt tests failure on Main domain R5 Cores and mcu1_1 core BOARD 07.01.00 J721E None Use Polled mode

2.1.9. Limitations

  • Active DP -> HDMI adapter doesn’t work. As a workaround use the display that supports Active DP
  • C7x TI RTOS : Task stack size shall be multiple of 16 KB (size less than 16 KB leads to unexpected behavior)