8. Frequently Asked QuestionsΒΆ
- 8.1. FAQ - Common
- 8.2. FAQ - CAN
- 8.3. FAQ - FVID2
- 8.4. FAQ - Why Vectors should be copied to ATCM (CCS)
- 8.5. FAQ - C7x : Steps to switch C7x SysBIOS application from secure mode to non-secure mode
- 8.5.1. Introduction
- 8.5.2. Step 1: SysBIOS config file changes to enable boot to non-secure
- 8.5.3. Step 2: Linker command file changes
- 8.5.4. Step 3: MMU initialization to setup secure and non-secure MMU tables
- 8.5.5. Step 4: CLEC initialization to allow non-secure mode access
- 8.5.6. Step 5: Cache initialization to partition L1/L2 as cache vs RAM
- 8.5.7. Step 6: Sciclient init to use non-secure mode
- 8.5.8. Step 7: Build and run
- 8.6. FAQ - Used Resources - Interrupt
- 8.6.1. J721E
- 8.6.1.1. MPU
- 8.6.1.2. MCU 10 (MCU Domain)
- 8.6.1.3. MCU 11 (MCU Domain)
- 8.6.1.4. MCU 11 (MCU Domain)
- 8.6.1.5. MCU 20 (Main Domain)
- 8.6.1.6. MCU 21 (Main Domain)
- 8.6.1.7. MCU 30 (Main Domain)
- 8.6.1.8. MCU 31 (Main Domain)
- 8.6.1.9. C66x 1 (Main Domain)
- 8.6.1.10. C66x 2 (Main Domain)
- 8.6.1.11. C7x 1 (Main Domain)
- 8.6.1. J721E
- 8.7. FAQ - Supported Cores by example applications