![]() |
PDK API Guide for J721E
|
DP83867 PHY configuration parameters.
Data Fields | |
| bool | txClkShiftEn |
| bool | rxClkShiftEn |
| uint32_t | txDelayInPs |
| uint32_t | rxDelayInPs |
| uint8_t | txFifoDepth |
| uint32_t | impedanceInMilliOhms |
| Dp83867_Gpio0Mode | gpio0Mode |
| Dp83867_Gpio1Mode | gpio1Mode |
| Dp83867_LedMode | ledMode [DP83867_LED_NUM] |
| bool Dp83867_Cfg::txClkShiftEn |
Enable TX clock shift
| bool Dp83867_Cfg::rxClkShiftEn |
Enable RX clock shift
| uint32_t Dp83867_Cfg::txDelayInPs |
TX delay value
| uint32_t Dp83867_Cfg::rxDelayInPs |
RX delay value
| uint8_t Dp83867_Cfg::txFifoDepth |
TX FIFO depth
| uint32_t Dp83867_Cfg::impedanceInMilliOhms |
Output impedance in milli-ohms. Ranging from 35 to 70 ohms in steps of 1.129 ohms
| Dp83867_Gpio0Mode Dp83867_Cfg::gpio0Mode |
Mux mode of the GPIO_0 pin
| Dp83867_Gpio1Mode Dp83867_Cfg::gpio1Mode |
Mux mode of the GPIO_1 pin
| Dp83867_LedMode Dp83867_Cfg::ledMode[DP83867_LED_NUM] |
LED mode (source) configuration