![]() |
MCUSW
|
The figure below depicts the AUTOSAR layered architecture as 3 distinct layers, Application, Runtime Environment (RTE) and Basic Software (BSW). The BSW is further divided into 4 layers, Services, Electronic Control Unit Abstraction, MicroController Abstraction (MCAL) and Complex Drivers.
MCAL is the lowest abstraction layer of the Basic Software. It contains software modules that interact with the Microcontroller and its internal peripherals directly. Wdg driver is part of the Microcontroller Drivers (block, shown above). Below shows the position of the Wdg driver in the AUTOSAR Architecture.
RTI(Real Time Interrupt) module supports three functional modes Counter mode, Capture mode & Windowed watchdog timer mode. Only Windowed watchdog timer mode is used to meet AUTOSAR WDG requirements.
The digital windowed watchdog generates an interrupt after a programmable period, if trigger is not serviced in the allowed time frame. TDA4x, DRA80x class of devices supports windowed watchdog timer where key can be only written in the configured window programmed through software. The watchdog opens a configurable time window in which it must be serviced. Any attempt to service the watchdog outside this time window, or a failure to service the watchdog in this time window, will cause the watchdog to generate a NMI interrupt.
Refer section (References) for more details on watchdog operation.
| Sl No | Specification | Comment / Link |
|---|---|---|
| 1 | AUTOSAR 4.3.1 | AUTOSAR Specification for WDG Driver Intranet Link |
| 2 | DRA80x and TDA4x TRM | Technical Reference Manual, DRA80X, TDA4X Watchdog modules is detailed |
| 3 | BSW General Requirements / Coding guidelines | Intranet Link |
| 4 | Software Product Specification (SPS) | Intranet Link Requirements are derived from 1 |
The Wdg driver shall implement as per requirements detailed in 1, 3 and 4. It’s recommended to refer 1 for clarification.
Below listed are some of the key features that are supported
| Design ID | DES_WDG_001 |
| Requirements Covered | MCAL-955, MCAL-920, MCAL-921, MCAL-922, MCAL-923, MCAL-925, MCAL-929, MCAL-930, MCAL-932, MCAL-933, MCAL-937, MCAL-938, MCAL-939, MCAL-942, MCAL-947, MCAL-980, MCAL-945, MCAL-1056, MCAL-2572, MCAL-4472 |
| Design ID | DES_WDG_002 |
| Non Requirements | MCAL-2566, MCAL-2568, MCAL-2570, MCAL-2574, MCAL-2583, MCAL-2584, MCAL-2585, MCAL-2586, MCAL-2588, MCAL-2600, MCAL-2611, MCAL-2612, MCAL-2613, MCAL-2614, MCAL-2615, MCAL-2616, MCAL-2617, MCAL-2618, MCAL-2619, MCAL-2620, MCAL-2621, MCAL-2634 |
Below listed are assumed to be valid for this design/implementation, exceptions and other deviations are listed for each explicitly. Care should be taken to ensure these assumptions are addressed.
Note that assumption 1 and 2 are specified by AUTOSAR WDG specification and 3 and 4 are device specific assumption.
Some of the critical constraints of this design are listed below
The Digital Watchdog Timer(DWT) generates reset after a programmable period, if not serviced within that period. In DWT, time-out boundary is configurable.In DWWD, along with configurable time-out boundary, the start time boundary is also configurable. The DWWD can generate Reset or Interrupt, if not serviced within window(Open Window) defined by start time and time-out boundary. Also the DWWD can generate Reset or Interrupt if serviced outside Open Window (i.e within Closed Window). Generation of Reset or Interrupt depends on the DWWD Reaction configuration.
DWWD Down Counter Overview :
Upper 12 bit part of the down counter is configurable and
remaining 13 bit are always 1.
Minimum possible time-out value is 2^13 RTI clock cycles.
Maximum possible time-out value is 2^25 RTI clock cycles.
Example :
The expiration time of the DWD Down Counter can be determined with following equation:
texp= (RTI_DWDPRLD + 1) x 2^13 / RTI_FCLK
where RTI_DWDPRLD(12 bit) = 0...4095 and RTI_FCLK is RTI functional frequency.
RTI_FCLK : 32kHz
12 bit preload value : 0x004
25 bit preload value : 0x0009FFF
time-out value(in RTI clock cycles) : 40959.
time-out value(in seconds) : (40959 + 1) / 32000 = 1.28 seconds.
DWWD Window Sizes Overview :
(timeout value),(timeout value - 1),(timeout value - 2),........................3 2 1 0
(100%)|___________________________Open Window_________________________|
(50%)| Closed Window |_________________Open Window__ |
(25%)| Closed Window |___OW________|
(12.5%)| Closed Window |__OW__|
(6.25%)| Closed Window |_OW_|
(3.125%)| Closed Window |OW|
As detailed in specification of 1, Driver will be in one of the following states.
The directory structure is as depicted in figures below, the source files can be categorized under “Driver Implementation” and “Example Application”
Driver Implemented by
Example Application
| Design ID | DES_WDG_003 |
| Requirements Covered | MCAL-2567, MCAL-2569 |
The AUTOSAR WDG Driver Specification details mandatory parameters that shall be configurable via the configurator. Please refer section 10 of 1
| Design ID | DES_WDG_004 |
| Requirements Covered | MCAL-2544, MCAL-2545, MCAL-2546, MCAL-2547, MCAL-2548, MCAL-2549, MCAL-2550, MCAL-2552, MCAL-2553, MCAL-2554, MCAL-2555, MCAL-2556, MCAL-2558, MCAL-2559, MCAL-2560, MCAL-2561, MCAL-2562, MCAL-2563, MCAL-2564, MCAL-2565, MCAL-2557, MCAL-2551, MCAL-2571 |
Following lists this design’s specific configurable parameters
| Parameter | Usage comment |
|---|---|
| WdgReaction | Watchdog reaction for timer expiration or incorrect service.0x5 = This is the default value. The windowed watchdog will cause a reset if the watchdog is serviced outside the time window defined by the configuration, or if the watchdog is not serviced at all. 0xA = The windowed watchdog will generate a non-maskable interrupt to the CPU if the watchdog is serviced outside the time window defined by the configuration, or if the watchdog is not serviced at all. Writing any other value will cause a system reset if the watchdog is serviced outside the time window. |
| WdgWindowSize | Digital Windowed Watchdog Window Size. Selecting 100% enables standard watchdog (not windowed). WWDSIZE: 0x00000050 = 50%, WWDSIZE: 0x00000500 = 25%, WWDSIZE: 0x00005000 = 12.5%, WWDSIZE: 0x00050000 = 6.25%, WWDSIZE: 0x00500000 = 3.125%, WWDSIZE: Any other value = 3.125% |
| WdgTimeoutValue | Watchdog timeout period in milli seconds.Watchdog generates a non-maskable interrupt to the CPU if the watchdog is serviced after this timeout period. |
| WdgDeviceVariant | Select SOC (DRA80X) variant. |
| WdgInstanceId | Selects Watchdog HW instance id. |
| WdgRtiFrequency | RTI Clock Frequency (Hz) used to calculate preload value during init time. |
| WdgRegisterReadbackApi | Compile switch to enable / disable the Critical Registers Readback API |
The driver shall support all variants VARIANT-PRE-COMPILE, VARIANT-LINK-TIME and VARIANT-POST-BUILD
| Design ID | DES_WDG_005 |
| Requirements Covered | MCAL-2635, MCAL-2636, MCAL-2637, MCAL-2638, MCAL-2639, MCAL-2640, MCAL-2642 |
In addition to dependencies listed in section 5 of 1, WDG driver shall depend on these modules to meet the required functionality. WDG uses RTI module present in the device to meet the required functionality.
This peripheral also requires 2 different clock to be operational, namely ICLK and FCLK.
There is no direct reset signal generation from watchdog when it expires instead it generates an ESM interrupt. ESM module will signal ESM pin error and then external controller resets the SOC.
| Design ID | DES_WDG_006 |
| Requirements Covered | MCAL-2651, MCAL-2653 |
Errors are classified in two categories, development error and runtime / production error.
| Type of Error | Related Error code | Value (Hex) |
| API service used in wrong context (e.g. module not initialized). | WDG_E_DRIVER_STATE | 0x10 |
| API service called with wrong / inconsistent parameter(s) | WDG_E_PARAM_MODE | 0x11 |
| API service called with wrong / inconsistent parameter(s) | WDG_E_PARAM_CONFIG | 0x12 |
| The passed timeout value is higher than the maximum timeout value | WDG_E_PARAM_TIMEOUT | 0x13 |
| API is called with wrong pointer value (e.g. NULL pointer) | WDG_E_PARAM_POINTER | 0x14 |
| Invalid configuration set selection | WDG_E_INIT_FAILED | 0x15 |
The detection of development errors is configurable (ON / OFF) at pre-compile time. The switch WdgDevErrorDetect will enable or disable the detection of all development errors.
All detected development errors are reported via Det_ReportError service of the Development Error Tracer (DET).
The following runtime/production errors shall be detectable by Wdg driver.
| Type of Error | Related Error code | Value (Hex) |
| Setting a watchdog mode failed (during initialization or mode switch). | WDG_E_MODE_FAILED | Defined By Integrator |
| Initialization or watchdog mode switch failed because it would disable the watchdog though this is not allowed in this configuration | WDG_E_DISABLE_REJECTED | Defined By Integrator |
All detected run time errors shall be reported via Dem_ReportErrorStatus() service of the Diagnostic Event Manager (DEM).
| Design ID | DES_WDG_008 |
| Requirements Covered | MCAL-2630, MCAL-2576, MCAL-2577, MCAL-2578, MCAL-2579, MCAL-2580, MCAL-2581, MCAL-2582 |
| Design ID | DES_WDG_009 |
| Requirements Covered | MCAL-2645 |
| Design ID | DES_WDG_010 |
| Requirements Covered | MCAL-2646 |
The detailed API and interface description is available as part of 1 & 4. This section describes the API supported by the MCAL driver and the requirements covered by each of the API.
The sections below lists some of key data structures that shall be implemented and used in driver implementation
Used to define watchdog hardware specific parameters per instance and the values of these are expected to be populated by configurator.
| Type | Variable Name | Comments |
|---|---|---|
| uint32 | reaction | Reaction type: 0x5 - This value causes a reset if the watchdog is serviced outside the time window defined by the configuration, or if the watchdog is not serviced at all. 0xA - The windowed watchdog will generate a non-maskable interrupt to the CPU if the watchdog is serviced outside the time window defined by the configuration, or if the watchdog is not serviced at all. |
| uint32 | windowSize | Digital Windowed Watchdog Window Size. Selecting 100% enables standard watchdog (not windowed). WWDSIZE: 0x00000050 = 50%, WWDSIZE: 0x00000500 = 25%, WWDSIZE: 0x00005000 = 12.5%, WWDSIZE: 0x00050000 = 6.25%, WWDSIZE: 0x00500000 = 3.125%, WWDSIZE: Any other value = 3.125% |
| uint32 | timeOutVal | Watchdog timeout period in milli seconds.Watchdog generates a non-maskable interrupt or reset to the CPU if the watchdog is serviced after this timeout period. |
| Design ID | DES_WDG_011 |
| Requirements Covered | MCAL-2601, MCAL-2635, MCAL-2636, MCAL-2637 |
Refer section 8.2.1 of 1 Used for pointers to structures holding configuration data provided to the Wdg module initialization routine for configuration of the module and watchdog hardware.
| Type | Variable Name | Comments |
|---|---|---|
| WdgIf_ModeType | defaultMode | Default watchdog mode(WDGIF_FAST_MODE/WDGIF_SLOW_MODE) |
| Wdg_ModeInfoType | fastModeCfg | Contains fast mode hardware specific configuration.(Wdg_ModeInfoType) |
| Wdg_ModeInfoType | slowModeCfg | Contains slow mode hardware specific configuration.(Wdg_ModeInfoType) |
| Design ID | DES_WDG_012 |
| Requirements Covered | MCAL-2602 |
Used to define Pre-Compile parameters populated by configurator.
| Type | Variable Name | Comments |
|---|---|---|
| uint16 | instanceId | Hardware Instance Id |
| uint32 | initialTimeOut | The initial timeout (seconds) for the trigger condition to be initialized during Init function. It shall be not larger than WdgMaxTimeout. |
| Design ID | DES_WDG_013 |
| Requirements Covered | MCAL-2639, MCAL-2552 |
| Name | Type | Range | Comments |
|---|---|---|---|
| rtiDwdCtrl | uint32 | 0 to 0xFFFFFFFF | Digital Watchdog Control, To Enable DWD |
| rtiDwdprld | uint32 | 0 to 0xFFFFFFFF | Digital Watchdog Preload Value |
| rtiWdStatus | uint32 | 0 to 0xFFFFFFFF | Digital Watchdog Status Register |
| rtiWdKey | uint32 | 0 to 0xFFFFFFFF | Digital Watchdog Key Register |
| rtiWwdRxnCtrl | uint32 | 0 to 0xFFFFFFFF | Digital Windowed Watchdog Reaction |
| rtiWwdSizeCtrl | uint32 | 0 to 0xFFFFFFFF | Digital Windowed Watchdog Window Size |
For the standard API's please refer 8.3 of 1. Sections below also highlight other design considerations for the implementation.
Refer section 8.3.1 of 1
| Design ID | DES_WDG_014 |
| Requirements Covered | MCAL-2603, MCAL-2604, MCAL-2605, MCAL-2606, MCAL-2607 MCAL-2608, MCAL-2609, MCAL-2610 |
Refer section 8.3.3 of 1
| Design ID | DES_WDG_015 |
| Requirements Covered | MCAL-2622, MCAL-2623, MCAL-2624, MCAL-2625, MCAL-2626, MCAL-2627 |
Refer section 8.3.4 of 1
| Design ID | DES_WDG_016 |
| Requirements Covered | MCAL-2628, MCAL-2629 |
| Design ID | DES_WDG_017 |
| Requirements Covered | MCAL-2593, MCAL-2587, MCAL-2589, MCAL-2590, MCAL-2591, MCAL-2592, MCAL-2594, MCAL-2595, MCAL-2596, MCAL-2644, MCAL-2647, MCAL-2573, MCAL-2575 |
| Service Name | Wdg_Trigger |
| Description | Trigger routine which should be called by application periodically |
| Syntax | void Wdg_Trigger(void) |
| Service ID | 0x05 |
As noted from previous implementation, the wdg configuration registers could be potentially corrupted by other entities (s/w or h/w). One of the recommended detection methods would be to periodically read-back the configuration and confirm configuration is consistent. The service API defined below shall be implemented to enable this detection. Constraint: Should be called only after module initialization
| Description | Comments | |
| Service Name | Wdg_RegisterReadback | Can potentially be turned OFF |
| Design ID | DES_WDG_018 | |
| Requirements Covered | MCAL-2643 | |
| Syntax | Std_ReturnType Wdg_RegisterReadback(P2VAR(Wdg_RegisterReadbackType, AUTOMATIC, WDG_APPL_DATA) regRbPtr) | Wdg_RegisterReadbackType defines the type, that holds critical values, refer below |
| Service ID | 0x06 | |
| Sync / Async | Sync | |
| Reentrancy | Non Reentrant | |
| Parameter in | None | None |
| Parameters out | regRbPtr | A pointer of type Wdg_RegisterReadbackType, which holds the read back values |
| Return Value | Standard return type | E_OK or E_NOT_OK in case of DET error |
The critical register listed is a recommendation and implementation shall determine appropriate registers.
This service could potentially be turned OFF in the configurator.
This design expects that implementation require to use following global variables.
| Variable | Type | Description | Default Value |
|---|---|---|---|
| Wdg_DrvStatus | Wdg_StatusType | Initialization status of the driver is maintained | WDG_UNINIT |
| Wdg_DrvObj | Wdg_DriverObjType | WDG driver object, local to the implementation and scope shall NOT be limited to Wdg.c | Undefined |
| Design ID | DES_WDG_019 |
| Requirements Covered | SWS_BSW_00130 |
Sections below list some of the important design decisions and rationale behind those decision.
The watchdog hardware generates a violation interrupt or ESM interrupt after a programmable period, if no correct key sequence is written to the RTI watchdog key register.
Guarantee reset on watchdog expiry and minimal software load on CPU.
Recommended to use ESM interrupt mode. ESM will make sure to signal the severe device failure if interrupt occurs.
The routine servicing a watchdog shall be implemented as an interrupt routine driven by a hardware timer/GPT.Refer SWS_Wdg_00166 AUTOSAR WDG specification 1.
There should be no dependency on external module.
To avoid dependency on the external module Wdg_Trigger API is provided which should be called by application periodically.
| Design ID | DES_WDG_020 |
| Requirements Covered | MCAL-2651, MCAL-2652, MCAL-2653 |
The sections below identify some of the aspects of design that would require emphasis during testing of this design implementation
| Revision | Date | Author | Description | Status |
|---|---|---|---|---|
| 0.1 | 30th Nov 2018 | Sunil M S | First version | Pending Review |
| 1.0 | 6th Dec 2018 | Sunil M S | Addressed Review Comments Intranet Link | Approved |