![]() |
TIOVX User Guide
|
Graph static configuration values.
Defines | |
| #define | TIVX_GRAPH_MAX_HEAD_NODES (8u) |
| Max possible head nodes in graph. | |
| #define | TIVX_GRAPH_MAX_LEAF_NODES (16u) |
| Max possible leaf nodes in graph. | |
| #define | TIVX_GRAPH_MAX_PARAMS (8u) |
| Max possible parameters in graph. | |
| #define | TIVX_GRAPH_MAX_DATA_REF_QUEUE (32u) |
| Max data ref queue in graph. | |
| #define | TIVX_GRAPH_MAX_DELAYS (8u) |
| Max possible delays in graph. | |
| #define | TIVX_GRAPH_MAX_DATA_REF (128u) |
| Max possible data references in a graph. | |
| #define | TIVX_DEFAULT_GRAPH_TIMEOUT (TIVX_EVENT_TIMEOUT_WAIT_FOREVER) |
| Default timeout value for graph level control event ACK waits. This is the default timeout value used within the following APIs. More... | |
| #define TIVX_DEFAULT_GRAPH_TIMEOUT (TIVX_EVENT_TIMEOUT_WAIT_FOREVER) |
Default timeout value for graph level control event ACK waits. This is the default timeout value used within the following APIs.
Definition at line 492 of file tivx_config.h.