![]() |
TIOVX User Guide
|
APIs for debug operations on the host.
Defines | |
| #define | VX_PRINT(zone, message, ...) do { tivx_print(((vx_enum)zone), "[%s:%u] "message, __FUNCTION__, __LINE__, ## __VA_ARGS__); } while (1 == 0) |
| The OpenVX Debugging Facility. | |
Enumerations | |
| enum | tivx_debug_zone_e { VX_ZONE_ERROR = 0, VX_ZONE_WARNING = 1, VX_ZONE_API = 2, VX_ZONE_INFO = 3, VX_ZONE_PERF = 4 } |
| These are the bit flags for debugging. More... | |
Functions | |
| void | tivx_print (vx_enum zone, const char *format,...) |
| Internal Printing Function. More... | |
| void | tivx_set_debug_zone (vx_enum zone) |
| Sets a zone bit in the debug mask. More... | |
| void | tivx_clr_debug_zone (vx_enum zone) |
| Clears the zone bit in the mask. More... | |
| vx_bool | tivx_get_debug_zone (vx_enum zone) |
| Returns true or false if the zone bit is set or cleared. More... | |
| enum tivx_debug_zone_e |
These are the bit flags for debugging.
Definition at line 76 of file tivx_debug.h.
| void tivx_print | ( | vx_enum | zone, |
| const char * | format, | ||
| ... | |||
| ) |
Internal Printing Function.
| [in] | zone | The debug zone from tivx_debug_zone_e. |
| [in] | format | The format string to print. |
| [in] | ... | The variable list of arguments. |
| void tivx_set_debug_zone | ( | vx_enum | zone | ) |
Sets a zone bit in the debug mask.
| [in] | zone | The debug zone from tivx_debug_zone_e. |
| void tivx_clr_debug_zone | ( | vx_enum | zone | ) |
Clears the zone bit in the mask.
| [in] | zone | The debug zone from tivx_debug_zone_e. |
Returns true or false if the zone bit is set or cleared.
| [in] | zone | The debug zone from tivx_debug_zone_e. |