2.4. Release Notes - 06_02_01

2.4.1. Introduction

This release notes provides important information that will assist you in using the PDK software package for the TPR12 family of devices. This document provides the product information and known issues that are specific to the PDK software package.

2.4.2. What’s New

  • CSL
    • Added CSL support for tpr12 devices with the SoC data
    • Added build support
  • EDMA
    • Added support for the EDMA driver
    • Added support for Polling, Callback and DMA modes
    • Added support for dma, qdma channels, chaining, linking
    • Added support for all instances of EDMA.
    • Added support for EDMA driver from both R5 and C66x cores
  • OSAL
    • Added support for the OSAL module
    • Added support for both baremetal and TIRTOS abstraction
    • Added support for semaphore, timer, delay, interrupts, queue and Cache

2.4.3. Upgrade and Compatibility

  • None

2.4.4. Device Support

  • TPR12 QT(BOARD=tpr12_evm)

2.4.5. Validation Information

This release is validated on tpr12 QT for the applicable components. For details on the validated examples refer to the platform specific test report present in PDK_INSTALL_DIR/docs/test_report folder.

2.4.6. Tool Chain Information

Component Version
Sys Bios 6_82_00_16
XDC Tools 3_61_00_10
TI ARM R5F code generation tools 18.12.5.LTS
C6x code generation tools c6000_8.3.2

2.4.7. Fixed Issues

  • None.
    • This is the first releasre for the TPR12 device.

2.4.8. Known Issues

ID Head Line Module Reported in Release Affected Platforms Workaround in this release
PDK-4965 Warnings while linking apps in release build BUILD PROCESSOR-SDK_06.02.01 TPR12 None. Release binary created with warning, which can be used

2.4.9. Limitations

  • None