5.2. Jacinto 7 SBL

5.2.1. Introduction

The Secondary Bootloader (SBL) for AM65xx/J721E device initializes the execution environment for multi-core applications and this can be used to demonstrate a real world product experience. This section covers additional details including execution sequence, tools and additional flashing instructions.

The SBL is essentially a baremetal application, and it uses many components from the Processor SDK

  • <PDK>/packages/ti/build : For build infrastructure
  • <PDK>/packages/ti/csl : For initialization and SoC addresses
  • <PDK>/packages/ti/board : For board and usecase specific initialization
  • <PDK>/packages/ti/drv/spi : For reading applications from OSPI flashes
  • <PDK>/packages/ti/drv/udma : For reading data from boot media using DMA
  • <PDK>/packages/ti/drv/mmcsd : For reading applications from MMC/SD/eMMC
  • <PDK>/packages/ti/fs/fatfs : For reading files from MMC/SD/eMMC
  • <PDK>/packages/ti/drv/sciclient : For communicating with DMSC sub-system
  • <PDK>/packages/ti/drv/uart : For log messages
  • <PDK>/packages/ti/osal : Primitives required by ti/drv components

The SBL is in turn used by the board framework to load and start diagnostics

Bootloader Execution Sequence

  • Power On Reset
  • ROM Bootloader (RBL)
    • Software pre-programmed in AM65xx/J721E ROM memory starts executing
    • The RBL performs platform configuration and initialization.
    • It then checks sysboot pins and chooses booting device
    • The RBL then configures PLL and clock settings for R5, and boot media like eMMC, SD/MMC, OSPI, UART, PCIe, Ethernet etc for reliable boot.
    • If no valid bootloader found on booting device, the RBL checks for next booting device, based on sysboot pins
    • It then gets image size and load address by checking the X.509 certificate that is part of the bootloader image.
    • The RBL then verifies, optionally decrypts and loads the binary to internal memory at the load address specified in the X.509 certificate.
    • Finally it resets the R5 and passes control to Secondary Bootloader(SBL) running on the R5.
  • Secondary bootloader(SBL)
    • User level secondary bootloader(SBL) begins execution from internal memory. It enables ATCM, starts PMU timers for profiling, initializes the MCU, and sets up the stack, heap and globals. It then jumps to main().
    • Board Initialization is done by calls to Board_init() API.For additional details refer Processor SDK Board Support.
    • The RAT is setup. Pin MUX and UART console are setup by calling Board_init() API. The system firmware (SYSFW) is then loaded from the boot media into the DMSC subsystem.
    • Once the SYSFW is up and running, the rest of the initialization can be done.
    • This includes optionally using Board_init() to configure PLLs, LPSCs and DDR.
    • The SBL then loads the application from the boot media. If the image is signed, the application will be copied into a user specified reserved memory, and the SBL will attempt to verify the image by calling system firmware APIs. On HS devices, the boot proceeds only if image verification passes.
    • The SBL parses application image(s) for each of the core(s) from boot media and scatter loads it to memory.
    • Once the application is loaded, the SBL communicates with the system firmware to setup the clocks for the core(s) and release it from reset.
    • The core then starts executing from application entry point.

NOTE

  • RBL requires boot loader (SBL) to be in a special format with the binary image appended to a X.509 certificate. The certificate contains the load address, size and SHA of the bootloader image.
  • For a detailed description of ROM bootloader and more information on the image format expected by the RBL refer the initialization chapter in the AM65xx Technical Reference Manual and the J721E Technical Reference Manual
  • In addition to the bootloader and application, the DMSC firmware binary is also needed for the SoC to complete the system boot flow.
  • The first 256 bytes of the ATCM are reserved by SBL for its use. The SBL initializes the ATCM with 0xFF before it uses it.
  • If the multicore application image is signed using the TI Dummy Key, instead of a degenerate key (default setting) the same binary can be used on GP and HS devices. For information on the application’s X.509 certificate format, please refer Security X509 Certificate Documentation
  • When the R5 is released from reset, it will always fetch and execute the first intruction from address 0x0.

5.2.2. Block Diagram

../_images/k3_sbl_arch_block_diag.png

5.2.3. Memory Map

../_images/k3_sbl_mem_usage.png

5.2.4. Directory structure

sbl
│
├── board
│   └── k3
│       └── sbl_main.c                                      <= define main() for SBL, board specific init
│
├── build
│   ├── makefile                                            <= makefile for the SBL component
│   ├── sbl_am65xx.sh                                       <= For legacy, called by Yocto build
│   ├── sbl_boot_test.mk                                    <= Builds SBL single core tests
│   ├── sbl_smp_test.mk                                     <= Builds example app for using SBL lib
│   ├── sbl_mcu0_boot_perf_test.mk                          <= Builds example app for SBL performance tuning
│   ├── sbl_mcu0_boot_xip_entry.mk                          <= Builds example trampoline app to demonstrate transitioning to a XIP app from SBL
│   ├── sbl_mcu0_boot_xip_test.mk                           <= Builds example app to demonstrate XIP execution from XIP capable boot media
│   ├── sbl_img.mk                                          <= builds SBL image that is loaded and executed by ROM code
│   ├── sbl_lib.mk                                          <= Builds sbl library that other apps can link into
│   ├── sbl_multicore_smp.mk                                <= Builds multi-core image from SBL lib eg. test to demonstrate symmetric multiprocessor boot (SMP)
│   └── sbl_multicore_amp.mk                                <= Builds multi-core image from single core tests to demonstrate asymmetric multiprocessor boot (AMP)
│
├── example
│   └── k3MulticoreApp
│       ├── binary
│       │   └── [soc]
│       │       ├── sbl_baremetal_*.appimage                <= SBL loadable board specific sample apps for testing SBL boot flow on GP devices
│       │       ├── sbl_baremetal_*.appimage.signed         <= SBL loadable board specific signed sample apps for testing SBL boot flow on HS devices
│       │       └── sbl_baremetal_*_release.x*.bin          <= Binary image that can be eXecuted In Place on XIP capable boot media
│       ├── mcuAmplinker.lds                                <= Linker comamnd file when TI CGT is used for Asym. Multiproc. boot
│       ├── mpuAmplinker.lds                                <= GCC linker command file (for Cortex Axx cores) for Asym. Multiproc. boot
│       ├── mcuBootPerfLinker.lds                           <= TI CGT Linker command file for SBL performance tuning example.
|       |── mcuBootPerfLinker_small.lds                     <= TI CGT Linker command file for SBL performance tuning example (for boot with MCU domain only)
│       ├── mcuLockStepLinker.lds                           <= Linker comamnd file when TI CGT is used for R5 lock-step boot
│       ├── mpuSmplinker.lds                                <= GCC linker command file (for Cortex Axx cores) for SMP boot
│       ├── mcuXiplinker.lds                                <= Linker command file for XIP trampoline app
│       ├── xip_entry.lds                                   <= Linker comamnd file for XIP test case
│       ├── xip_entry.asm                                   <= Entry point of XIP trampoline app
│       ├── xip_stub.c                                      <= Simple SBL test app that demonstrates transitioning to a XIP app
│       ├── sbl_amp_multicore.c                             <= Simple SBL test that displays UART message
│       ├── sbl_amp_multicore_sections.h                    <= Allows same source to be loaded to different sections for different cores.
│       ├── sbl_mcu_0_boot_perf_benchmark.c                 <= SBL Test to tune boot performance.
│       ├── sbl_multicore_a53.asm                           <= Test case entry point  for Cortex-Axx cores
│       ├── sbl_multicore_r5.asm                            <= Test case entry point for Cortex-R5 cores
│       ├── sbl_multicore_r5_sections.inc                   <= Allows same source to be loaded to different sections for different MCUs.
│       ├── sbl_printf.c                                    <= Lightweight UART printf function for SBL testing
│       ├── sbl_smp_multicore.c                             <= Simple SBL SMP test that uses SBL lib to reset MPUs
│       └── sbl_smp_r5.asm                                  <= Provides dummy override function for __mpu_init for SMP testcase.
│
├── binary                                                  <= ROM bootable SBL images for each board/boot media
│   ├── [board]
│       └── [bootmedia]
│           └── bin
│               └── sbl_[bootmedia]_img_mcu1_0_release.tiimage
│
├── lib                                                     <= SBL lib for each boot media/board supported
│   ├── [bootmedia]
│   │   └── [board]
│   │       └── r5f
│   │           └── release
│   │               └── sbl_lib_[bootmedia].aer5f
│   └── cust
│       └── [board]
│           └── r5f
│               └── release
│                   └── sbl_lib_cust.aer5f
│
├── soc                                                     <= SOC specific SBL code
│   └── k3
│       ├── linker.cmd                                      <= Linker file used for generating ROM loadable SBL image.
│       ├── sbl_err_trap.h                                  <= Error loops for SBL
│       ├── sbl_init.asm                                    <= SBL Entry point
│       ├── sbl_misc.asm                                    <= SBL Assembly utility functions
│       ├── sbl_log.h                                       <= SBL logging framework
│       ├── sbl_sci_client.c                                <= Calls SYSFW on DMSC
│       ├── sbl_sci_client.h
│       ├── sbl_slave_core_boot.c                           <= Code that contains the sequence to release a core from reset
│       ├── sbl_slave_core_boot.h
│       ├── sbl_soc.c                                       <= Cache Ops, PMU init, image verfication, etc & SoC specific code like RAT Init..
│       ├── sbl_soc_cfg.h                                   <= Abstraction layer for hiding SoC level changes from SBL
│       └── sbl_profile.h                                   <= SBL profiling framework
│
├── src                                                     <= Common drivers used across SOCs
│   ├── mmcsd
│   ├── hyperflash
│   ├── ospi
│   ├── qspi
│   ├── uart
│   ├── rprc                                                <= RPRC image parser used by SBL
│   └── spi
│
└── tools
    ├── btoccs
    ├── byteswap
    ├── ccsutil
    ├── flashWriter                                         <= Unused for AM65xx/J721E. AM65xx/J721E uses Uniflash to program flashes.
    ├── multicoreImageGen                                   <= Stitches multiple RPRC images for different cores into a single image
    ├── omapl13x_boot_utils                                 <= Unused for AM65xx/J721E
    ├── omapl13x_sd_card_format                             <= Unused for AM65xx/J721E
    ├── out2rprc                                            <= Converts .out into .rprc files, so that SBL can load non-continuous memory sections
    ├── scripts                                             <= Scripts used by .out  generated by CCS projects into SBL loadable images
    │   ├── K3ImageGen.bat
    │   └── K3ImageGen.sh
    └── tiImageGen                                          <= Unused for AM65xx/J721E. Image generation is handled by PDK build framework (<prsdk_install_path>/pdk_*/packages/ti/build/)

5.2.5. Image Formats

SBL format:

To generate the a bootable image, the SBL build uses the x509CertificateGen script to sign the sbl binary with so that the ROM Boot Loader (RBL) can parse it. The image format expected by the RBL has been described in detail in the Image Format Section of the AM65xx Technical Reference Manual and the J721E Technical Reference Manual

Note

For HS devices, the SBL and system firmware have to be signed with the MPK. For an easy out-of-box experience, the Processor SDK for HS devices signs the SBL and system firmware with a TI Dummy Key. Images signed with a TI dummy key will boot on both GP and HS boards from TI. The build system invokes the script <PDK>/packages/ti/build/makerules/x509CertificateGen* which inturn calls OpenSSL to create the X509 certificate.

Warning

The TI Dummy Key(s) MUST be replaced by customers during production with their own Private Keys. If the TI Dummy Keys are used in a production system, the system will be open to security attacks. The path of the default (dummy) key used by the signing script for HS devices is <PDK>/packages/ti/build/makerules/k3_dev_mpk.pem

Warning

While SBL and system firmware images signed with the TI Dummy Keys will work on both GP and HS devices, the boot time will be significantly impacted on GP devices. Using SBL signed by TI Dummy Keys on GP devices is only recommended during the prototyping phase - when porting code developed on GP to HS devices.

Application image format:

Two utilities - out2rprc and multicoreImageGen are used to convert an application elf image(s) into an image loadable by the SBL. The structure of a multicore application image is provided below:

../_images/multicore_app_image.png

RPRC File Header Format

Offset Binary value
0x00000000 Magic Word(43525052)
0x00000004 Entry Point (Location)
0x00000008 Reserved Addr
0x0000000C Section Count
0x00000010 Version

RPRC Section Header Format

Offset Binary value
0x00000000 Section start Address
0x00000004 Reserved Addr
0x00000008 Size
0x0000000C Reserved CRC
0x00000010 Reserved

Multicore boot image format

Meta Header Start

Offset Binary value
0x00000000 Magic String (0x5254534D)
0x00000004 Number of Files
0x00000008 Device ID
0x0000000C Reserved

Meta Header per Core

Offset Binary value
0x00000000 Core ID
0x00000004 Image Offset

Signed application image format:

To convert the multicore application image into a format that can be verified, the build flow uses the x509CertificateGen script to create a x509 certificate for the app image. Images that have a x509 certificate are called signed images. Signed applications images are mandatory for HS devices, but will work also work on GP devices.

Signed images are automatically detected by the SBL and loaded into a scratch memory area specified during SBL build. The scratch memory area used by default is specified in sbl_lib.mk via the flags SBL_SCRATCH_MEM_START and SBL_SCRATCH_MEM_SIZE. The SBL_SCRATCH_MEM* options can also be specified for custom builds to override the defaults.

The SBL scratch memory is unavailable to applications during app load time, as the SBL is still active. Once the SBL transfers control to the application, this memory is available for app use - in other words SBL_SCRATCH_MEM* is available during app runtime.

For information on the application’s X.509 certificate format, please refer Security X509 Certificate Documentation

5.2.6. Building the SBL and its components

Pre-requisites to Building

  • Set your environment using pdksetupenv.bat or pdksetupenv.sh. Refer to Processor SDK RTOS Building for information on setting up your build environment

NOTE

  • SBL needs openssl to build. To check if openssl is present, type the following at the linux or windows prompt.
openssl version
  • To build on Linux, you need to have mono installed.
  • Refer Build Dependencies for instructions on how to install these tools, if they are not already present on your system.

Compiling the SBL

To build all the SBL components:

cd <PDK>/packages/ti/boot/sbl/build
gmake clean all (for windows)
make clean all  (for Linux)
  • SBL image files are be located at: <PDK>/packages/ti/boot/sbl/binary/
  • SBL examples are located at <PDK>/packages/ti/boot/sbl/examples/k3MulticoreApp/binary
  • SBL lib are located at <PDK>/packages/ti/boot/sbl/lib/

Compile time options for the SBL

The SBL supports several compile time options to tweak the SBL to satisfy requirements of ease of use, boot time and size. These can be enabled or disabled by editing sbl/sbl_component.mk

  • SBL_LOG_LEVEL : Controls amount of SBL logs (on the MCU UART) and system firmware logs(on WAKEUP UART). Varies from 0(no logs) to 3 (all logs)
  • SBL_USE_DMA : Valid values are 0 (use CPU to access boot media) or 1 (use DMA to access boot media).
  • SBL_DISPLAY_PROFILE_INFO : At the end of the boot process, displays a log of timestamps at which different SBL profile points are hit. This is useful to see how much time the SBL spends in different functions. SBL_LOG_LEVEL can significantly affect performance numbers.
  • SBL_ENABLE_PLL : Dials up all the PLLs calling Board_init(). Makes it easier for applications as they no longer have to initialize the PLLs. However, enabling this significantly increases boot time and power consumption. Requires system firmware to be loaded.
  • SBL_ENABLE_CLOCKS : Enables all the module clocks by calling Board_init(). Makes it easier for applications as they no longer have to enable clocks.
  • SBL_ENABLE_DDR : Initializes the DDR. At the cost of boot time, this enables applications to run from and use DDR. SBL_ENABLE_CLOCKS and SBL_ENABLE_PLL must also be enabed for this to work. Enabling this option increases the boot time.
  • SBL_SKIP_MCU_RESET : Jumps to the MCU0 application entry point without resetting the core. Enables faster boot time. Will not change the MCU’s mode (lock-step/split). Application also inherits the MCU state as the SBL left it in.
  • SBL_ENABLE_DEV_GRP_MCU : Will cause the system firmware to only use MCU domain resources during system firmware initialization. This can be done either to support boot when the main power domain is off, or to save boot time.
  • SBL_HLOS_OWNS_FLASH : Ensures the SBL will not leave the OSPI flash in XIP mode, so that the MAIN domain Cortex-A code (e.g., HLOS) can reset the flash and take control of it, if needed.
  • SBL_SKIP_PINMUX_ENABLE : SBL will skip any PINMUX init being done in the bootloader and expect that it will be handled by a subsequent application.
  • SBL_SKIP_LATE_INIT : SBL will skip calling the SoC Late Init functions, normally contained in SBL_SocLateInit()
  • SBL_USE_MCU_DOMAIN_ONLY : SBL will configure & boot MCU domain cores ONLY. Saves boot time when configuring & using MCU domain only (especially when testing MCU-only boot or measuring Early CAN response).

The SBL also supports a “custom” build, in addition to standard out-of-box builds. A custom build is a useful way of testing out the effect of different build options - like when optimizing for boot time, or enabling custom usecases like eXecute In Place (XIP) to reduce memory usage.

For an example of how to use such custom builds, please refer to sbl/sbl_component.mk. It shows how to specify a select list of build options while building SBL images and libs.

SBL Startup

The SBL can specify the R5 configuration (lockstep or split) that ROM needs to use when it starts up the SBL. This info is passed to ROM as a field in the X509 certificate. The value in this field can be controlled by editing the build flag R5_STARTUP_MODE in sbl/build/sbl_img.mk

  • EFUSE_DEFAULT : SBL will run with the same R5 configuration the boot rom ran in.
  • SPLIT_MODE : ROM will switch the R5 to split mode before starting the SBL (default).

Enabling/Disabling JTAG on secure devices

JTAG access is controlled using a field in the X509 certificate.

By default, for an easy out of box experience, the Processor SDK enables debug via JTAG on High Secure devices. Leaving JTAG enabled, while making it easy for software development, creates a major security hole in production devices.

To disable/change the level of JTAG access on HS devices, update the value of the debugType field in the signing scripts build/makerules/x509template.txt (when building from windows) and build/makerules/x509CertificateGen.sh (when building from linux).

Valid values are

  • 0 : Disable all JTAG access (most secure and most restrictive)
  • 1 : Use device defaults (most secure and most restrictive)
  • 2 : Allow debug of non-secure code, when the CPU is running in secure mode, JTAG connectivity will be lost
  • 4 : Allow debug of both secure and non-secure code (least secure and least restrictive). This is the default.

Compiling apps that can be loaded by SBL:

Memory Map Considerations

Applications that the SBL loads must comply with the sbl-memory-usage. In the application’s linker command file, care must be taken to not use the first 0x100 bytes of any R5 MCU’s ATCM memory and SBL reserved memory from 0x41C00100 to 0x41C3E000. If the applications are signed, no loadable sections must be placed in the SBL scratch memory area. The scratch memory can be used at application runtime for stacks, heaps, etc.

NOTE

  • The local address 0x0 of the MPU is not accessible from the MCU, so any MPU linker command file must not specify any loadable sections in that memory region. The SBL will not be able to access that memory to load code or data.

Converting ELF executables to SBL loadable image

Depending on the usecase, an ELF application executable can be converted into an image that can be loaded by SBL in many ways.

  • Using CCS: Any project created using the pdkProjectCreate scripts will automatically generate a SBL loadable app, as part of a post-build step.
  • Using makefiles: Add the following lines to the component’s .mk file
app_name_SBL_APPIMAGEGEN = yes
export app_name_SBL_APPIMAGEGEN
  • Existing ELF executable: By calling the K3ImageGen script.
Linux Syntax: K3ImageGen.sh <CoreID> <.out>

Example:
cd  <prsdk_install_path>/pdk_*/packages/ti/boot/sbl/example/ampMulticoreApp/binary/am65xx_evm/
K3ImageGen.sh 4 sbl_baremetal_boot_test_am65xx_evm_mcu1_0TestApp_release.xer5f
Windows Syntax: K3ImageGen.bat "<CoreID> <.out>"

Example:
cd  <prsdk_install_path>\pdk_*\packages\ti\boot\sbl\example\ampMulticoreApp\binary\am65xx_evm\
K3ImageGen.bat "4 sbl_baremetal_boot_test_am65xx_evm_mcu1_0TestApp_release.xer5f"
  • Multicore Images: Multicore images, as the name suggests, allows the SBL to load applications for multiple cores from a single image. Creating such images invloves three steps.
  1. Generate the ELF application executables for individual cores
  2. Convert the ELF executables into intermediate .rprc images
  3. Combine the .rprc images of individual cores to create a single multicore image

To covert any .out into the intermediate .rprc format, execute the following commands

For Linux:
mono <PDK>/packages/ti/boot/sbl/tools/out2rprc/bin/out2rprc.exe input.out output.rprc
For Windows:
<PDK>\packages\ti\boot\sbl\tools\out2rprc\bin\out2rprc.exe input.out output.rprc

To stitch multiple .rprc images into a multicore image, execute the following command

For Linux:
<PDK>/packages/ti/boot/sbl/tools/multicoreImageGen/bin/MulticoreImageGen LE 55 output.appimage  <core_id_1> core_1.rprc <core_id_2> core_2.rprc
For Windows:
<PDK>/packages/ti/boot/sbl/tools/multicoreImageGen/bin/MulticoreImageGen.exe LE 55 output.appimage  <core_id_1> core_1.rprc <core_id_2> core_2.rprc

NOTE

  • The linux host environment needs to have mono installed.
  • The values used for the Core ID and Device ID can be found in sbl/soc/k3/ sbl_slave_core_boot.h
  • To simply load an ELF without executing it, use CoreID value ONLY_LOAD_ID
  • If an image for MCU_1 core is provided, the SBL will attempt to switch to split mode.
  • If only an image for MCU_0 is provided, the SBL will not change the mode of the MCU subsystem.
  • To enable SMP on the MPU, ie, to get multiple MPUs execute from a single binary from the same address, use one of the following core_ids
    • MPU1_SMP_ID: The same app binary runs on both cores in MPU cluster 1
    • MPU2_SMP_ID: The same app binary runs on both cores in MPU cluster 2
    • MPU_SMP_ID: The same app binary runs all the MPUs

Converting ELF executables to executable binary images

Sometimes, for exteremely constrained and specialized usecases like ultra-low-latency boot or DDR-less systems, an ELF application executable can be converted into a binary image that can executed directly from the boot media, without loading into internal memory.

As internal memory is always accessible, this mode of execution allows some otherwise mandatory steps steps like DDR initlization or clock initialization to be done later or skipped altogether.

Working with such highly contrained systems require some special steps..

  • Make sure that the boot media supports eXecuting In Place (XIP).
  • Use the custom SBL build to select the build options to build a SBL that meets the usecase requirements.
  • In the linker command file for the application, make sure that all the data sections, stacks, heaps and globals are in internal read/write memory
  • In the linker command file for the application, make sure that there are no holes in the loadable sections. Such non-contiguous sections can drastically blow up the binary image size, when comapred to the ELF executable size.
  • To generate an executable binary image from the applications ELF file, add the following lines to the component’s .mk file
app_name_SBL_APP_BINIMAGEGEN = yes
export app_name_SBL_APP_BINIMAGEGEN

5.2.7. Testing the SBL

SBL provides test applications to demonstrate booting the A53/A72 and R5 cores in both symmetric/lock step & asymmetric/split-mode and other features. The multicore sample application prints a message on the UART for each core. The functionality the different tests exercises are listed below.

  • sbl_*_boot_test_*_all_coresTestApp_release: A single multicore boot test case that boots each core in the SoC with a separate app. Also tests DDR loading
  • sbl_*_boot_test_*_xxxx_xTestApp_release.appimage: A simple testcase for booting core xxxx_x (eg. MCU1_0, MPU2_0 etc.)
  • sbl_*_smp_test_*_all_coresTestApp_release.appimage: A single SMP boot test case that boots MCUs in lock step. The MCU app then uses the SBL lib to boot all the MPUs in SMP mode, ie, all the MPUs execute a single binary from the same address.
  • sbl_baremetal_boot_perf_*_mcu1_0TestApp_release.appimage: A single MCU1_0 test case that can be used to measure the effect of enabling/disabling the perf. tuning knobs in the SBL for OSPI boot. The size of the test case can be easily modified by changing the values of .space directives in sbl/example/k3MulticoreApp/ sbl_boot_perf_r5.asm to profile for different app image sizes.
  • sbl_baremetal_boot_xip_test_*_mcu1_0TestApp_release.xer5f.bin: A testcase demonstrating booting an XIP application from OSPI flash. Please refer sbl/build/ sbl_mcu0_boot_xip_test.mk and sbl/example/k3MulticoreApp/mcuXiplinker.lds to see how to convert an existing application into an XIP application. The sbl_*_xip_entry_*.appimage works in tandem with sbl_*xip_test_*.xer5f.bin to transition the system from non-xip to xip boot, as the ROM, by default, does not support XIP from boot media. After programming the sbl and syfw, to program both sbl_*_xip_entry_*.appimage and sbl_*xip_test_*.xer5f.bin into OSPI flash, use the following uniflash commands
For Windows:
.\dslite.bat --mode processors -c COM9 -f <PDK>\packages\ti\boot\sbl\example\k3MulticoreApp\binary\am65xx\sbl_baremetal_boot_xip_entry_am65xx_evm_mcu1_0TestApp_release.appimage -d 3 -o A0000
.\dslite.bat --mode processors -c COM9 -f <PDK>\packages\ti\boot\sbl\example\k3MulticoreApp\binary\am65xx\sbl_baremetal_boot_xip_test_am65xx_evm_mcu1_0TestApp_release.xer5f.bin -d 3 -o E0000
For Linux:
sudo ./dslite.sh --mode processors -c /dev/ttyUSB1 -f <PDK>/packages/ti/boot/sbl/example/k3MulticoreApp/binary/am65xx/sbl_baremetal_boot_xip_entry_am65xx_evm_mcu1_0TestApp_release.appimage -d 3 -o A0000
sudo ./dslite.sh --mode processors -c /dev/ttyUSB1 -f <PDK>/packages/ti/boot/sbl/example/k3MulticoreApp/binary/am65xx/sbl_baremetal_boot_xip_test_am65xx_evm_mcu1_0TestApp_release.xer5f.bin -d 3 -o E0000

An example test log for sbl_*_boot_test_*_all_coresTestApp_release is

SYSFW  ver xx.x.x-v20xx.xx (xxx xxx) running
SBL Revision: xx.xx.xx.xx (MMM  DD YYYY - HH:MM:SS)
MPU1_0 running
MPU1_1 running
MPU2_0 running
MPU2_1 running
MCU1_1 running
MCU1_0 running
MCU1_0 reports: All tests have passed

An example log for sbl_*_smp_test_*_all_coresTestApp_release.appimage is

SYSFW  ver xx.x.x-v20xx.xx (xxx xxx) running
SBL Revision: xx.xx.xx.xx (MMM  DD YYYY - HH:MM:SS)
MPU SMP boot test
Cores 0 & 1 will boot from 0x801007a0
Cores 2 & 3 will boot from 0x803007a0
Resetting all ARM cores now...
No of Cortex-A core(s) running: 1
No of Cortex-A core(s) running: 2
No of Cortex-A core(s) running: 3
No of Cortex-A core(s) running: 4
All tests have passed

An example log for sbl_baremetal_boot_perf_*_mcu1_0TestApp_release.appimage, when the best boot time is reached is

Time elapsed since start of SBL:     36665us
fxn:boot_perf_test_main     cycles:  14666041

Attempting board config ...BOARD_INIT_PLL ...passed
BOARD_INIT_MODULE_CLOCK...passed
BOARD_INIT_DDR...passed

Analyzing run results ....
Boot time is now optimized....
All tests have passed

Profiling info ....
MCU @ 400000000Hz.
cycles per usec  = 400
  fxn:                            main      line:  75       cycle:  xxx     timestamp:       432us
                                    .
                                    .
                                    .
  fxn:               SBL_SlaveCoreBoot      line: 231       cycle:  xxx     timestamp:     36149us

The test log for sbl_*_xip_test_*.xer5f.bin is

MCU1_0 running

5.2.8. Boot Modes

The SBL supports MMCSD, OSPI, and UART Boot modes. The different boot modes supported for all the boards is tabulated below.

  MMCSD OSPI UART PCIe ETH HYPERFLASH
AM65xx EVM YES YES YES NO NO NO
AM65xx IDK YES YES YES NO NO NO
J721E EVM YES YES YES NO NO NO

Booting Via SD Card

  1. Preparing the SD card.
  2. Booting the testcase from SD card.

Preparing the SD card

  1. To boot the target the SD card should be bootable. Follow the steps at Creating bootable SD card in windows or Creating bootable SD card in Linux.
  2. To update the SBL with a newer version, copy the sbl image (sbl_mmcsd_img_mcu1_0_release.tiimage) to the SD card. Rename it to tiboot3.bin
  3. To update the SYSFW with a newer version, copy the system firmware image binary (or, for HS device, use the encrypted system firmware binary) to the SD card as sysfw.bin.
  4. Copy the generated application image(*.appimage or *.appimage.signed) to the SD card. Rename it to app

Booting the testcase from SD card

  1. Insert SD card into the SD card slot of the board.
  2. Refer to the Boot Modes section in the AM6x EVM Hardware Users Guide and J721E EVM Hardware Users Guide to setup the EVM to boot from MMCSD.
  3. Open a serial communication terminal like TeraTerm, MiniCom on host PC and connect to the MCU UART console port
  4. Power cycle the board to boot the application from the SD card.
  5. The test logs will be displayed on the MCU UART

Booting Via OSPI flash

  1. Programming the OSPI flash
  2. Booting the testcase from OSPI flash

Booting the testcase from OSPI flash

  1. Refer to the Boot Modes section in the AM6x EVM Hardware Users Guide and J721E EVM Hardware Users Guide to setup the EVM to boot from OSPI.
  2. Open a serial communication terminal like TeraTerm, MiniCom on host PC and connect to the MCU UART console port
  3. Power cycle the board to boot the application from the OSPI flash.
  4. The test logs will be displayed on the MCU UART

Booting the testcase from UART

  1. Refer to the Boot Modes section in the AM6x EVM Hardware Users Guide and J721E EVM Hardware Users Guide to setup the EVM to boot from UART.
  2. Open a serial communication terminal like TeraTerm, MiniCom on host PC and connect to the MCU UART console port
  3. Power cycle the board, the console should show a sequence of CCC being printed
  4. Choose the X-Modem interface and send the SBL that was built for UART. After the transfer is completed, repeat the same step for sysfw.bin (or, for HS device, use the ‘sysfw-hs-enc.bin’) and the application. You will see notifications to perform these actions.

Warning

If sysfw.bin is not present in the boot media, the boot will fail without displaying any logs on the MCU UART. SBL enables UART logging only after successfully starting the system firmware image. If the system firmware load fails, the RBL will eventually reset the system.

Booting Via Hyperflash

  1. Programming the Hyperflash
  2. Booting the testcase from Hyperflashflash

Booting the testcase from Hyperflash

  1. Refer to the Boot Modes section in the J721E EVM Hardware Users Guide to setup the EVM to boot from Hyperflash.
  2. Open a serial communication terminal like TeraTerm, MiniCom on host PC and connect to the MCU UART console port
  3. Power cycle the board to boot the application from the Hyperflash.
  4. The test logs will be displayed on the MCU UART

5.2.9. EVM Setup for testing SBL

For information on board specific requirements like power supply, UART console port connections refer the Hardware User guide of the respective boards.

The configurations needed to setup UART console through a serial terminal application on host PC are listed in the next section.

UART Console Setup

PDK SBL prints messages on the UART Serial Console running on the host. Hence, a serial terminal application (like Tera Term/HyperTerminal/minicom) should be running on the host.

  • The host serial port must be configured at 115200 baud, no parity, 1 stop bit and no flow control.
  • Please ensure that the local echo setting for the terminal is turned off.
  • All SBL prints are routed to the MCU UART
  • To verify setup is correct, setup the EVM to boot from UART as the Primary Boot Device (refer to AM6x EVM Hardware Users Guide and J721E EVM Hardware Users Guide ) Power cycle the EVM, and look for the string CCCCCCC on the UART.