PDK API Guide for J721E
|
Connfiguration parameters of DOF.
struct Vhwa_M2mDofPrms
Data Fields | |
uint32_t | tPrmdLvl |
uint32_t | skipTempPredLine |
uint32_t | flowVectorHeight |
uint32_t | tPredictor |
uint32_t | mPredictor1 |
uint32_t | mPredictor2 |
uint32_t | bPredictor1 |
uint32_t | bPredictor2 |
Fvid2_Format | inOutImgFmt [DOF_MAX_PYR_LVL_SUPPORTED][VHWA_M2M_DOF_MAX_BUFFER] |
Dof_Config | coreCfg |
Vhwa_FocoPrms | focoPrms |
uint32_t Vhwa_M2mDofPrms::tPrmdLvl |
Total number of pyramid
uint32_t Vhwa_M2mDofPrms::skipTempPredLine |
Enter Value 1 if alternate line is to be skipped 0 for other wise
uint32_t Vhwa_M2mDofPrms::flowVectorHeight |
Height of the flow vector in case of SOF is used
uint32_t Vhwa_M2mDofPrms::tPredictor |
Predictor used by the top layer possible values DOF_PREDICTOR_DELEY_LEFT
uint32_t Vhwa_M2mDofPrms::mPredictor1 |
Predictor used by the middle pyramidal layer, possible values DOF_PREDICTOR_DELEY_LEFT DOF_PREDICTOR_PYR_LEFT DOF_PREDICTOR_PYR_COLOCATED
uint32_t Vhwa_M2mDofPrms::mPredictor2 |
Predictor used by the middle pyramidal layer, possible values DOF_PREDICTOR_DELEY_LEFT DOF_PREDICTOR_PYR_LEFT DOF_PREDICTOR_PYR_COLOCATED
uint32_t Vhwa_M2mDofPrms::bPredictor1 |
Predictor used by the base layer, possible values DOF_PREDICTOR_DELEY_LEFT DOF_PREDICTOR_PYR_LEFT DOF_PREDICTOR_PYR_COLOCATED DOF_PREDICTOR_TEMPORAL
uint32_t Vhwa_M2mDofPrms::bPredictor2 |
Predictor used by the base layer, possible values DOF_PREDICTOR_DELEY_LEFT DOF_PREDICTOR_PYR_LEFT DOF_PREDICTOR_PYR_COLOCATED DOF_PREDICTOR_TEMPORAL
Fvid2_Format Vhwa_M2mDofPrms::inOutImgFmt[DOF_MAX_PYR_LVL_SUPPORTED][VHWA_M2M_DOF_MAX_BUFFER] |
Input Frame format, describing input frames storage format Following parametes are used from this pitch = line offset for the input data, used based on the data format dataFormat = Input DataFormat, Only used for Current frame, same value is used for reference frame sfcc = Storage format, Only used for Current frame, same value is used for reference frame
Dof_Config Vhwa_M2mDofPrms::coreCfg |
DOF configuration
Vhwa_FocoPrms Vhwa_M2mDofPrms::focoPrms |
DOF FOCO Parameters