PDK API Guide for J721E
|
Basic SwiP Parameters.
Structure that contains the parameters passed into SwiP_create when creating a SwiP instance. The SwiP_Params_init function should be used to initialize the fields to default values before the application sets the fields manually. The SwiP default parameters are noted in SwiP_Params_init.
Data Fields | |
uintptr_t | arg0 |
uintptr_t | arg1 |
uintptr_t SwiP_Params::arg0 |
Argument 0 passed into the Swi function.
uintptr_t SwiP_Params::arg1 |
Argument 1 passed into the Swi function.