PDK API Guide for J721E
|
ROM messaging: Payload for loading firmware .
Data Fields | |
uint32_t | bufferAddress |
uint32_t | bufferSizeBytes |
uint32_t Sciclient_RomFirmwareLoadPayload_t::bufferAddress |
Address at which the firmware is located
uint32_t Sciclient_RomFirmwareLoadPayload_t::bufferSizeBytes |
Size of firmware. Note : This field is not used read by the ROM. Its value is taken from x509 certificate .