PDK API Guide for J721E
|
Sub-Frame information.
This is used in drivers supporting sub-frame level processing, for application and driver interaction
Data Fields | |
uint32_t | subFrameNum |
uint32_t | numInLines |
uint32_t | numOutLines |
uint32_t Fvid2_SubFrameInfo::subFrameNum |
[IN]/[OUT] Current sub-frame number in this frame, range is from 0 to (number of sub-frames in frame - 1). Set by application and used by driver in case of M2M mode. Set by driver and used by application in case of capture mode.
uint32_t Fvid2_SubFrameInfo::numInLines |
[IN] Number of lines available in input frame at the end of this sub-frame. Used only in M2M mode. Not used in capture mode.
uint32_t Fvid2_SubFrameInfo::numOutLines |
[OUT] Number of lines generated in output buffer after processing current sub-frame. Set by driver and used by application.