PDK API Guide for J721E
|
Structure containing position configuration - used in VCOMP and CIG.
struct Fvid2_PosConfig
Data Fields | |
uint32_t | startX |
uint32_t | startY |
uint32_t Fvid2_PosConfig::startX |
Horizontal offset from which picture needs to be positioned.
uint32_t Fvid2_PosConfig::startY |
Vertical offset from which picture needs to be positioned.