PDK API Guide for J721E
|
Structure for error event parameters Used to register callback for the given set of events.
struct Dof_ErrEventParams
Data Fields | |
uint32_t | errEvents |
Dof_ErrEventCbFxn | cbFxn |
void * | appData |
uint32_t Dof_ErrEventParams::errEvents |
bitmask of error events, Multiple error events can be registered with the same callback, Driver returns bitmask of events, which has occured, Refer to Dof_ErrorEvents for valid values.
Dof_ErrEventCbFxn Dof_ErrEventParams::cbFxn |
Callback function to be call on error events
void* Dof_ErrEventParams::appData |
private data