PDK API Guide for J721E
Csirx_EventStatus Struct Reference

Detailed Description

CSIRX event status parameters. Instance of this structure will passed to the application call-back.

Data Fields

uint32_t eventGroup
 
uint32_t eventMasks
 
Fdrv_Handle drvHandle
 

Field Documentation

uint32_t Csirx_EventStatus::eventGroup

Event group from which event/s has happened. Refer CsirxDrv_EventGroup for event groups

uint32_t Csirx_EventStatus::eventMasks

Events have occurred. Driver can set multiple flags depending on events happened Refer CsirxDrv_EventTypeError for Error events

Fdrv_Handle Csirx_EventStatus::drvHandle

CSIRX driver handle pointer obtained during Fvid2_create()