PDK API Guide for J721E
|
Input args for CPSW_IOCTL_SET_HOSTPORT_TRAFFIC_SHAPING command.
Data Fields | |
CpswPort_TrafficShapingConfig | trafficShapingConfig |
uint32_t | txBlocksRem |
CpswPort_TrafficShapingConfig Cpsw_SetHostPortTrafficShapingInArgs::trafficShapingConfig |
Generic traffic shaping configuration
uint32_t Cpsw_SetHostPortTrafficShapingInArgs::txBlocksRem |
Transmit FIFO blocks that must be free before a non rate-limited host port 0 receive thread can begin sending a packet