PDK API Guide for J721E
|
CPSW IOCTL param.
IOCTL params structure argument for all CPSW IOCTL commands
Data Fields | |
const void * | inArgs |
uint32_t | inArgsSize |
void * | outArgs |
uint32_t | outArgsSize |
const void* Cpsw_IoctlPrms::inArgs |
Pointer to an actual input args struct for the IOCTL cmd
uint32_t Cpsw_IoctlPrms::inArgsSize |
Size of inArgs structure
void* Cpsw_IoctlPrms::outArgs |
Pointer to an actual output args struct for the IOCTL cmd
uint32_t Cpsw_IoctlPrms::outArgsSize |
Size of outArgs structure