PDK API Guide for J721E
|
Input args for CPSW_IOCTL_CLEAR_INTERVLAN_ROUTE_UNI_EGRESS command.
Data Fields | |
Cpsw_InterVlanRouteIngressPktMatchCfg | inPktMatchCfg |
Cpsw_InterVlanEgressPortCfg | egressCfg |
uint32_t | delAleEntryMask |
Cpsw_InterVlanRouteIngressPktMatchCfg Cpsw_ClearInterVlanRouteUniEgressInArgs::inPktMatchCfg |
Ingress packet match criteria for the interVLAN route. If the packet matches the given criteria and the destination port of the packet is host port then the interVLAN route will take effect
Cpsw_InterVlanEgressPortCfg Cpsw_ClearInterVlanRouteUniEgressInArgs::egressCfg |
Egress packet modification configuration for the interVLAN route
uint32_t Cpsw_ClearInterVlanRouteUniEgressInArgs::delAleEntryMask |
Bitmask to indicate which ALE entries associated with the ingress packet match classifier needs to be deleted