PDK API Guide for J721E
|
CPSW utils parameters.
Data Fields | |
Cpsw_PrintFxnCb | printFxn |
Cpsw_TraceFxnCb | traceFxn |
Cpsw_VirtToPhyFxn | virtToPhyFxn |
Cpsw_PhyToVirtFxn | phyToVirtFxn |
Cpsw_PrintFxnCb CpswUtils_Prms::printFxn |
If not NULL, this function will be called to print debug/info message with appropriate string
Cpsw_TraceFxnCb CpswUtils_Prms::traceFxn |
If not NULL, this function will be called to log trace message with appropriate string
Cpsw_VirtToPhyFxn CpswUtils_Prms::virtToPhyFxn |
If not NULL, this function will be called to convert virtual address to physical address to be provided to CPSW. If NULL, the driver will assume a one-one mapping.
Note: The init fxn will initialize this to the default one-one map function CpswUtils_virtToPhyFxn
Cpsw_PhyToVirtFxn CpswUtils_Prms::phyToVirtFxn |
If not NULL, this function will be called to convert physical address to virtual address to access the pointer returned by the CPSW. If NULL, the driver will assume a one-one mapping.
Note: The init fxn will initialize this to the default one-one map function CpswUtils_phyToVirtFxn