PDK API Guide for J721E
|
Input args for CPSW_ALE_IOCTL_SET_POLICER_THREADCFG command.
Configuration to set the thread/flow id associated with a classifier.
Data Fields | |
CpswAle_PolicerMatchParams | policerMatch |
bool | threadIdEnable |
uint32_t | threadId |
CpswAle_PolicerMatchParams CpswAle_SetPolicerThreadConfigInArgs::policerMatch |
Policer match config
bool CpswAle_SetPolicerThreadConfigInArgs::threadIdEnable |
Enable/Disable threadid setting for this policer entry
uint32_t CpswAle_SetPolicerThreadConfigInArgs::threadId |
Thread Id which will be enabled for this policer match