PDK API Guide for J721E
|
Input args for CPSW_ALE_IOCTL_SET_POLICER command.
Data Fields | |
uint32_t | ouiAleEntryIndex |
uint32_t | srcMacAleEntryIndex |
uint32_t | dstMacAleEntryIndex |
uint32_t | ivlanAleEntryIndex |
uint32_t | ovlanAleEntryIndex |
uint32_t | etherTypeAleEntryIndex |
uint32_t | srcIpAleEntryIndex |
uint32_t | dstIpAleEntryIndex |
uint32_t | policerEntryIndex |
uint32_t CpswAle_SetPolicerEntryOutArgs::ouiAleEntryIndex |
OUI ALE table entry index to match Is valid if bit CPSW_ALE_POLICER_MATCH_OUI in policerMatchEnableMask is set
uint32_t CpswAle_SetPolicerEntryOutArgs::srcMacAleEntryIndex |
MAC address ALE table entry index to match source MAC address Is valid if bit CPSW_ALE_POLICER_MATCH_MACSRC in policerMatchEnableMask is set
uint32_t CpswAle_SetPolicerEntryOutArgs::dstMacAleEntryIndex |
MAC address ALE table entry index to match destination MAC address Is valid if bit CPSW_ALE_POLICER_MATCH_MACDST in policerMatchEnableMask is set
uint32_t CpswAle_SetPolicerEntryOutArgs::ivlanAleEntryIndex |
Inner VLAN ALE table entry index to match Is valid if bit CPSW_ALE_POLICER_MATCH_IVLAN in policerMatchEnableMask is set
uint32_t CpswAle_SetPolicerEntryOutArgs::ovlanAleEntryIndex |
Outer VLAN ALE table entry index to match Is valid if bit CPSW_ALE_POLICER_MATCH_OVLAN in policerMatchEnableMask is set
uint32_t CpswAle_SetPolicerEntryOutArgs::etherTypeAleEntryIndex |
Ethertype ALE table entry index to match Is valid if bit CPSW_ALE_POLICER_MATCH_ETHERTYPE in policerMatchEnableMask is set
uint32_t CpswAle_SetPolicerEntryOutArgs::srcIpAleEntryIndex |
IP address ALE table entry index to match as source IP address Is valid if bit CPSW_ALE_POLICER_MATCH_IPSRC in policerMatchEnableMask is set
uint32_t CpswAle_SetPolicerEntryOutArgs::dstIpAleEntryIndex |
IP address ALE table entry index to match as destination IP address Is valid if bit CPSW_ALE_POLICER_MATCH_IPDST in policerMatchEnableMask is set
uint32_t CpswAle_SetPolicerEntryOutArgs::policerEntryIndex |
ALE policer table entry index