PDK API Guide for J721E
|
Output args for CPSW_ALE_IOCTL_SET_DEFAULT_THREADCFG IOCTL command.
InterVLAN routing configuration in ALE is associated with each Policer/Classifier entry.
Data Fields | |
CpswAle_PolicerMatchParams | policerMatch |
bool | enableTTLCheck |
uint32_t | destPortMask |
uint32_t | routeIndex |
uint32_t | egressTrunkIndex |
CpswAle_PolicerMatchParams CpswAle_SetInterVLANConfigInArgs::policerMatch |
Policer match config
bool CpswAle_SetInterVLANConfigInArgs::enableTTLCheck |
Enable TTL field check for non-zero value
uint32_t CpswAle_SetInterVLANConfigInArgs::destPortMask |
Destination Port mask to route the packet matching policerMatch
uint32_t CpswAle_SetInterVLANConfigInArgs::routeIndex |
Destination port route index which has info on the MAC SA/DA to be replaced for the out going packet
uint32_t CpswAle_SetInterVLANConfigInArgs::egressTrunkIndex |
The Egress Trunk Index is the calculated trunk index from the SA,DA or VLAN if modified to that InterVLAN routing will work on trunks as well. The DA, SA and VLAN are ignored for trunk generation on InterVLAN Routing so that this field is the index generated from the Egress Op replacements elclusive or'd together into a three bit index