PDK API Guide for J721E
|
Input args for CPSW_ALE_IOCTL_SET_DEFAULT_THREADCFG IOCTL command.
Data Fields | |
bool | defaultThreadEnable |
uint32_t | threadId |
bool | enablePriorityOR |
bool | disableMacPortDefaultThread |
bool CpswAle_SetDefaultThreadConfigInArgs::defaultThreadEnable |
Default thread enable - When set the switch will use the defthreadval for the host interface thread ID if no classifier is matched. If clear the switch will generate its own thread ID based on port and priority if there is no classifier match
uint32_t CpswAle_SetDefaultThreadConfigInArgs::threadId |
This field specifies the default thread ID value.
bool CpswAle_SetDefaultThreadConfigInArgs::enablePriorityOR |
OR priority of packet with default thread
bool CpswAle_SetDefaultThreadConfigInArgs::disableMacPortDefaultThread |
Do not use default thread for mac only port