PDK API Guide for J721E
|
Structure for bcast/mcast bw limit configuration parameters.
Data Fields | |
uint32_t | portNum |
bool | enableBRateLimitForPort |
bool | enableMRateLimitForPort |
uint32_t | bcastLimitNumPktsPerSec |
uint32_t | mcastLimitNumPktsPerSec |
uint32_t CpswAle_PortBcastMcastRateLimitParams::portNum |
Port number for which BCAST/MCAST rate limiting cfg is to be done
bool CpswAle_PortBcastMcastRateLimitParams::enableBRateLimitForPort |
Enable Broadcast Rate Limit for port. If set to TRUE, bcastLimitNumPktsPerSec should be non-zero
bool CpswAle_PortBcastMcastRateLimitParams::enableMRateLimitForPort |
Enable Multicast Rate Limit for port. If set to TRUE, mcastLimitNumPktsPerSec should be non-zero
uint32_t CpswAle_PortBcastMcastRateLimitParams::bcastLimitNumPktsPerSec |
Broadcast packet limit per sec
uint32_t CpswAle_PortBcastMcastRateLimitParams::mcastLimitNumPktsPerSec |
Multicast packet limit per sec