PDK API Guide for J721E
|
Structure for MAC authentication configuration.
Data Fields | |
bool | enableAuthMode |
uint32_t | macAuthDisableMask |
bool CpswAle_MacAuthConfig::enableAuthMode |
Enable MAC Authorization mode
uint32_t CpswAle_MacAuthConfig::macAuthDisableMask |
Disable Port authorization - When set will allow unknown addresses to arrive on a switch in authorization mode. It is intended for device to device network connection on ports which do not require MACSEC encryption